<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Developer Resources for Android Customisation?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Developer-Resources-for-Android-Customisation/m-p/331595#M44798</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've got an iMX6 based dev board for android, and I need to customize some things for our product. But I cannot find any usable resources/documents on this topic. Android seems to be App, App, and App again, but if you need to deal with the low level stuff, you only get a "leaflet" telling you how to compile the stuff from an Android BSP and copy it to the SD, but no further help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, for example, I stubled about the "navigation bar problem". When I used the desktop monitor or the large touch screen with a 1280x800 resolution, the navigation bar with the home and back button is there. If I use the lower resolution display (or the HDMI with a sumulated lower resolution) with 800x480, the navigation bar is gone. Somewhere in the Android source jungle there must be a constant or configured value that tells Android from which height it is allowed to have a navigation bar. But hwere can I find documentation on that? Where should I start?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or: This dev board, as well as the final product, has no battery. But it still cries for a charger, and if I don't mark "don't sleep" in the developers options, it reboots after a few minutes. How cann I tell Android that a charger is not necessary? I could not find any resources on this - its all app, apps, apps, or "how to prolong my battary life", but nothing for adaption on a specific hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any tips for my specific problems? Any hints or resources to get insights into adapting/configuring Android?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;Christian Treczoks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Jan 2015 10:53:47 GMT</pubDate>
    <dc:creator>christiantreczo</dc:creator>
    <dc:date>2015-01-29T10:53:47Z</dc:date>
    <item>
      <title>Developer Resources for Android Customisation?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Developer-Resources-for-Android-Customisation/m-p/331595#M44798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've got an iMX6 based dev board for android, and I need to customize some things for our product. But I cannot find any usable resources/documents on this topic. Android seems to be App, App, and App again, but if you need to deal with the low level stuff, you only get a "leaflet" telling you how to compile the stuff from an Android BSP and copy it to the SD, but no further help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, for example, I stubled about the "navigation bar problem". When I used the desktop monitor or the large touch screen with a 1280x800 resolution, the navigation bar with the home and back button is there. If I use the lower resolution display (or the HDMI with a sumulated lower resolution) with 800x480, the navigation bar is gone. Somewhere in the Android source jungle there must be a constant or configured value that tells Android from which height it is allowed to have a navigation bar. But hwere can I find documentation on that? Where should I start?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or: This dev board, as well as the final product, has no battery. But it still cries for a charger, and if I don't mark "don't sleep" in the developers options, it reboots after a few minutes. How cann I tell Android that a charger is not necessary? I could not find any resources on this - its all app, apps, apps, or "how to prolong my battary life", but nothing for adaption on a specific hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any tips for my specific problems? Any hints or resources to get insights into adapting/configuring Android?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;Christian Treczoks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jan 2015 10:53:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Developer-Resources-for-Android-Customisation/m-p/331595#M44798</guid>
      <dc:creator>christiantreczo</dc:creator>
      <dc:date>2015-01-29T10:53:47Z</dc:date>
    </item>
    <item>
      <title>Re: Developer Resources for Android Customisation?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Developer-Resources-for-Android-Customisation/m-p/331596#M44799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the Android Developers resource:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://developer.android.com/index.html" target="_blank"&gt;http://developer.android.com/index.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jan 2015 13:32:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Developer-Resources-for-Android-Customisation/m-p/331596#M44799</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-01-29T13:32:50Z</dc:date>
    </item>
  </channel>
</rss>