<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: SDMA transfer to/from memory shared with PCIe root</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SDMA-transfer-to-from-memory-shared-with-PCIe-root/m-p/331008#M44687</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are no direct references, however&lt;/P&gt;&lt;P&gt;for example there is no PCIe in&lt;/P&gt;&lt;P&gt;Table A-1. SDMA Scripts Overview &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQRM&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Oct 2014 08:20:55 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-10-17T08:20:55Z</dc:date>
    <item>
      <title>SDMA transfer to/from memory shared with PCIe root</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDMA-transfer-to-from-memory-shared-with-PCIe-root/m-p/331005#M44684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an imx6 set up as PCIe endpoint where the lower 16MB of DDR memory (address 0x10000000-0x11000000) is shared with the PCIe root on the other side of the PCIe link.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use SDMA on the imx6 to copy to/from this memory. Is this possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reason I ask is because of this discussion &lt;A href="https://community.nxp.com/thread/305942"&gt;PCIe DMA problems with i.MX6&lt;/A&gt; which seems to imply that that is not the case.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Oct 2014 16:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDMA-transfer-to-from-memory-shared-with-PCIe-root/m-p/331005#M44684</guid>
      <dc:creator>FredrikMoller</dc:creator>
      <dc:date>2014-10-16T16:51:56Z</dc:date>
    </item>
    <item>
      <title>Re: SDMA transfer to/from memory shared with PCIe root</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDMA-transfer-to-from-memory-shared-with-PCIe-root/m-p/331006#M44685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Frederik&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes correct, SDMA can not be used with PCIe module.&lt;/P&gt;&lt;P&gt;Also it may be useful to look at&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95014"&gt;i.MX6Q PCIe EP/RC Validation System&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Oct 2014 23:51:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDMA-transfer-to-from-memory-shared-with-PCIe-root/m-p/331006#M44685</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-16T23:51:34Z</dc:date>
    </item>
    <item>
      <title>Re: SDMA transfer to/from memory shared with PCIe root</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDMA-transfer-to-from-memory-shared-with-PCIe-root/m-p/331007#M44686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Btw, you don't happen to know where this limitation is documented in the reference manual for imx6?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Fredrik&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Oct 2014 08:15:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDMA-transfer-to-from-memory-shared-with-PCIe-root/m-p/331007#M44686</guid>
      <dc:creator>FredrikMoller</dc:creator>
      <dc:date>2014-10-17T08:15:49Z</dc:date>
    </item>
    <item>
      <title>Re: SDMA transfer to/from memory shared with PCIe root</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDMA-transfer-to-from-memory-shared-with-PCIe-root/m-p/331008#M44687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are no direct references, however&lt;/P&gt;&lt;P&gt;for example there is no PCIe in&lt;/P&gt;&lt;P&gt;Table A-1. SDMA Scripts Overview &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQRM&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Oct 2014 08:20:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDMA-transfer-to-from-memory-shared-with-PCIe-root/m-p/331008#M44687</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-17T08:20:55Z</dc:date>
    </item>
  </channel>
</rss>