<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TEMPMON accuracy without RTC XTAL in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/TEMPMON-accuracy-without-RTC-XTAL/m-p/330556#M44621</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi fred&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;no ring oscillator will not introduce additional inaccuracies.&lt;/P&gt;&lt;P&gt;BTW operation without crystal is not recommended due to ERR007926.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Oct 2014 23:59:06 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-10-16T23:59:06Z</dc:date>
    <item>
      <title>TEMPMON accuracy without RTC XTAL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TEMPMON-accuracy-without-RTC-XTAL/m-p/330555#M44620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We intend to use the i.MX6 Dual without the RTC crystal, yet I see that TEMPMON takes the 32KHz clock as input. Will the ring oscillator wide frequency tolerance lead to inaccurate die temperature readings?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Oct 2014 15:27:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TEMPMON-accuracy-without-RTC-XTAL/m-p/330555#M44620</guid>
      <dc:creator>fredstewart</dc:creator>
      <dc:date>2014-10-16T15:27:34Z</dc:date>
    </item>
    <item>
      <title>Re: TEMPMON accuracy without RTC XTAL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TEMPMON-accuracy-without-RTC-XTAL/m-p/330556#M44621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi fred&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;no ring oscillator will not introduce additional inaccuracies.&lt;/P&gt;&lt;P&gt;BTW operation without crystal is not recommended due to ERR007926.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Oct 2014 23:59:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TEMPMON-accuracy-without-RTC-XTAL/m-p/330556#M44621</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-10-16T23:59:06Z</dc:date>
    </item>
  </channel>
</rss>