<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Bootup with yocto build image getting stuck</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Bootup-with-yocto-build-image-getting-stuck/m-p/330286#M44571</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dan,&lt;/P&gt;&lt;P&gt;I recreated the SD card using the User Guide and was successful in booting.&lt;/P&gt;&lt;P&gt;Some dtb related issue it seems. Will try TFTP boot later.&lt;/P&gt;&lt;P&gt;Marking this as assumend answered.&lt;/P&gt;&lt;P&gt;Sorry I didn't update the issue earlier.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Boot parameters saved on the new SD card.&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; printenv&lt;/P&gt;&lt;P&gt;baudrate=115200&lt;/P&gt;&lt;P&gt;boot_fdt=try&lt;/P&gt;&lt;P&gt;bootargs_base=setenv bootargs console=ttymxc0,115200&lt;/P&gt;&lt;P&gt;bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24&lt;/P&gt;&lt;P&gt;bootcmd=run bootcmd_mmc&lt;/P&gt;&lt;P&gt;bootcmd_mfg=run mfgtool_args;bootm ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;/P&gt;&lt;P&gt;bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 1;mmc read ${loadaddr} 0x800 0x4000;mmc read ${fdt_addr} 0x5000 0x800;bootm ${loadaddr} - ${fdt_addr}&lt;/P&gt;&lt;P&gt;bootdelay=1&lt;/P&gt;&lt;P&gt;bootscript=echo Running bootscript from mmc ...; source&lt;/P&gt;&lt;P&gt;console=ttymxc0&lt;/P&gt;&lt;P&gt;ethact=FEC&lt;/P&gt;&lt;P&gt;ethaddr=00:04:9f:02:df:ac&lt;/P&gt;&lt;P&gt;ethprime=FEC&lt;/P&gt;&lt;P&gt;fdt_addr=0x18000000&lt;/P&gt;&lt;P&gt;fdt_file=imx6q-sabresd.dtb&lt;/P&gt;&lt;P&gt;fdt_high=0xffffffff&lt;/P&gt;&lt;P&gt;initrd_addr=0x12C00000&lt;/P&gt;&lt;P&gt;initrd_high=0xffffffff&lt;/P&gt;&lt;P&gt;ip_dyn=yes&lt;/P&gt;&lt;P&gt;loadaddr=0x12000000&lt;/P&gt;&lt;P&gt;loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};&lt;/P&gt;&lt;P&gt;loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}&lt;/P&gt;&lt;P&gt;loaduimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${uimage}&lt;/P&gt;&lt;P&gt;mfgtool_args=setenv bootargs console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x&lt;/P&gt;&lt;P&gt;37FF g_mass_storage.iSerialNumber="" enable_wait_mode=off &lt;/P&gt;&lt;P&gt;mmcargs=setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot}&lt;/P&gt;&lt;P&gt;mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootm ${loadaddr} - ${fdt_addr}; else if test ${b&lt;/P&gt;&lt;P&gt;oot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;&lt;/P&gt;&lt;P&gt;mmcdev=1&lt;/P&gt;&lt;P&gt;mmcpart=1&lt;/P&gt;&lt;P&gt;mmcroot=/dev/mmcblk0p2 rootwait rw&lt;/P&gt;&lt;P&gt;netargs=setenv bootargs console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp&lt;/P&gt;&lt;P&gt;netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${uimage}; if test ${boot_fdt} = yes&lt;/P&gt;&lt;P&gt; || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot&lt;/P&gt;&lt;P&gt; load the DT; fi; fi; else bootm; fi;&lt;/P&gt;&lt;P&gt;script=boot.scr&lt;/P&gt;&lt;P&gt;uimage=uImage&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Environment size: 2211/8188 bytes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Oct 2014 06:35:23 GMT</pubDate>
    <dc:creator>subodh</dc:creator>
    <dc:date>2014-10-21T06:35:23Z</dc:date>
    <item>
      <title>Bootup with yocto build image getting stuck</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bootup-with-yocto-build-image-getting-stuck/m-p/330284#M44569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I build an image using the yocto build refering to the following link.&lt;/P&gt;&lt;P&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/fsl-arm-yocto-bsp.git/tree/README?h=imx-3.10.31-1.1.0_beta" title="http://git.freescale.com/git/cgit.cgi/imx/fsl-arm-yocto-bsp.git/tree/README?h=imx-3.10.31-1.1.0_beta"&gt;fsl-arm-yocto-bsp.git - Freescale i.MX Yocto Project manifests&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the NFS boot fails with the 3.10 kernel, hence I tried the 3.0 kernel instead. &lt;/P&gt;&lt;P&gt;Please can anyone help me in resolving this issue.&lt;/P&gt;&lt;P&gt;I have also posted the issue on meta fsl&lt;/P&gt;&lt;P&gt;&lt;A href="https://lists.yoctoproject.org/pipermail/meta-freescale/2014-October/010865.html" title="https://lists.yoctoproject.org/pipermail/meta-freescale/2014-October/010865.html"&gt;https://lists.yoctoproject.org/pipermail/meta-freescale/2014-October/010865.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following are the boot up logs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using FEC device&lt;/P&gt;&lt;P&gt;TFTP from server 10.1.1.41; our IP address is 10.1.1.32&lt;/P&gt;&lt;P&gt;Filename 'uImage_alsa'.&lt;/P&gt;&lt;P&gt;Load address: 0x10800000&lt;/P&gt;&lt;P&gt;Loading: #################################################################&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #################################################################&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #################################################################&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #############################&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.3 MiB/s&lt;/P&gt;&lt;P&gt;done&lt;/P&gt;&lt;P&gt;Bytes transferred = 3279476 (320a74 hex)&lt;/P&gt;&lt;P&gt;## Booting kernel from Legacy Image at 10800000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; Linux-3.0.35-2666-gbdde708&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; ARM Linux Kernel Image (uncompressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 3279412 Bytes = 3.1 MiB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 10008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 10008000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Loading Kernel Image ... OK&lt;/P&gt;&lt;P&gt;No gpc device node -9, force to ldo-enable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Uncompressing Linux... done, booting the kernel.&lt;/P&gt;&lt;P&gt;Linux version 3.0.35-2666-gbdde708 (ufouser@ufouser-virtual-machine) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #&lt;/P&gt;&lt;P&gt;7 SMP PREEMPT Wed Sep 3 12:59:20 IST 2014&lt;/P&gt;&lt;P&gt;CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d&lt;/P&gt;&lt;P&gt;CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;/P&gt;&lt;P&gt;Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board&lt;/P&gt;&lt;P&gt;Memory policy: ECC disabled, Data cache writealloc&lt;/P&gt;&lt;P&gt;CPU identified as i.MX6Q, silicon rev 1.2&lt;/P&gt;&lt;P&gt;PERCPU: Embedded 7 pages/cpu @8c008000 s5184 r8192 d15296 u32768&lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 227328&lt;/P&gt;&lt;P&gt;Kernel command line: console=ttymxc0,115200 ip=10.1.1.32:10.1.1.41:10.1.1.1:255.255.255.0::eth0:off nwhwconf=device:eth0,hwaddr:00:04:9f:02:df:ac rw root=/dev/nfs nfsroot=/home&lt;/P&gt;&lt;P&gt;/subodh/TFTP-FS,v3,tcp video=mxcfb1:dev=1db,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24&lt;/P&gt;&lt;P&gt;PID hash table entries: 4096 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)&lt;/P&gt;&lt;P&gt;Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;/P&gt;&lt;P&gt;Memory: 640MB 256MB = 896MB total&lt;/P&gt;&lt;P&gt;Memory: 901636k/901636k available, 146940k reserved, 0K highmem&lt;/P&gt;&lt;P&gt;Virtual kernel memory layout:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xfff00000 - 0xfffe0000&amp;nbsp;&amp;nbsp; ( 896 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0xf4600000 - 0xffe00000&amp;nbsp;&amp;nbsp; ( 184 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0xc0800000 - 0xf2000000&amp;nbsp;&amp;nbsp; ( 792 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0x80000000 - 0xc0000000&amp;nbsp;&amp;nbsp; (1024 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pkmap&amp;nbsp;&amp;nbsp; : 0x7fe00000 - 0x80000000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 2 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0x7f000000 - 0x7fe00000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 14 MB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0x80008000 - 0x8003b000&amp;nbsp;&amp;nbsp; ( 204 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0x8003b000 - 0x80610010&amp;nbsp;&amp;nbsp; (5973 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0x80612000 - 0x80664dc0&amp;nbsp;&amp;nbsp; ( 332 kB)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bss : 0x80664de4 - 0x806913f4&amp;nbsp;&amp;nbsp; ( 178 kB)&lt;/P&gt;&lt;P&gt;SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1&lt;/P&gt;&lt;P&gt;Preemptible hierarchical RCU implementation.&lt;/P&gt;&lt;P&gt;NR_IRQS:624&lt;/P&gt;&lt;P&gt;MXC GPIO hardware&lt;/P&gt;&lt;P&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms&lt;/P&gt;&lt;P&gt;arm_max_freq=1GHz&lt;/P&gt;&lt;P&gt;MXC_Early serial console at MMIO 0x2020000 (options '115200')&lt;/P&gt;&lt;P&gt;bootconsole [ttymxc0] enabled&lt;/P&gt;&lt;P&gt;Console: colour dummy device 80x30&lt;/P&gt;&lt;P&gt;Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)&lt;/P&gt;&lt;P&gt;pid_max: default: 32768 minimum: 301&lt;/P&gt;&lt;P&gt;Mount-cache hash table entries: 512&lt;/P&gt;&lt;P&gt;CPU: Testing write buffer coherency: ok&lt;/P&gt;&lt;P&gt;hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available&lt;/P&gt;&lt;P&gt;CPU1: Booted secondary processor&lt;/P&gt;&lt;P&gt;CPU2: Booted secondary processor&lt;/P&gt;&lt;P&gt;CPU3: Booted secondary processor&lt;/P&gt;&lt;P&gt;Brought up 4 CPUs&lt;/P&gt;&lt;P&gt;SMP: Total of 4 processors activated (6324.22 BogoMIPS).&lt;/P&gt;&lt;P&gt;print_constraints: dummy: &lt;/P&gt;&lt;P&gt;NET: Registered protocol family 16&lt;/P&gt;&lt;P&gt;print_constraints: vddpu: 725 &amp;lt;--&amp;gt; 1300 mV at 700 mV fast normal &lt;/P&gt;&lt;P&gt;print_constraints: vddcore: 725 &amp;lt;--&amp;gt; 1300 mV at 1150 mV fast normal &lt;/P&gt;&lt;P&gt;print_constraints: vddsoc: 725 &amp;lt;--&amp;gt; 1300 mV at 1175 mV fast normal &lt;/P&gt;&lt;P&gt;print_constraints: vdd2p5: 2000 &amp;lt;--&amp;gt; 2775 mV at 2400 mV fast normal &lt;/P&gt;&lt;P&gt;print_constraints: vdd1p1: 800 &amp;lt;--&amp;gt; 1400 mV at 1100 mV fast normal &lt;/P&gt;&lt;P&gt;print_constraints: vdd3p0: 2625 &amp;lt;--&amp;gt; 3400 mV at 3000 mV fast normal &lt;/P&gt;&lt;P&gt;No AHCI save PWR: PDDQ enabled&lt;/P&gt;&lt;P&gt;hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.&lt;/P&gt;&lt;P&gt;hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.&lt;/P&gt;&lt;P&gt;hw-breakpoint: maximum watchpoint size is 4 bytes.&lt;/P&gt;&lt;P&gt;L310 cache controller enabled&lt;/P&gt;&lt;P&gt;l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B&lt;/P&gt;&lt;P&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;/P&gt;&lt;P&gt;mxs-dma mxs-dma-apbh: initialized&lt;/P&gt;&lt;P&gt;print_constraints: SPKVDD: 4200 mV &lt;/P&gt;&lt;P&gt;print_constraints: vmmc: 3300 mV &lt;/P&gt;&lt;P&gt;SCSI subsystem initialized&lt;/P&gt;&lt;P&gt;spi_imx imx6q-ecspi.0: probed&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbfs&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver hub&lt;/P&gt;&lt;P&gt;usbcore: registered new device driver usb&lt;/P&gt;&lt;P&gt;mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 1&lt;/P&gt;&lt;P&gt;mc_pfuze 1-0008: FAB: 0 ,FIN: 0&lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SW1A: 300 &amp;lt;--&amp;gt; 1875 mV at 1300 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SW1B: 300 &amp;lt;--&amp;gt; 1875 mV at 300 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SW1C: 300 &amp;lt;--&amp;gt; 1875 mV at 1300 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SW2: 800 &amp;lt;--&amp;gt; 3950 mV at 3300 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SW3A: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SW3B: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SW4: 800 &amp;lt;--&amp;gt; 3950 mV at 3150 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_SWBST: 5000 &amp;lt;--&amp;gt; 5150 mV at 5000 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VSNVS: 1200 &amp;lt;--&amp;gt; 3000 mV at 1800 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VREFDDR: at 750 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VGEN1: 800 &amp;lt;--&amp;gt; 1550 mV at 1500 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VGEN2: 800 &amp;lt;--&amp;gt; 1550 mV at 1500 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VGEN3: 1800 &amp;lt;--&amp;gt; 3300 mV at 2800 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VGEN4: 1800 &amp;lt;--&amp;gt; 3300 mV at 1800 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VGEN5: 1800 &amp;lt;--&amp;gt; 3300 mV at 3000 mV &lt;/P&gt;&lt;P&gt;print_constraints: PFUZE100_VGEN6: 1800 &amp;lt;--&amp;gt; 3300 mV at 3300 mV &lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)&lt;/P&gt;&lt;P&gt;Advanced Linux Sound Architecture Driver Version 1.0.24.&lt;/P&gt;&lt;P&gt;Bluetooth: Core ver 2.16&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 31&lt;/P&gt;&lt;P&gt;Bluetooth: HCI device and connection manager initialized&lt;/P&gt;&lt;P&gt;Bluetooth: HCI socket layer initialized&lt;/P&gt;&lt;P&gt;Bluetooth: L2CAP socket layer initialized&lt;/P&gt;&lt;P&gt;Bluetooth: SCO socket layer initialized&lt;/P&gt;&lt;P&gt;max17135 2-0048: PMIC MAX17135 for eInk display&lt;/P&gt;&lt;P&gt;i2c-core: driver [max17135] using legacy suspend method&lt;/P&gt;&lt;P&gt;i2c-core: driver [max17135] using legacy resume method&lt;/P&gt;&lt;P&gt;Switching to clocksource mxc_timer1&lt;/P&gt;&lt;P&gt;Clockevents: could not switch to one-shot mode:&lt;/P&gt;&lt;P&gt;Clockevents: could not switch to one-shot mode:&lt;/P&gt;&lt;P&gt;Clockevents: could not switch to one-shot mode:&lt;/P&gt;&lt;P&gt;Clockevents: could not switch to one-shot mode: dummy_timer is not functional.&lt;/P&gt;&lt;P&gt; dummy_timer is not functional.&lt;/P&gt;&lt;P&gt; dummy_timer is not functional.&lt;/P&gt;&lt;P&gt;Could not switch to high resolution mode on CPU 0&lt;/P&gt;&lt;P&gt;Could not switch to high resolution mode on CPU 1&lt;/P&gt;&lt;P&gt;Could not switch to high resolution mode on CPU 2&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 2&lt;/P&gt;&lt;P&gt;IP route cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;/P&gt;&lt;P&gt;TCP established hash table entries: 131072 (order: 8, 1048576 bytes)&lt;/P&gt;&lt;P&gt;TCP bind hash table entries: 65536 (order: 7, 786432 bytes)&lt;/P&gt;&lt;P&gt;TCP: Hash tables configured (established 131072 bind 65536)&lt;/P&gt;&lt;P&gt;TCP reno registered&lt;/P&gt;&lt;P&gt;UDP hash table entries: 512 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 1&lt;/P&gt;&lt;P&gt;RPC: Registered named UNIX socket transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered udp transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered tcp transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;/P&gt;&lt;P&gt;PMU: registered new PMU device of type 0&lt;/P&gt;&lt;P&gt;Static Power Management for Freescale i.MX6&lt;/P&gt;&lt;P&gt;wait mode is enabled for i.MX6&lt;/P&gt;&lt;P&gt;cpaddr = c0880000 suspend_iram_base=c091c000&lt;/P&gt;&lt;P&gt;PM driver module loaded&lt;/P&gt;&lt;P&gt;IMX usb wakeup probe&lt;/P&gt;&lt;P&gt;cpu regulator mode:ldo_bypass&lt;/P&gt;&lt;P&gt;_regulator_get: get() with no identifier&lt;/P&gt;&lt;P&gt;mx6_cpu_regulator_init: failed to get pu regulator&lt;/P&gt;&lt;P&gt;i.MXC CPU frequency driver&lt;/P&gt;&lt;P&gt;JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.&lt;/P&gt;&lt;P&gt;msgmni has been set to 1761&lt;/P&gt;&lt;P&gt;cryptodev: driver loaded.&lt;/P&gt;&lt;P&gt;io scheduler noop registered&lt;/P&gt;&lt;P&gt;io scheduler deadline registered&lt;/P&gt;&lt;P&gt;io scheduler cfq registered (default)&lt;/P&gt;&lt;P&gt; dummy_timer is not functional.&lt;/P&gt;&lt;P&gt;Could not switch to high resolution mode on CPU 3&lt;/P&gt;&lt;P&gt;mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver hdmi&lt;/P&gt;&lt;P&gt;mxc_hdmi mxc_hdmi: Detected HDMI controller 0x13:0xa:0xa0:0xc1&lt;/P&gt;&lt;P&gt;fbcvt: 1920x1080@60: CVT Name - 2.073M9&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)&lt;/P&gt;&lt;P&gt;Console: switching to colour frame buffer device 240x67&lt;/P&gt;&lt;P&gt;mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver 1db&lt;/P&gt;&lt;P&gt;mxc_sdc_fb mxc_sdc_fb.1: NO mxc display driver found!&lt;/P&gt;&lt;P&gt;mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver lcd&lt;/P&gt;&lt;P&gt;mxc_sdc_fb mxc_sdc_fb.2: ipu0-di0 already in use&lt;/P&gt;&lt;P&gt;mxc_sdc_fb: probe of mxc_sdc_fb.2 failed with error -16&lt;/P&gt;&lt;P&gt;mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb&lt;/P&gt;&lt;P&gt;_regulator_get: get() with no identifier&lt;/P&gt;&lt;P&gt;imx-sdma imx-sdma: loaded firmware 1.1&lt;/P&gt;&lt;P&gt;imx-sdma imx-sdma: initialized&lt;/P&gt;&lt;P&gt;Serial: IMX driver&lt;/P&gt;&lt;P&gt;imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX&lt;/P&gt;&lt;P&gt;imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX&lt;/P&gt;&lt;P&gt;console [ttymxc0] enabled, bootconsole disabled&lt;/P&gt;&lt;P&gt;console [ttymxc0] enabled, bootconsole disabled&lt;/P&gt;&lt;P&gt;loop: module loaded&lt;/P&gt;&lt;P&gt;m25p80 spi0.0: found m25p05-nonjedec, expected sst25vf016b&lt;/P&gt;&lt;P&gt;m25p80 spi0.0: m25p05-nonjedec (64 Kbytes)&lt;/P&gt;&lt;P&gt;Creating 2 MTD partitions on "m25p80":&lt;/P&gt;&lt;P&gt;0x000000000000-0x000000100000 : "bootloader"&lt;/P&gt;&lt;P&gt;mtd: partition "bootloader" extends beyond the end of device "m25p80" -- size truncated to 0x10000&lt;/P&gt;&lt;P&gt;0x000000010000-0x000000010000 : "kernel"&lt;/P&gt;&lt;P&gt;mtd: partition "kernel" is out of reach -- disabled&lt;/P&gt;&lt;P&gt;GPMI NAND driver registered. (IMX)&lt;/P&gt;&lt;P&gt;vcan: Virtual CAN interface driver&lt;/P&gt;&lt;P&gt;FEC Ethernet Driver&lt;/P&gt;&lt;P&gt;fec_enet_mii_bus: probed&lt;/P&gt;&lt;P&gt;Initializing USB Mass Storage driver...&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usb-storage&lt;/P&gt;&lt;P&gt;USB Mass Storage support registered.&lt;/P&gt;&lt;P&gt;ARC USBOTG Device Controller driver (1 August 2005)&lt;/P&gt;&lt;P&gt;add wake up source irq 75&lt;/P&gt;&lt;P&gt;g_file_storage gadget: controller 'fsl-usb2-udc' not recognized&lt;/P&gt;&lt;P&gt;check_parameters:UTP settings are in place now, overriding defaults&lt;/P&gt;&lt;P&gt;g_file_storage gadget: No serial-number string provided!&lt;/P&gt;&lt;P&gt;g_file_storage gadget: File-backed Storage Gadget, version: 1 September 2010&lt;/P&gt;&lt;P&gt;g_file_storage gadget: Number of LUNs=1&lt;/P&gt;&lt;P&gt;fsl-usb2-udc: bind to driver g_file_storage &lt;/P&gt;&lt;P&gt;mousedev: PS/2 mouse device common for all mice&lt;/P&gt;&lt;P&gt;egalax_ts 1-0004: egalax_ts: failed to read firmware version&lt;/P&gt;&lt;P&gt;egalax_ts: probe of 1-0004 failed with error -5&lt;/P&gt;&lt;P&gt;egalax_ts 2-0004: egalax_ts: failed to read firmware version&lt;/P&gt;&lt;P&gt;egalax_ts: probe of 2-0004 failed with error -5&lt;/P&gt;&lt;P&gt;snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0&lt;/P&gt;&lt;P&gt;i2c /dev entries driver&lt;/P&gt;&lt;P&gt;Linux video capture interface: v2.00&lt;/P&gt;&lt;P&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16&lt;/P&gt;&lt;P&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17&lt;/P&gt;&lt;P&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18&lt;/P&gt;&lt;P&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19&lt;/P&gt;&lt;P&gt;imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)&lt;/P&gt;&lt;P&gt;Bluetooth: Virtual HCI driver ver 1.3&lt;/P&gt;&lt;P&gt;Bluetooth: Generic Bluetooth USB driver ver 0.6&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver btusb&lt;/P&gt;&lt;P&gt;sdhci: Secure Digital Host Controller Interface driver&lt;/P&gt;&lt;P&gt;sdhci: Copyright(c) Pierre Ossman&lt;/P&gt;&lt;P&gt;mmc0: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA&lt;/P&gt;&lt;P&gt;mmc1: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA&lt;/P&gt;&lt;P&gt;mmc2: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA&lt;/P&gt;&lt;P&gt;mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed&lt;/P&gt;&lt;P&gt;VPU initialized&lt;/P&gt;&lt;P&gt;mxc_asrc registered&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbhid&lt;/P&gt;&lt;P&gt;usbhid: USB HID core driver&lt;/P&gt;&lt;P&gt;mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio&lt;/P&gt;&lt;P&gt;Cirrus Logic CS42888 ALSA SoC Codec Driver&lt;/P&gt;&lt;P&gt;i2c-core: driver [cs42888] using legacy suspend method&lt;/P&gt;&lt;P&gt;i2c-core: driver [cs42888] using legacy resume method&lt;/P&gt;&lt;P&gt;wm8962 0-001a: customer id 0 revision D&lt;/P&gt;&lt;P&gt;input: WM8962 Beep Generator as /devices/platform/imx-i2c.0/i2c-0/0-001a/input/input0&lt;/P&gt;&lt;P&gt;asoc: wm8962 &amp;lt;-&amp;gt; imx-ssi.1 mapping ok&lt;/P&gt;&lt;P&gt;input: wm8962-audio DMIC as /devices/platform/soc-audio.5/sound/card0/input1&lt;/P&gt;&lt;P&gt;input: wm8962-audio Ext Spk as /devices/platform/soc-audio.5/sound/card0/input2&lt;/P&gt;&lt;P&gt;imx_3stack asoc driver&lt;/P&gt;&lt;P&gt;asoc: mxc-hdmi-soc &amp;lt;-&amp;gt; imx-hdmi-soc-dai.0 mapping ok&lt;/P&gt;&lt;P&gt;mmc0: new high speed DDR MMC card at address 0001&lt;/P&gt;&lt;P&gt;mmcblk0: mmc0:0001 SEM08G 7.39 GiB &lt;/P&gt;&lt;P&gt;ALSA device list:&lt;/P&gt;&lt;P&gt;&amp;nbsp; #0: wm8962-audio&lt;/P&gt;&lt;P&gt;&amp;nbsp; #1: imx-hdmi-soc&lt;/P&gt;&lt;P&gt;TCP cubic registered&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 17&lt;/P&gt;&lt;P&gt;can: controller area network core (rev 20090105 abi 8)&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 29&lt;/P&gt;&lt;P&gt;can: raw protocol (rev 20090105)&lt;/P&gt;&lt;P&gt;can: broadcast manager protocol (rev 20090105 t)&lt;/P&gt;&lt;P&gt;Bluetooth: RFCOMM TTY layer initialized&lt;/P&gt;&lt;P&gt;Bluetooth: RFCOMM socket layer initialized&lt;/P&gt;&lt;P&gt;Bluetooth: RFCOMM ver 1.11&lt;/P&gt;&lt;P&gt;Bluetooth: BNEP (Ethernet Emulation) ver 1.3&lt;/P&gt;&lt;P&gt;Bluetooth: BNEP filters: protocol multicast&lt;/P&gt;&lt;P&gt;Bluetooth: HIDP (Human Interface Emulation) ver 1.2&lt;/P&gt;&lt;P&gt;Registering the dns_resolver key type&lt;/P&gt;&lt;P&gt;VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4&lt;/P&gt;&lt;P&gt;mmcblk0boot0: mmc0:0001 SEM08G partition 1 2.00 MiB&lt;/P&gt;&lt;P&gt;Bus freq driver module loaded&lt;/P&gt;&lt;P&gt;Bus freq driver Enabled&lt;/P&gt;&lt;P&gt;mmcblk0boot1: mmc0:0001 SEM08G partition 2 2.00 MiB&lt;/P&gt;&lt;P&gt; mmcblk0: p1 p2&lt;/P&gt;&lt;P&gt;mxc_dvfs_core_probe&lt;/P&gt;&lt;P&gt;DVFS driver module loaded&lt;/P&gt;&lt;P&gt;regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 06:54:45 UTC (24885)&lt;/P&gt;&lt;P&gt; mmcblk0boot1: unknown partition table&lt;/P&gt;&lt;P&gt;eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=1:01, irq=-1)&lt;/P&gt;&lt;P&gt; mmcblk0boot0: unknown partition table&lt;/P&gt;&lt;P&gt;mmc2: new high speed SDHC card at address aaaa&lt;/P&gt;&lt;P&gt;mmcblk1: mmc2:aaaa SU08G 7.40 GiB &lt;/P&gt;&lt;P&gt; mmcblk1: p1&lt;/P&gt;&lt;P&gt;PHY: 1:01 - Link is Up - 100/Full&lt;/P&gt;&lt;P&gt;IP-Config: Complete:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; device=eth0, addr=10.1.1.32, mask=255.255.255.0, gw=10.1.1.1,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; host=10.1.1.32, domain=, nis-domain=(none),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bootserver=10.1.1.41, rootserver=10.1.1.41, rootpath=&lt;/P&gt;&lt;P&gt;VFS: Mounted root (nfs filesystem) on device 0:12.&lt;/P&gt;&lt;P&gt;Freeing init memory: 204K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Oct 2014 14:06:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bootup-with-yocto-build-image-getting-stuck/m-p/330284#M44569</guid>
      <dc:creator>subodh</dc:creator>
      <dc:date>2014-10-16T14:06:05Z</dc:date>
    </item>
    <item>
      <title>Re: Bootup with yocto build image getting stuck</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bootup-with-yocto-build-image-getting-stuck/m-p/330285#M44570</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sudbodh C,&lt;/P&gt;&lt;P&gt;Can you show me your parameters setting in u-boot? When your u-boot boot up, you can put in "print" in console line. Then you can see all the environment you have set.&lt;BR /&gt;Have a great day&lt;BR /&gt;(Dan)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Oct 2014 06:24:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bootup-with-yocto-build-image-getting-stuck/m-p/330285#M44570</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2014-10-21T06:24:39Z</dc:date>
    </item>
    <item>
      <title>Re: Bootup with yocto build image getting stuck</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bootup-with-yocto-build-image-getting-stuck/m-p/330286#M44571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dan,&lt;/P&gt;&lt;P&gt;I recreated the SD card using the User Guide and was successful in booting.&lt;/P&gt;&lt;P&gt;Some dtb related issue it seems. Will try TFTP boot later.&lt;/P&gt;&lt;P&gt;Marking this as assumend answered.&lt;/P&gt;&lt;P&gt;Sorry I didn't update the issue earlier.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Boot parameters saved on the new SD card.&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; printenv&lt;/P&gt;&lt;P&gt;baudrate=115200&lt;/P&gt;&lt;P&gt;boot_fdt=try&lt;/P&gt;&lt;P&gt;bootargs_base=setenv bootargs console=ttymxc0,115200&lt;/P&gt;&lt;P&gt;bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24&lt;/P&gt;&lt;P&gt;bootcmd=run bootcmd_mmc&lt;/P&gt;&lt;P&gt;bootcmd_mfg=run mfgtool_args;bootm ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;/P&gt;&lt;P&gt;bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 1;mmc read ${loadaddr} 0x800 0x4000;mmc read ${fdt_addr} 0x5000 0x800;bootm ${loadaddr} - ${fdt_addr}&lt;/P&gt;&lt;P&gt;bootdelay=1&lt;/P&gt;&lt;P&gt;bootscript=echo Running bootscript from mmc ...; source&lt;/P&gt;&lt;P&gt;console=ttymxc0&lt;/P&gt;&lt;P&gt;ethact=FEC&lt;/P&gt;&lt;P&gt;ethaddr=00:04:9f:02:df:ac&lt;/P&gt;&lt;P&gt;ethprime=FEC&lt;/P&gt;&lt;P&gt;fdt_addr=0x18000000&lt;/P&gt;&lt;P&gt;fdt_file=imx6q-sabresd.dtb&lt;/P&gt;&lt;P&gt;fdt_high=0xffffffff&lt;/P&gt;&lt;P&gt;initrd_addr=0x12C00000&lt;/P&gt;&lt;P&gt;initrd_high=0xffffffff&lt;/P&gt;&lt;P&gt;ip_dyn=yes&lt;/P&gt;&lt;P&gt;loadaddr=0x12000000&lt;/P&gt;&lt;P&gt;loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};&lt;/P&gt;&lt;P&gt;loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}&lt;/P&gt;&lt;P&gt;loaduimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${uimage}&lt;/P&gt;&lt;P&gt;mfgtool_args=setenv bootargs console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x&lt;/P&gt;&lt;P&gt;37FF g_mass_storage.iSerialNumber="" enable_wait_mode=off &lt;/P&gt;&lt;P&gt;mmcargs=setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot}&lt;/P&gt;&lt;P&gt;mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootm ${loadaddr} - ${fdt_addr}; else if test ${b&lt;/P&gt;&lt;P&gt;oot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;&lt;/P&gt;&lt;P&gt;mmcdev=1&lt;/P&gt;&lt;P&gt;mmcpart=1&lt;/P&gt;&lt;P&gt;mmcroot=/dev/mmcblk0p2 rootwait rw&lt;/P&gt;&lt;P&gt;netargs=setenv bootargs console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp&lt;/P&gt;&lt;P&gt;netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${uimage}; if test ${boot_fdt} = yes&lt;/P&gt;&lt;P&gt; || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot&lt;/P&gt;&lt;P&gt; load the DT; fi; fi; else bootm; fi;&lt;/P&gt;&lt;P&gt;script=boot.scr&lt;/P&gt;&lt;P&gt;uimage=uImage&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Environment size: 2211/8188 bytes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Oct 2014 06:35:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bootup-with-yocto-build-image-getting-stuck/m-p/330286#M44571</guid>
      <dc:creator>subodh</dc:creator>
      <dc:date>2014-10-21T06:35:23Z</dc:date>
    </item>
    <item>
      <title>Re: Bootup with yocto build image getting stuck</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bootup-with-yocto-build-image-getting-stuck/m-p/330287#M44572</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Subodh C,&lt;/P&gt;&lt;P&gt;It's great you have boot up the board from SD card. If you have solved the question, would you please help us close the thread by click the Correct Answer button or Helpful Answer button?&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;&lt;P&gt;If any other questions contact us easily.&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Oct 2014 08:58:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bootup-with-yocto-build-image-getting-stuck/m-p/330287#M44572</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2014-10-21T08:58:36Z</dc:date>
    </item>
  </channel>
</rss>