<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: DAI SSI as capture from an external source</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DAI-SSI-as-capture-from-an-external-source/m-p/330050#M44515</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Cristian &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;both options are possibel since AUDMUX can change TX and RX by bit&lt;/P&gt;&lt;P&gt;TXRXEN, 0 No switch (Transmit Pin = Transmit, Receive Pin = Receive)&lt;/P&gt;&lt;P&gt;1 Switch (Transmit Pin = Receive, Receive Pin = Transmit)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Jan 2015 09:18:56 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-01-29T09:18:56Z</dc:date>
    <item>
      <title>DAI SSI as capture from an external source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DAI-SSI-as-capture-from-an-external-source/m-p/330049#M44514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear *,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a schematic like this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49727iC6CF09CF481AE0D2/image-size/large?v=v2&amp;amp;px=999" title="gpt_schematic_AUD4.png" alt="gpt_schematic_AUD4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I know that the MODEM_SSI_TXD provide the data output to a DAC, now I would like capture this data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is right the configuration of AUD4_TXD to MODEM_SSI_TXD?&lt;/P&gt;&lt;P&gt;Or the right configuration is AUD4_RXD to MODEM_SSI_TXD?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Cristian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jan 2015 08:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DAI-SSI-as-capture-from-an-external-source/m-p/330049#M44514</guid>
      <dc:creator>cristiansicilia</dc:creator>
      <dc:date>2015-01-29T08:17:38Z</dc:date>
    </item>
    <item>
      <title>Re: DAI SSI as capture from an external source</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DAI-SSI-as-capture-from-an-external-source/m-p/330050#M44515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Cristian &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;both options are possibel since AUDMUX can change TX and RX by bit&lt;/P&gt;&lt;P&gt;TXRXEN, 0 No switch (Transmit Pin = Transmit, Receive Pin = Receive)&lt;/P&gt;&lt;P&gt;1 Switch (Transmit Pin = Receive, Receive Pin = Transmit)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jan 2015 09:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DAI-SSI-as-capture-from-an-external-source/m-p/330050#M44515</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-29T09:18:56Z</dc:date>
    </item>
  </channel>
</rss>