<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: dhcp</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/dhcp/m-p/329285#M44328</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Niklas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please describe the network scenario where you are trying to connect the board?, Are you using a Router or Switch to provide the IP address or it is a server? do you have any segmentation&amp;nbsp; or any other filter that not allow to have the DHCP request that not came into the network?.&amp;nbsp; Do you set the MAC Address of the boarD?&amp;nbsp; If you set the IP static address always works?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The BSP does not have something like the dhclient.conf, but it can be done usign the same packages that contains ubuntu. But this need to be done at Uboot.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Aug 2014 15:04:24 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2014-08-06T15:04:24Z</dc:date>
    <item>
      <title>dhcp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/dhcp/m-p/329284#M44327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to configure dhcp on i.MX6 (built in Yocto).&lt;/P&gt;&lt;P&gt;It seems like if I have interface set to DHCP and there is no network connection, it tries a few times, but then stops.&lt;/P&gt;&lt;P&gt;Is there a way to configure this to continue to try or to have a fallback static address, like there is in Ubuntu (dhclient.conf using static leases if there is a timeout)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jul 2014 22:06:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/dhcp/m-p/329284#M44327</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2014-07-31T22:06:18Z</dc:date>
    </item>
    <item>
      <title>Re: dhcp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/dhcp/m-p/329285#M44328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Niklas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please describe the network scenario where you are trying to connect the board?, Are you using a Router or Switch to provide the IP address or it is a server? do you have any segmentation&amp;nbsp; or any other filter that not allow to have the DHCP request that not came into the network?.&amp;nbsp; Do you set the MAC Address of the boarD?&amp;nbsp; If you set the IP static address always works?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The BSP does not have something like the dhclient.conf, but it can be done usign the same packages that contains ubuntu. But this need to be done at Uboot.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jaime&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Aug 2014 15:04:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/dhcp/m-p/329285#M44328</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2014-08-06T15:04:24Z</dc:date>
    </item>
  </channel>
</rss>