<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX23 SPI USER MODE</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX23-SPI-USER-MODE/m-p/165843#M4427</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It should appear. If not, check if the driver's platform data is defined in the board configuration file for the imx23.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Balaji.V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Jun 2012 09:04:06 GMT</pubDate>
    <dc:creator>Balaji_ng</dc:creator>
    <dc:date>2012-06-14T09:04:06Z</dc:date>
    <item>
      <title>iMX23 SPI USER MODE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX23-SPI-USER-MODE/m-p/165842#M4426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I'm trying to use SPI from user space. I have already configured the kernel:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;*&amp;gt; User mode SPI device driver support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I can't see /dev/spidev. Am I missing something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jun 2012 14:58:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX23-SPI-USER-MODE/m-p/165842#M4426</guid>
      <dc:creator>AndracsEstacvez</dc:creator>
      <dc:date>2012-06-04T14:58:51Z</dc:date>
    </item>
    <item>
      <title>Re: iMX23 SPI USER MODE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX23-SPI-USER-MODE/m-p/165843#M4427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It should appear. If not, check if the driver's platform data is defined in the board configuration file for the imx23.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Balaji.V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jun 2012 09:04:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX23-SPI-USER-MODE/m-p/165843#M4427</guid>
      <dc:creator>Balaji_ng</dc:creator>
      <dc:date>2012-06-14T09:04:06Z</dc:date>
    </item>
    <item>
      <title>Re: iMX23 SPI USER MODE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX23-SPI-USER-MODE/m-p/165844#M4428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Balaji,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for your reply. I think that there are some problem because SPI is being used by ethernet. Should it be?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Apart from that, I have another problem: I don't have the commands flash_eraseall, ubiattach and ubimkvol. I don't know why. However, I have kobs-ng&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jun 2012 09:50:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX23-SPI-USER-MODE/m-p/165844#M4428</guid>
      <dc:creator>AndracsEstacvez</dc:creator>
      <dc:date>2012-06-14T09:50:44Z</dc:date>
    </item>
    <item>
      <title>Re: iMX23 SPI USER MODE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX23-SPI-USER-MODE/m-p/165845#M4429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Answers inline.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;I think that there are some problem because SPI is being used by ethernet. Should it be?&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;If your target hardware is imx23 evk, you may try loading enc28j60 as module. If you are using spidev, do not load enc28j60.ko module, if you think that is an issue.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Apart from that, I have another problem: I don't have the commands flash_eraseall, ubiattach and ubimkvol. I don't know why. However, I have kobs-ng&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I think these are available with mtd-utils package. Try enabling mtd-utils package in ltib configuration. You could refer the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://processors.wiki.ti.com/index.php/MTD_Utilities#MTD-Utils_User-space_tools" target="_blank"&gt;http://processors.wiki.ti.com/index.php/MTD_Utilities#MTD-Utils_User-space_tools&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Balaji&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jun 2012 03:15:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX23-SPI-USER-MODE/m-p/165845#M4429</guid>
      <dc:creator>Balaji_ng</dc:creator>
      <dc:date>2012-06-15T03:15:59Z</dc:date>
    </item>
  </channel>
</rss>