<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: PCIe host controller driver in 3.10.17 kernel</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-host-controller-driver-in-3-10-17-kernel/m-p/328178#M44179</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Krishnan P,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you enable RC or EP option in the kernel configuration when build the kernel image?&lt;/P&gt;&lt;P&gt;These two options are only used in imx6 pcie ep/rc validation system, please disable them if they are enabled in your kernel configuration.&lt;BR /&gt;Otherwise, imx6 pcie wouldn't work properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;based on the 3.10.17 and imx6dl sd, intel iwl633agn wifi card.&lt;/P&gt;&lt;P&gt;Here is the log.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Booting Linux on physical CPU 0x0&lt;/P&gt;&lt;P&gt;Linux version 3.10.17-01767-g97f757e (r65037@shlinux1) (gcc version 4.8.1 (GCC) ) #205 SMP PREEMPT Wed Aug 6 13:25:41 CST 2014&lt;/P&gt;&lt;P&gt;CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d&lt;/P&gt;&lt;P&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;/P&gt;&lt;P&gt;Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 DualLite SABRE Smart Device Board(PFUZE100)&lt;/P&gt;&lt;P&gt;cma: CMA: reserved 320 MiB at 2c000000&lt;/P&gt;&lt;P&gt;Memory policy: ECC disabled, Data cache writealloc&lt;/P&gt;&lt;P&gt;PERCPU: Embedded 8 pages/cpu @813d3000 s8896 r8192 d15680 u32768&lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 195072&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;MIPI CSI2 driver module loaded&lt;/P&gt;&lt;P&gt;Advanced Linux Sound Architecture Driver Initialized.&lt;/P&gt;&lt;P&gt;cfg80211: Calling CRDA to update world regulatory domain&lt;/P&gt;&lt;P&gt;pureg-dummy: no parameters&lt;/P&gt;&lt;P&gt;Switching to clocksource mxc_timer1&lt;/P&gt;&lt;P&gt;PCI host bridge to bus 0000:00&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [io&amp;nbsp; 0x1000-0x10000]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]&lt;/P&gt;&lt;P&gt;PCI: bus0: Fast back to back transfers disabled&lt;/P&gt;&lt;P&gt;PCI: bus1: Fast back to back transfers disabled&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 8: assigned [mem 0x01100000-0x011fffff]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 6: assigned [mem 0x01200000-0x0120ffff pref]&lt;/P&gt;&lt;P&gt;pci 0000:01:00.0: BAR 0: assigned [mem 0x01100000-0x01101fff 64bit]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PCI bridge to [bus 01]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0:&amp;nbsp; bridge window [mem 0x01100000-0x011fffff]&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 2&lt;/P&gt;&lt;P&gt;TCP established hash table entries: 8192 (order: 4, 65536 bytes)&lt;/P&gt;&lt;P&gt;TCP bind hash table entries: 8192 (order: 4, 65536 bytes)&lt;/P&gt;&lt;P&gt;TCP: Hash tables configured (established 8192 bind 8192)&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;udevd[196]: starting version 182&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: loaded firmware version 9.221.4.1 build 25532 op_mode iwldvm&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: CONFIG_IWLWIFI_DEBUG disabled&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: CONFIG_IWLWIFI_DEBUGFS disabled&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: CONFIG_IWLWIFI_DEVICE_TRACING disabled&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: CONFIG_IWLWIFI_DEVICE_TESTMODE disabled&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: CONFIG_IWLWIFI_P2P enabled&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: Detected Intel(R) Centrino(R) Ultimate-N 6300 AGN, REV=0x74&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: L1 Disabled; Enabling L0S&lt;/P&gt;&lt;P&gt;EXT2-fs (mmcblk0p1): warning: mounting unchecked fs, running e2fsck is recommended&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6qdlsolo:~# lspci&lt;/P&gt;&lt;P&gt;00:00.0 PCI bridge: Device 16c3:abcd (rev 01)&lt;/P&gt;&lt;P&gt;01:00.0 Network controller: Intel Corporation Centrino Ultimate-N 6300 (rev 35)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Aug 2014 17:49:02 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2014-08-06T17:49:02Z</dc:date>
    <item>
      <title>PCIe host controller driver in 3.10.17 kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-host-controller-driver-in-3-10-17-kernel/m-p/328176#M44177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to bring up a PCIe based wireless card on i.MX6 custom board. The card has been verified&amp;nbsp; with 3.10.9 kernel&amp;nbsp; using the same board.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Looks like PCIe host driver got additional features&amp;nbsp; like RC mode EP mode in this&amp;nbsp; 3.10.17 kernel.&amp;nbsp; I can see the wi-fi card is getting detected. But the firmware download fails.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;root@imx6qsabrelite:~# lspci &lt;/P&gt;&lt;P&gt;00:00.0 PCI bridge: Device 16c3:abcd (rev 01)&lt;/P&gt;&lt;P&gt;01:00.0 Ethernet controller: Marvell Technology Group Ltd. Device 2b38&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have attached the console logs.&amp;nbsp; Your suggestions are welcome.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336171"&gt;3.10.17_pcie_console_log.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jul 2014 13:31:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-host-controller-driver-in-3-10-17-kernel/m-p/328176#M44177</guid>
      <dc:creator>krishnanp</dc:creator>
      <dc:date>2014-07-31T13:31:18Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe host controller driver in 3.10.17 kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-host-controller-driver-in-3-10-17-kernel/m-p/328177#M44178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Krishnan P,&lt;/P&gt;&lt;P&gt;We are reviewing your request internally, you will get a response soon.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Aug 2014 17:33:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-host-controller-driver-in-3-10-17-kernel/m-p/328177#M44178</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2014-08-05T17:33:49Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe host controller driver in 3.10.17 kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-host-controller-driver-in-3-10-17-kernel/m-p/328178#M44179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Krishnan P,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you enable RC or EP option in the kernel configuration when build the kernel image?&lt;/P&gt;&lt;P&gt;These two options are only used in imx6 pcie ep/rc validation system, please disable them if they are enabled in your kernel configuration.&lt;BR /&gt;Otherwise, imx6 pcie wouldn't work properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;based on the 3.10.17 and imx6dl sd, intel iwl633agn wifi card.&lt;/P&gt;&lt;P&gt;Here is the log.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Booting Linux on physical CPU 0x0&lt;/P&gt;&lt;P&gt;Linux version 3.10.17-01767-g97f757e (r65037@shlinux1) (gcc version 4.8.1 (GCC) ) #205 SMP PREEMPT Wed Aug 6 13:25:41 CST 2014&lt;/P&gt;&lt;P&gt;CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d&lt;/P&gt;&lt;P&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;/P&gt;&lt;P&gt;Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 DualLite SABRE Smart Device Board(PFUZE100)&lt;/P&gt;&lt;P&gt;cma: CMA: reserved 320 MiB at 2c000000&lt;/P&gt;&lt;P&gt;Memory policy: ECC disabled, Data cache writealloc&lt;/P&gt;&lt;P&gt;PERCPU: Embedded 8 pages/cpu @813d3000 s8896 r8192 d15680 u32768&lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 195072&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;MIPI CSI2 driver module loaded&lt;/P&gt;&lt;P&gt;Advanced Linux Sound Architecture Driver Initialized.&lt;/P&gt;&lt;P&gt;cfg80211: Calling CRDA to update world regulatory domain&lt;/P&gt;&lt;P&gt;pureg-dummy: no parameters&lt;/P&gt;&lt;P&gt;Switching to clocksource mxc_timer1&lt;/P&gt;&lt;P&gt;PCI host bridge to bus 0000:00&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [io&amp;nbsp; 0x1000-0x10000]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]&lt;/P&gt;&lt;P&gt;PCI: bus0: Fast back to back transfers disabled&lt;/P&gt;&lt;P&gt;PCI: bus1: Fast back to back transfers disabled&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 8: assigned [mem 0x01100000-0x011fffff]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 6: assigned [mem 0x01200000-0x0120ffff pref]&lt;/P&gt;&lt;P&gt;pci 0000:01:00.0: BAR 0: assigned [mem 0x01100000-0x01101fff 64bit]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PCI bridge to [bus 01]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0:&amp;nbsp; bridge window [mem 0x01100000-0x011fffff]&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 2&lt;/P&gt;&lt;P&gt;TCP established hash table entries: 8192 (order: 4, 65536 bytes)&lt;/P&gt;&lt;P&gt;TCP bind hash table entries: 8192 (order: 4, 65536 bytes)&lt;/P&gt;&lt;P&gt;TCP: Hash tables configured (established 8192 bind 8192)&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;udevd[196]: starting version 182&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: loaded firmware version 9.221.4.1 build 25532 op_mode iwldvm&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: CONFIG_IWLWIFI_DEBUG disabled&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: CONFIG_IWLWIFI_DEBUGFS disabled&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: CONFIG_IWLWIFI_DEVICE_TRACING disabled&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: CONFIG_IWLWIFI_DEVICE_TESTMODE disabled&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: CONFIG_IWLWIFI_P2P enabled&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: Detected Intel(R) Centrino(R) Ultimate-N 6300 AGN, REV=0x74&lt;/P&gt;&lt;P&gt;iwlwifi 0000:01:00.0: L1 Disabled; Enabling L0S&lt;/P&gt;&lt;P&gt;EXT2-fs (mmcblk0p1): warning: mounting unchecked fs, running e2fsck is recommended&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx6qdlsolo:~# lspci&lt;/P&gt;&lt;P&gt;00:00.0 PCI bridge: Device 16c3:abcd (rev 01)&lt;/P&gt;&lt;P&gt;01:00.0 Network controller: Intel Corporation Centrino Ultimate-N 6300 (rev 35)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Aug 2014 17:49:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-host-controller-driver-in-3-10-17-kernel/m-p/328178#M44179</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2014-08-06T17:49:02Z</dc:date>
    </item>
    <item>
      <title>Re: Re: PCIe host controller driver in 3.10.17 kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-host-controller-driver-in-3-10-17-kernel/m-p/328179#M44180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class="font-color-meta" style="padding: 0 0 5px; font-size: 1.2em; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #8b8b8b; background-color: #e6e6e6;"&gt;&lt;SPAN class="replyToName" style="font-weight: inherit; font-style: inherit; font-size: 15.5999994277954px; font-family: inherit;"&gt;CarlosCasillas,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even I am facing same problem with kernel 3.10.53. My boot-up stops here:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting udev&lt;/P&gt;&lt;P&gt;udevd[199]: starting version 182&lt;/P&gt;&lt;P&gt;iwl4965 0000:01:00.0: request for firmware file 'iwlwifi-4965-2.ucode' failed.&lt;/P&gt;&lt;P&gt;iwl4965 0000:01:00.0: no suitable firmware found!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 13px;"&gt; imx6 pcie ep/rc&amp;nbsp; are disabled&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached please find my config file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Mar 2015 15:08:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-host-controller-driver-in-3-10-17-kernel/m-p/328179#M44180</guid>
      <dc:creator>faisaltaj</dc:creator>
      <dc:date>2015-03-27T15:08:25Z</dc:date>
    </item>
  </channel>
</rss>