<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6Q android BSP API for multiple network.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-android-BSP-API-for-multiple-network/m-p/327380#M44053</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, it's not exactly so. First, the Android OS itself has many various APIs to manage network connections, please refer to the following Android Developer site links:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://developer.android.com/reference/java/net/package-summary.html"&gt;http://developer.android.com/reference/java/net/package-summary.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://developer.android.com/reference/android/net/package-summary.html"&gt;http://developer.android.com/reference/android/net/package-summary.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Second, in the Android BSP by Freescale, you can access the system console through the following API:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://developer.android.com/reference/java/io/Console.html"&gt;http://developer.android.com/reference/java/io/Console.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then, on the console, you can use regular Linux network management utilities, such as 'ifconfig'.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Dec 2014 10:21:39 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2014-12-10T10:21:39Z</dc:date>
    <item>
      <title>i.MX6Q android BSP API for multiple network.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-android-BSP-API-for-multiple-network/m-p/327379#M44052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to confirm my understanding about i.MX6Q android BSP.&lt;/P&gt;&lt;P&gt;I understand android can use wired LAN and wireless LAN simultaneously.&lt;/P&gt;&lt;P&gt;However, user (or a application) cannot select which network use for a specific process because android API does not support it.&lt;/P&gt;&lt;P&gt;(e.g. wired LAN for process A, and wireless LAN for process B)&lt;/P&gt;&lt;P&gt;And I think freescale does not customize about this API, so if user want to select the network to use for specific process, user should customize the android API by themselves.&lt;/P&gt;&lt;P&gt;Is this correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Dec 2014 08:31:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-android-BSP-API-for-multiple-network/m-p/327379#M44052</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-12-05T08:31:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q android BSP API for multiple network.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-android-BSP-API-for-multiple-network/m-p/327380#M44053</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, it's not exactly so. First, the Android OS itself has many various APIs to manage network connections, please refer to the following Android Developer site links:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://developer.android.com/reference/java/net/package-summary.html"&gt;http://developer.android.com/reference/java/net/package-summary.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://developer.android.com/reference/android/net/package-summary.html"&gt;http://developer.android.com/reference/android/net/package-summary.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Second, in the Android BSP by Freescale, you can access the system console through the following API:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://developer.android.com/reference/java/io/Console.html"&gt;http://developer.android.com/reference/java/io/Console.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then, on the console, you can use regular Linux network management utilities, such as 'ifconfig'.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Dec 2014 10:21:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-android-BSP-API-for-multiple-network/m-p/327380#M44053</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2014-12-10T10:21:39Z</dc:date>
    </item>
  </channel>
</rss>