<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: u-boot otp</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-otp/m-p/327311#M44038</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you use the latest boot you can activate the fuse API by adding the following options in your config file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define CONFIG_CMD_FUSE&lt;/P&gt;&lt;P&gt;#ifdef CONFIG_CMD_FUSE&lt;/P&gt;&lt;P&gt;#define CONFIG_MXC_OCOTP&lt;/P&gt;&lt;P&gt;#endif&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can look at mx6sabre_common.h as reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These following docs are also helpful to understand how the fuse api works:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;doc/README.mxc_ocotp&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;doc/README.imx6&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 30 Aug 2014 12:27:28 GMT</pubDate>
    <dc:creator>fabio_estevam</dc:creator>
    <dc:date>2014-08-30T12:27:28Z</dc:date>
    <item>
      <title>u-boot otp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-otp/m-p/327310#M44037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running the u-boot generated from the Yocto project (2014).&lt;/P&gt;&lt;P&gt;I'm trying to see what values the OTPs have (check the speed grade etc.) and I saw a another post that mentioned imxotp command.&lt;/P&gt;&lt;P&gt;But it seems like it's not in this u-boot version.&lt;/P&gt;&lt;P&gt;Is there a config settings (when compiling) I need to do to enable this or is there another way in this u-boot version?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Aug 2014 16:16:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-otp/m-p/327310#M44037</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2014-08-29T16:16:55Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot otp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-otp/m-p/327311#M44038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you use the latest boot you can activate the fuse API by adding the following options in your config file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define CONFIG_CMD_FUSE&lt;/P&gt;&lt;P&gt;#ifdef CONFIG_CMD_FUSE&lt;/P&gt;&lt;P&gt;#define CONFIG_MXC_OCOTP&lt;/P&gt;&lt;P&gt;#endif&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can look at mx6sabre_common.h as reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These following docs are also helpful to understand how the fuse api works:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;doc/README.mxc_ocotp&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;doc/README.imx6&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Aug 2014 12:27:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-otp/m-p/327311#M44038</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2014-08-30T12:27:28Z</dc:date>
    </item>
  </channel>
</rss>