<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Difference between pf0100 and pf0200 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-pf0100-and-pf0200/m-p/326374#M43843</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JHY&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MMPF0200 is MMPF0100 (pin compatible) minus SW1C and SW4, SW2=1.5A.&lt;/P&gt;&lt;P&gt;Since SW1C is absent in the PF0200, both VDDCORE and VDDSOC&lt;/P&gt;&lt;P&gt;are powered by the SW1AB regulator. Peripherals connected to the SW4&lt;/P&gt;&lt;P&gt;regulator in the original reference design can be powered by the SW2 regulator&lt;/P&gt;&lt;P&gt;when using the PF0200.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Jan 2015 09:06:55 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-01-28T09:06:55Z</dc:date>
    <item>
      <title>Difference between pf0100 and pf0200</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-pf0100-and-pf0200/m-p/326373#M43842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to replace pf0100 with pf0200 in i.MX6DL boards.&lt;/P&gt;&lt;P&gt;Are they pin-to-pin compatible or need another work for PCB?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jan 2015 08:07:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-pf0100-and-pf0200/m-p/326373#M43842</guid>
      <dc:creator>JHY</dc:creator>
      <dc:date>2015-01-28T08:07:45Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between pf0100 and pf0200</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-pf0100-and-pf0200/m-p/326374#M43843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JHY&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MMPF0200 is MMPF0100 (pin compatible) minus SW1C and SW4, SW2=1.5A.&lt;/P&gt;&lt;P&gt;Since SW1C is absent in the PF0200, both VDDCORE and VDDSOC&lt;/P&gt;&lt;P&gt;are powered by the SW1AB regulator. Peripherals connected to the SW4&lt;/P&gt;&lt;P&gt;regulator in the original reference design can be powered by the SW2 regulator&lt;/P&gt;&lt;P&gt;when using the PF0200.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jan 2015 09:06:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-pf0100-and-pf0200/m-p/326374#M43843</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-01-28T09:06:55Z</dc:date>
    </item>
  </channel>
</rss>