<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX53 MACRO for eboot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-MACRO-for-eboot/m-p/326078#M43802</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi cheng&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;frankly speaking I am not aware of such macros.&lt;/P&gt;&lt;P&gt;In general NAND algorithms (and BBT in particular) are quite complex&lt;/P&gt;&lt;P&gt;to be implemeneted as macros.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Jul 2014 13:49:35 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-07-31T13:49:35Z</dc:date>
    <item>
      <title>i.MX53 MACRO for eboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-MACRO-for-eboot/m-p/326077#M43801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'm developing a wince7 BSP on an i.MX53 board, my board is boot from nand flash, so the nand driver would be used by both eboot and OS, but now I have some code in nand driver should be used only in eboot, so I want to use some macro to make those code out of build when I building the OS, are there any macros could distinguish which program is building(eboot or OS)? Or are there any macro &amp;amp; environment only available in eboot/OS?&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Thank you very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jul 2014 10:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-MACRO-for-eboot/m-p/326077#M43801</guid>
      <dc:creator>chengwu</dc:creator>
      <dc:date>2014-07-30T10:22:37Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 MACRO for eboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-MACRO-for-eboot/m-p/326078#M43802</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi cheng&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;frankly speaking I am not aware of such macros.&lt;/P&gt;&lt;P&gt;In general NAND algorithms (and BBT in particular) are quite complex&lt;/P&gt;&lt;P&gt;to be implemeneted as macros.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jul 2014 13:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-MACRO-for-eboot/m-p/326078#M43802</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-31T13:49:35Z</dc:date>
    </item>
  </channel>
</rss>