<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Graphic accelerated browsing on IMX6 using QWebkit in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Graphic-accelerated-browsing-on-IMX6-using-QWebkit/m-p/325833#M43761</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Communitiy,&lt;/P&gt;&lt;P&gt;I tried to build an graphic accelerated browser on a Wayland rootfs based on the Yocto (daisy) release.&lt;/P&gt;&lt;P&gt;I currently have a working rootfs with Wayland(weston compositor), Qt, Qtwayland plugin and Qwebkit integrated. I created a small QwebView browser which is working successfully with HTML5 and Javascript content but doesn't using hardware acceleration.&lt;/P&gt;&lt;P&gt;It is possible to create OpenGL application with QML and the wayland-egl plugin and also QWidget based applications so that it is sure that OpenGL support is available for Wayland.&lt;/P&gt;&lt;P&gt;Using a QGraphicsWebView or a accelerated QML WebView doesn't work. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have expieriences using hardware accelerated browsing with th IMX6 using QWebkit? I'm using the Nitrogen6x board from BoundaryDevices&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Regards Christian Eissler&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Jul 2014 07:29:57 GMT</pubDate>
    <dc:creator>christianeissle</dc:creator>
    <dc:date>2014-07-29T07:29:57Z</dc:date>
    <item>
      <title>Graphic accelerated browsing on IMX6 using QWebkit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Graphic-accelerated-browsing-on-IMX6-using-QWebkit/m-p/325833#M43761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Communitiy,&lt;/P&gt;&lt;P&gt;I tried to build an graphic accelerated browser on a Wayland rootfs based on the Yocto (daisy) release.&lt;/P&gt;&lt;P&gt;I currently have a working rootfs with Wayland(weston compositor), Qt, Qtwayland plugin and Qwebkit integrated. I created a small QwebView browser which is working successfully with HTML5 and Javascript content but doesn't using hardware acceleration.&lt;/P&gt;&lt;P&gt;It is possible to create OpenGL application with QML and the wayland-egl plugin and also QWidget based applications so that it is sure that OpenGL support is available for Wayland.&lt;/P&gt;&lt;P&gt;Using a QGraphicsWebView or a accelerated QML WebView doesn't work. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have expieriences using hardware accelerated browsing with th IMX6 using QWebkit? I'm using the Nitrogen6x board from BoundaryDevices&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Regards Christian Eissler&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jul 2014 07:29:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Graphic-accelerated-browsing-on-IMX6-using-QWebkit/m-p/325833#M43761</guid>
      <dc:creator>christianeissle</dc:creator>
      <dc:date>2014-07-29T07:29:57Z</dc:date>
    </item>
  </channel>
</rss>