<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックError in code generated by IOMUX tool for iMX6SDL using USDHC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-code-generated-by-IOMUX-tool-for-iMX6SDL-using-USDHC/m-p/325132#M43635</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was trying to generate pin-muxing code for a custom board capable to use both iMX6DQ and iMX6SDL CPU flavors.&lt;/P&gt;&lt;P&gt;I had no problems building the code for iMX6DQ, but got a few undefined symbols when trying to compile for iMX6SDL, namely:&lt;/P&gt;&lt;P&gt;HW_IOMUXC_USDHC1_CARD_CLK_IN_SELECT_INPUT_WR&lt;/P&gt;&lt;P&gt;HW_IOMUXC_USDHC2_CARD_CLK_IN_SELECT_INPUT_WR&lt;/P&gt;&lt;P&gt;HW_IOMUXC_USDHC4_CARD_CLK_IN_SELECT_INPUT_WR&lt;/P&gt;&lt;P&gt;(this happen because I am only using USDHC interfaces 1, 2 and 4)&lt;/P&gt;&lt;P&gt;These symbols are not defined in the headers generated, however the register is listed in the iMX6SDL manual, with just one valid setting (the other is reserved), which is not the default, so it seems that setting it would be required. Interestingly, these registers aren't there in the iMX6DQ manual. Actually, I was a bit surprised to find a daisy-chain setting for SD clock signals that are output-only,&lt;/P&gt;&lt;P&gt;So, one of the following must be true:&lt;/P&gt;&lt;P&gt;1. Setting these registers is not required, then the lines of code referencing them shouldn't have been generated, nor should the input selection be available in the relevant "registers" page&lt;/P&gt;&lt;P&gt;2. Setting these registers is required, then the relevant definitions should be present in the generated headers&lt;/P&gt;&lt;P&gt;In either case, this is a bug to be fixed in the IOMUX tool. I think it may be rather simple to fix, and was wondering why isn't it possible to access the source code, so that users may submit patches themselves when they find a bug or create an enhancement (I have some in mind that could make the tool more powerful and easier to use...).&lt;/P&gt;&lt;P&gt;For now, I chose option 1 and commented out the extra lines in order to compile the code. Please tell me if I'm wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Jul 2014 18:55:12 GMT</pubDate>
    <dc:creator>marcocontenti</dc:creator>
    <dc:date>2014-07-25T18:55:12Z</dc:date>
    <item>
      <title>Error in code generated by IOMUX tool for iMX6SDL using USDHC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-code-generated-by-IOMUX-tool-for-iMX6SDL-using-USDHC/m-p/325132#M43635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was trying to generate pin-muxing code for a custom board capable to use both iMX6DQ and iMX6SDL CPU flavors.&lt;/P&gt;&lt;P&gt;I had no problems building the code for iMX6DQ, but got a few undefined symbols when trying to compile for iMX6SDL, namely:&lt;/P&gt;&lt;P&gt;HW_IOMUXC_USDHC1_CARD_CLK_IN_SELECT_INPUT_WR&lt;/P&gt;&lt;P&gt;HW_IOMUXC_USDHC2_CARD_CLK_IN_SELECT_INPUT_WR&lt;/P&gt;&lt;P&gt;HW_IOMUXC_USDHC4_CARD_CLK_IN_SELECT_INPUT_WR&lt;/P&gt;&lt;P&gt;(this happen because I am only using USDHC interfaces 1, 2 and 4)&lt;/P&gt;&lt;P&gt;These symbols are not defined in the headers generated, however the register is listed in the iMX6SDL manual, with just one valid setting (the other is reserved), which is not the default, so it seems that setting it would be required. Interestingly, these registers aren't there in the iMX6DQ manual. Actually, I was a bit surprised to find a daisy-chain setting for SD clock signals that are output-only,&lt;/P&gt;&lt;P&gt;So, one of the following must be true:&lt;/P&gt;&lt;P&gt;1. Setting these registers is not required, then the lines of code referencing them shouldn't have been generated, nor should the input selection be available in the relevant "registers" page&lt;/P&gt;&lt;P&gt;2. Setting these registers is required, then the relevant definitions should be present in the generated headers&lt;/P&gt;&lt;P&gt;In either case, this is a bug to be fixed in the IOMUX tool. I think it may be rather simple to fix, and was wondering why isn't it possible to access the source code, so that users may submit patches themselves when they find a bug or create an enhancement (I have some in mind that could make the tool more powerful and easier to use...).&lt;/P&gt;&lt;P&gt;For now, I chose option 1 and commented out the extra lines in order to compile the code. Please tell me if I'm wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jul 2014 18:55:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-code-generated-by-IOMUX-tool-for-iMX6SDL-using-USDHC/m-p/325132#M43635</guid>
      <dc:creator>marcocontenti</dc:creator>
      <dc:date>2014-07-25T18:55:12Z</dc:date>
    </item>
    <item>
      <title>Re: Error in code generated by IOMUX tool for iMX6SDL using USDHC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-code-generated-by-IOMUX-tool-for-iMX6SDL-using-USDHC/m-p/325133#M43636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which BSP are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jul 2014 06:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-code-generated-by-IOMUX-tool-for-iMX6SDL-using-USDHC/m-p/325133#M43636</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2014-07-30T06:27:29Z</dc:date>
    </item>
    <item>
      <title>Re: Error in code generated by IOMUX tool for iMX6SDL using USDHC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-code-generated-by-IOMUX-tool-for-iMX6SDL-using-USDHC/m-p/325134#M43637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem does not depend on the BSP or OS used, you can even run the Platform SDK on bare metal.&lt;/P&gt;&lt;P&gt;All the symbols needed to compile the files generated should be in the header files in the sdk\include\mx6sdl\registers folder, also generated by the tool, but these symols are missing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jul 2014 13:05:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-code-generated-by-IOMUX-tool-for-iMX6SDL-using-USDHC/m-p/325134#M43637</guid>
      <dc:creator>marcocontenti</dc:creator>
      <dc:date>2014-07-30T13:05:58Z</dc:date>
    </item>
    <item>
      <title>Re: Error in code generated by IOMUX tool for iMX6SDL using USDHC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-code-generated-by-IOMUX-tool-for-iMX6SDL-using-USDHC/m-p/325135#M43638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm sort of answering myself. At least I have found a workaround. Just when checking the iMX6 Platform SDK (v.1.1.0) source tree, which contains IOMUX generated files for some evaluation platforms, I realized that the regsiomuxc.h file in there is different and contains the missing declarations, so replacing the file generated by IOMUX with that from the Platform SDK solves the problem. Obviously, this still ought to be fixed on IOMUX.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FINAL ANSWER: I was actually using IOMUX version 3.4.0.3, which is still available for download from the Freescale website as stand-alone. The latest version 3.4.0.4 fixes the issue. IOMUX version 3.4.0.4 is contained in the iMX6 Platform SDK (I didn't check if it's in any other package as well), but if you look for IOMUX itself you will find an outdated version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jul 2014 13:19:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-code-generated-by-IOMUX-tool-for-iMX6SDL-using-USDHC/m-p/325135#M43638</guid>
      <dc:creator>marcocontenti</dc:creator>
      <dc:date>2014-07-30T13:19:50Z</dc:date>
    </item>
    <item>
      <title>Re: Error in code generated by IOMUX tool for iMX6SDL using USDHC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-code-generated-by-IOMUX-tool-for-iMX6SDL-using-USDHC/m-p/325136#M43639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In Linux BSP, all the iomux setting of pins are defined in arch&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;/arm/plat-mxc/include/mach/iomux-mx6q.h (for i.MX6Q). &lt;/SPAN&gt; So, if I want to use different function of iomux pin, I will modify/add&amp;nbsp; the name of the iomux pin in arch/arm/mach-mx6/board-mx6q_sabresd.h (e.g. for the SabreSD board). &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jul 2014 08:22:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-code-generated-by-IOMUX-tool-for-iMX6SDL-using-USDHC/m-p/325136#M43639</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2014-07-31T08:22:01Z</dc:date>
    </item>
    <item>
      <title>Re: Error in code generated by IOMUX tool for iMX6SDL using USDHC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-code-generated-by-IOMUX-tool-for-iMX6SDL-using-USDHC/m-p/325137#M43640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Of course I know that, my problem was with the interactive IOMUX tool. As you can see from my other post, it was just an issue with an outdated version still available for download.&lt;/P&gt;&lt;P&gt;The IOMUX tool is very powerful and prevents making mistakes, but could be made much better with two key improvements:&lt;/P&gt;&lt;P&gt;- make daisy-chain (SELECT_INPUT) automatic with pin selection, as it is now in the Linux headers you mention&lt;/P&gt;&lt;P&gt;- allow for multiple device options (DQ and SDL which have the same BGA layout) on the same board in one design&lt;/P&gt;&lt;P&gt;The great advantage with IOMUX is having one reference source of information for many tasks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jul 2014 09:04:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-code-generated-by-IOMUX-tool-for-iMX6SDL-using-USDHC/m-p/325137#M43640</guid>
      <dc:creator>marcocontenti</dc:creator>
      <dc:date>2014-07-31T09:04:17Z</dc:date>
    </item>
  </channel>
</rss>