<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Watchdog Timer in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Watchdog-Timer/m-p/324994#M43628</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Murali&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for high reliability applications (such as medical)&lt;/P&gt;&lt;P&gt;it is recommedned to use external watchdog.&lt;/P&gt;&lt;P&gt;If the software hangs, I.MX6 Watch Dog will effectively detect and reset the entire processor.&lt;/P&gt;&lt;P&gt;However if processor hangs (for example due to EMI), Watch Dog may malfunction&lt;/P&gt;&lt;P&gt;(due to absence of internal clocks).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 27 Jul 2014 15:58:30 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-07-27T15:58:30Z</dc:date>
    <item>
      <title>Watchdog Timer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Watchdog-Timer/m-p/324993#M43627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using i.MX6 Quad Processor in our design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;We are developing one of the&amp;nbsp; product for &lt;/SPAN&gt;&lt;STRONG style=": ; color: #ff0000; font-size: 12pt;"&gt;Critical Medical Application&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We need some clarifiaction on the Internal Watchdog Functionality.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is internal Watchdog is able to detect the hanging the Software of the any particular core in the processor and resets the entier processor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In otherwords if the software hangs, how effectively the Internal Watch Dog circuitry will detect and reset the entire processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the Watchdog circuitry falls in particular core and software hanging/ not working of that particular part core is not functioning then how effectively watchdog processor will reset the entire core. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly Clarify.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in Advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jul 2014 14:27:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Watchdog-Timer/m-p/324993#M43627</guid>
      <dc:creator>muralikrishna</dc:creator>
      <dc:date>2014-07-25T14:27:56Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog Timer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Watchdog-Timer/m-p/324994#M43628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Murali&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for high reliability applications (such as medical)&lt;/P&gt;&lt;P&gt;it is recommedned to use external watchdog.&lt;/P&gt;&lt;P&gt;If the software hangs, I.MX6 Watch Dog will effectively detect and reset the entire processor.&lt;/P&gt;&lt;P&gt;However if processor hangs (for example due to EMI), Watch Dog may malfunction&lt;/P&gt;&lt;P&gt;(due to absence of internal clocks).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 27 Jul 2014 15:58:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Watchdog-Timer/m-p/324994#M43628</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-27T15:58:30Z</dc:date>
    </item>
  </channel>
</rss>