<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow to set USB serial as debug port / console?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-set-USB-serial-as-debug-port-console/m-p/324752#M43574</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on an iMX23 cpu with linux-2.6.35.3 and wondering if this is even possible to implement.&lt;/P&gt;&lt;P&gt;I can build g_serial and g_multi and use the serial port function, which uses /dev/ttyGS0.&lt;/P&gt;&lt;P&gt;Do I just have to change [console=ttyS0] to [console=ttyGS0] on the kernel command line?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Jun 2014 08:18:34 GMT</pubDate>
    <dc:creator>yurirellosa</dc:creator>
    <dc:date>2014-06-26T08:18:34Z</dc:date>
    <item>
      <title>How to set USB serial as debug port / console?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-set-USB-serial-as-debug-port-console/m-p/324752#M43574</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on an iMX23 cpu with linux-2.6.35.3 and wondering if this is even possible to implement.&lt;/P&gt;&lt;P&gt;I can build g_serial and g_multi and use the serial port function, which uses /dev/ttyGS0.&lt;/P&gt;&lt;P&gt;Do I just have to change [console=ttyS0] to [console=ttyGS0] on the kernel command line?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2014 08:18:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-set-USB-serial-as-debug-port-console/m-p/324752#M43574</guid>
      <dc:creator>yurirellosa</dc:creator>
      <dc:date>2014-06-26T08:18:34Z</dc:date>
    </item>
    <item>
      <title>Re: How to set USB serial as debug port / console?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-set-USB-serial-as-debug-port-console/m-p/324753#M43575</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I added another console setting in [/etc/inittab]&lt;/P&gt;&lt;P&gt;::respawn:/sbin/getty -L ttyAM0 115200 vt100&lt;/P&gt;&lt;P&gt;It works fine!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jun 2014 00:56:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-set-USB-serial-as-debug-port-console/m-p/324753#M43575</guid>
      <dc:creator>yurirellosa</dc:creator>
      <dc:date>2014-06-27T00:56:48Z</dc:date>
    </item>
  </channel>
</rss>