<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6Q: using parallel CSI on second IPU</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-using-parallel-CSI-on-second-IPU/m-p/324646#M43545</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;maybe yes, anyway i will attach the new DTS files that make USB H1 and USB OTG working on&amp;nbsp; phyflex &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Jun 2014 07:16:44 GMT</pubDate>
    <dc:creator>Selea</dc:creator>
    <dc:date>2014-06-26T07:16:44Z</dc:date>
    <item>
      <title>IMX6Q: using parallel CSI on second IPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-using-parallel-CSI-on-second-IPU/m-p/324644#M43543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to use a parallel sensor on the second parallel CSI input. this second paralle (according with documentation) can be routed only on the second IPU.&lt;/P&gt;&lt;P&gt;so in my DTS i have IPU_id=1 and CSI_id=1.&lt;/P&gt;&lt;P&gt;the driver probe is working fine, the sensor is found , configured and the signal seems to be present and correct. the V4L2 device is created (/dev/video2) but when i try to read from it it sat read timeout...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestion.&lt;/P&gt;&lt;P&gt;Omar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2014 15:56:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-using-parallel-CSI-on-second-IPU/m-p/324644#M43543</guid>
      <dc:creator>Selea</dc:creator>
      <dc:date>2014-06-25T15:56:32Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q: using parallel CSI on second IPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-using-parallel-CSI-on-second-IPU/m-p/324645#M43544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Time to start a new thread?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2014 16:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-using-parallel-CSI-on-second-IPU/m-p/324645#M43544</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2014-06-25T16:03:08Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q: using parallel CSI on second IPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-using-parallel-CSI-on-second-IPU/m-p/324646#M43545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;maybe yes, anyway i will attach the new DTS files that make USB H1 and USB OTG working on&amp;nbsp; phyflex &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2014 07:16:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-using-parallel-CSI-on-second-IPU/m-p/324646#M43545</guid>
      <dc:creator>Selea</dc:creator>
      <dc:date>2014-06-26T07:16:44Z</dc:date>
    </item>
    <item>
      <title>Re: Re: IMX6Q: using parallel CSI on second IPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-using-parallel-CSI-on-second-IPU/m-p/324647#M43546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I add my DTS files (they are customized for our board startting from phytec one). As you will see I addedd a Cmos sensor AR0134 that shoul use the parallel input port on the second IPU.&lt;/P&gt;&lt;P&gt;and i configured the second paralle port pins as well.&lt;/P&gt;&lt;P&gt;The driver is loaded, the sensor is configured on I2C, and i see the device created, but when i try to read from that one it not works : just say timeout... seems that the port is not capturing&lt;/P&gt;&lt;P&gt;so i think i missing some initialization on CSI or IPU.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Sep 2014 07:05:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-using-parallel-CSI-on-second-IPU/m-p/324647#M43546</guid>
      <dc:creator>Selea</dc:creator>
      <dc:date>2014-09-11T07:05:39Z</dc:date>
    </item>
  </channel>
</rss>