<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX280 on Nucleus</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX280-on-Nucleus/m-p/324397#M43466</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ramesh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;probably voltage still high than VBUSVALID_TRSH level &lt;/P&gt;&lt;P&gt;(defined in register HW_POWER_5VCTRL) due to capacitor.on 5v input.&lt;/P&gt;&lt;P&gt;One try to ground it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Jul 2014 13:41:18 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-07-24T13:41:18Z</dc:date>
    <item>
      <title>IMX280 on Nucleus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX280-on-Nucleus/m-p/324396#M43465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Running a Nucleus kernel on an imx280 board.&lt;/P&gt;&lt;P&gt;When 5v input&amp;nbsp; is removed, Power STS bit 15 is still high meaning that there is power. ANy idea why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jul 2014 05:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX280-on-Nucleus/m-p/324396#M43465</guid>
      <dc:creator>rameshnair</dc:creator>
      <dc:date>2014-07-24T05:26:48Z</dc:date>
    </item>
    <item>
      <title>Re: IMX280 on Nucleus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX280-on-Nucleus/m-p/324397#M43466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ramesh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;probably voltage still high than VBUSVALID_TRSH level &lt;/P&gt;&lt;P&gt;(defined in register HW_POWER_5VCTRL) due to capacitor.on 5v input.&lt;/P&gt;&lt;P&gt;One try to ground it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jul 2014 13:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX280-on-Nucleus/m-p/324397#M43466</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-24T13:41:18Z</dc:date>
    </item>
  </channel>
</rss>