<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックWiFi / Ethernet do not coexist well in Android</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-Ethernet-do-not-coexist-well-in-Android/m-p/324193#M43406</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see that in both ICS and JB, WiFi and Ethernet cannot coexist.&lt;/P&gt;&lt;P&gt;I have quite figured out the reason: ConnectivityService.java manages kind of policy, where all the network connections are prioritized, so the one with the lower priority is torn down (Ethernet happens to be prioritized over WiFi).&lt;/P&gt;&lt;P&gt;In case the unrequired network is disconnected (e.g. Ethernet cable is pulled out or WiFi is off), the other network is Ok.&lt;/P&gt;&lt;P&gt;But in order to use my device (i.mx6) as an access point, I would like to have them both.&lt;/P&gt;&lt;P&gt;I have tried to merely delete the policy checks from the code, but, at least with JB, it seems to screw the networking altogether.&lt;/P&gt;&lt;P&gt;How can it be done ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Jun 2014 13:54:17 GMT</pubDate>
    <dc:creator>andreygelman</dc:creator>
    <dc:date>2014-06-25T13:54:17Z</dc:date>
    <item>
      <title>WiFi / Ethernet do not coexist well in Android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-Ethernet-do-not-coexist-well-in-Android/m-p/324193#M43406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see that in both ICS and JB, WiFi and Ethernet cannot coexist.&lt;/P&gt;&lt;P&gt;I have quite figured out the reason: ConnectivityService.java manages kind of policy, where all the network connections are prioritized, so the one with the lower priority is torn down (Ethernet happens to be prioritized over WiFi).&lt;/P&gt;&lt;P&gt;In case the unrequired network is disconnected (e.g. Ethernet cable is pulled out or WiFi is off), the other network is Ok.&lt;/P&gt;&lt;P&gt;But in order to use my device (i.mx6) as an access point, I would like to have them both.&lt;/P&gt;&lt;P&gt;I have tried to merely delete the policy checks from the code, but, at least with JB, it seems to screw the networking altogether.&lt;/P&gt;&lt;P&gt;How can it be done ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2014 13:54:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-Ethernet-do-not-coexist-well-in-Android/m-p/324193#M43406</guid>
      <dc:creator>andreygelman</dc:creator>
      <dc:date>2014-06-25T13:54:17Z</dc:date>
    </item>
    <item>
      <title>Re: WiFi / Ethernet do not coexist well in Android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-Ethernet-do-not-coexist-well-in-Android/m-p/324194#M43407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I haven't tried this before but I haven't heard of anyone doing it, this is a Google limitation I guess&lt;/P&gt;&lt;P&gt;Nevertheless, I did a google search and I found a person that wanted to do the exact same thing that you want, and he was able to work-around-it by using a USB to Ethernet adapter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Sergio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2014 19:06:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-Ethernet-do-not-coexist-well-in-Android/m-p/324194#M43407</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2014-06-25T19:06:19Z</dc:date>
    </item>
  </channel>
</rss>