<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Start up time and FPS problem using QT5 with different version of kernel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Start-up-time-and-FPS-problem-using-QT5-with-different-version/m-p/323930#M43358</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Some progress:&lt;/P&gt;&lt;P&gt;the slow start up time of QT on 3.0.35 kernel is because the slow close time of /dev/input/event* device files.&lt;/P&gt;&lt;P&gt;It takes 0.3s for each of them in 3.0.35 kernel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Jun 2014 06:58:33 GMT</pubDate>
    <dc:creator>qiangyu</dc:creator>
    <dc:date>2014-06-30T06:58:33Z</dc:date>
    <item>
      <title>Start up time and FPS problem using QT5 with different version of kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Start-up-time-and-FPS-problem-using-QT5-with-different-version/m-p/323929#M43357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using IMX6Q Sabre Lite to run a QT5 demo, but there are two problems:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;the start up time of the demo on 3.0.35 kernel is 3s slower than on 3.10.17 kernel&lt;/LI&gt;&lt;LI&gt;the FPS periodically drops using a 3.10.17 graphic stack while it remains 60 using a 3.5.7 graphic stack&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The start up time diffs only on the call of &lt;/P&gt;&lt;PRE class="jive-pre"&gt;&lt;SPAN style="color: #800080;"&gt;QGuiApplication&lt;/SPAN&gt;&lt;SPAN style="color: #c0c0c0;"&gt; &lt;/SPAN&gt;&lt;SPAN style="color: #000000;"&gt;app&lt;/SPAN&gt;&lt;SPAN style="color: #000000;"&gt;(&lt;/SPAN&gt;&lt;SPAN style="color: #000000;"&gt;argc&lt;/SPAN&gt;&lt;SPAN style="color: #000000;"&gt;,&lt;/SPAN&gt;&lt;SPAN style="color: #c0c0c0;"&gt; &lt;/SPAN&gt;&lt;SPAN style="color: #000000;"&gt;argv&lt;/SPAN&gt;&lt;SPAN style="color: #000000;"&gt;);&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some info about my platform:&lt;/P&gt;&lt;P&gt;IMX6Q Sabre Lite&lt;/P&gt;&lt;P&gt;QT5.2.1 &amp;amp; QT5.3.0&lt;/P&gt;&lt;P&gt;Buildroot&lt;/P&gt;&lt;P&gt;LVDS 1280x480&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've test many combination of kernel version and graphic stack, here is my conclusion:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;the start up time only depends on the kernel version, not the graphic stack. &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Because the same graphic stack (including kernel part) with different kernel version will cause the problem; the same kernel (not the GPU driver part) with different graphic stack (including kernel part) won't cause the problem.&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;the FPS mainly depends on the graphic stack, kernel version only affects the drop amount. The 3.10.17 graphic stack drop more on 3.10.17 kernel while drop less on 3.0.35 kernel.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does any one have the same problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Qiang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2014 06:52:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Start-up-time-and-FPS-problem-using-QT5-with-different-version/m-p/323929#M43357</guid>
      <dc:creator>qiangyu</dc:creator>
      <dc:date>2014-06-25T06:52:39Z</dc:date>
    </item>
    <item>
      <title>Re: Start up time and FPS problem using QT5 with different version of kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Start-up-time-and-FPS-problem-using-QT5-with-different-version/m-p/323930#M43358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Some progress:&lt;/P&gt;&lt;P&gt;the slow start up time of QT on 3.0.35 kernel is because the slow close time of /dev/input/event* device files.&lt;/P&gt;&lt;P&gt;It takes 0.3s for each of them in 3.0.35 kernel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jun 2014 06:58:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Start-up-time-and-FPS-problem-using-QT5-with-different-version/m-p/323930#M43358</guid>
      <dc:creator>qiangyu</dc:creator>
      <dc:date>2014-06-30T06:58:33Z</dc:date>
    </item>
  </channel>
</rss>