<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic U-Boot on I.Mx35 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-on-I-Mx35/m-p/323504#M43314</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to port U-Boot for an custom I.Mx35 board with only NAND-Flash, t&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;he board comes with an RedBoot bootloader.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there someone who has any experience with booting from NAND flash?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have read some I.Mx configurations and I could only find one device booting directly from NAND (Karo - tx25, I.Mx25).&lt;/P&gt;&lt;P&gt;But I'm not sure if this will also work for the I.Mx35?!?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Jul 2014 15:18:51 GMT</pubDate>
    <dc:creator>m_f_vankessel</dc:creator>
    <dc:date>2014-07-22T15:18:51Z</dc:date>
    <item>
      <title>U-Boot on I.Mx35</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-on-I-Mx35/m-p/323504#M43314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to port U-Boot for an custom I.Mx35 board with only NAND-Flash, t&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;he board comes with an RedBoot bootloader.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there someone who has any experience with booting from NAND flash?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have read some I.Mx configurations and I could only find one device booting directly from NAND (Karo - tx25, I.Mx25).&lt;/P&gt;&lt;P&gt;But I'm not sure if this will also work for the I.Mx35?!?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jul 2014 15:18:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-on-I-Mx35/m-p/323504#M43314</guid>
      <dc:creator>m_f_vankessel</dc:creator>
      <dc:date>2014-07-22T15:18:51Z</dc:date>
    </item>
    <item>
      <title>Re: U-Boot on I.Mx35</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-on-I-Mx35/m-p/323505#M43315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to app note AN4172 (U-Boot® for i.MX35 Based Designs)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/dsp/doc/app_note/AN4172.pdf"&gt;http://cache.freescale.com/files/dsp/doc/app_note/AN4172.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jul 2014 01:42:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-on-I-Mx35/m-p/323505#M43315</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-07-23T01:42:50Z</dc:date>
    </item>
  </channel>
</rss>