<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx6  camera interface I/O voltage levels in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-camera-interface-I-O-voltage-levels/m-p/323403#M43301</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi erdem&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NVCC_CSI can be from 1.65 to 3.6V&lt;/P&gt;&lt;P&gt;please check Table 6 "Operating Ranges'&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation"&gt;IMX6DQCEC&lt;/A&gt; i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One can also check sect.4.6.2 "General Purpose I/O (GPIO) DC Parameters",&lt;/P&gt;&lt;P&gt;Table 100 "21 x 21 mm Functional Contact Assignments".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Jul 2014 12:01:16 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-07-22T12:01:16Z</dc:date>
    <item>
      <title>imx6  camera interface I/O voltage levels</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-camera-interface-I-O-voltage-levels/m-p/323402#M43300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi guys &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;does imx6 camera interface I/O&amp;nbsp; s are&amp;nbsp; 2.8V ? or 1.8V ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jul 2014 11:11:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-camera-interface-I-O-voltage-levels/m-p/323402#M43300</guid>
      <dc:creator>erdempamuk</dc:creator>
      <dc:date>2014-07-22T11:11:22Z</dc:date>
    </item>
    <item>
      <title>Re: imx6  camera interface I/O voltage levels</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-camera-interface-I-O-voltage-levels/m-p/323403#M43301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi erdem&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NVCC_CSI can be from 1.65 to 3.6V&lt;/P&gt;&lt;P&gt;please check Table 6 "Operating Ranges'&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation"&gt;IMX6DQCEC&lt;/A&gt; i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One can also check sect.4.6.2 "General Purpose I/O (GPIO) DC Parameters",&lt;/P&gt;&lt;P&gt;Table 100 "21 x 21 mm Functional Contact Assignments".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jul 2014 12:01:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-camera-interface-I-O-voltage-levels/m-p/323403#M43301</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-22T12:01:16Z</dc:date>
    </item>
  </channel>
</rss>