<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: HAB enabled or not?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HAB-enabled-or-not/m-p/323377#M43295</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; In some sense the HAB is always enabled, meaning that the boot ROM checks &lt;BR /&gt; the IVT, SRK, CSF before boot code executing. If SRK or CSF are not present (or illegal), &lt;BR /&gt; the boot code starts only in “Open” security configuration. Please refer to section 8.2.6 &lt;BR /&gt; (Boot security settings) of the i.MX6 DQ Reference Manual (RM) about security configurations.&lt;BR /&gt; Also, for more details please use section 8.6.1.1 (Image Vector Table Structure) of the RM&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;and Figure 1 (Secure Boot Flow from Device) of app note AN4581 (Secure Boot on i.MX50, &lt;BR /&gt; i.MX53, and i.MX 6 Series using HABv4).&lt;BR /&gt; &lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Jun 2014 04:21:11 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2014-06-25T04:21:11Z</dc:date>
    <item>
      <title>HAB enabled or not?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HAB-enabled-or-not/m-p/323376#M43294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am working on HAB feature of imx6. I just want to know, how the ROM will know, if HAB is enabled or not? Will ROM check for&amp;nbsp; HW_OCOTP_CFG5 fuse or SRK fuses to check if HAB is enabled or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While testing, &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;I have not fused both the above things (and by default, HAB is in open configuration), but enabled secure boot on u-boot (by defining CONFIG_SECURE_BOOT macro). When I tried booting the resultant u-boot.imx(without adding CSF data), some HAB events are printed on the console. I saw from the u-boot source code, that if "CONFIG_SECURE_BOOT" is defined, call "get_hab_status"&amp;nbsp; and so it prints the HAB events. My question, is the HAB check really performed or it just prints some spurious HAB events on the console since I have not fused either HW_OCOTP_CFG5 nor SRK fuses.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jun 2014 10:55:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HAB-enabled-or-not/m-p/323376#M43294</guid>
      <dc:creator>jaiganesh</dc:creator>
      <dc:date>2014-06-24T10:55:06Z</dc:date>
    </item>
    <item>
      <title>Re: HAB enabled or not?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HAB-enabled-or-not/m-p/323377#M43295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; In some sense the HAB is always enabled, meaning that the boot ROM checks &lt;BR /&gt; the IVT, SRK, CSF before boot code executing. If SRK or CSF are not present (or illegal), &lt;BR /&gt; the boot code starts only in “Open” security configuration. Please refer to section 8.2.6 &lt;BR /&gt; (Boot security settings) of the i.MX6 DQ Reference Manual (RM) about security configurations.&lt;BR /&gt; Also, for more details please use section 8.6.1.1 (Image Vector Table Structure) of the RM&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;and Figure 1 (Secure Boot Flow from Device) of app note AN4581 (Secure Boot on i.MX50, &lt;BR /&gt; i.MX53, and i.MX 6 Series using HABv4).&lt;BR /&gt; &lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2014 04:21:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HAB-enabled-or-not/m-p/323377#M43295</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-06-25T04:21:11Z</dc:date>
    </item>
  </channel>
</rss>