<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LVDS Display resolution in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323372#M43291</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you can achieve 1080p by using split channel mode.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Sergio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Jun 2014 18:43:51 GMT</pubDate>
    <dc:creator>SergioSolis</dc:creator>
    <dc:date>2014-06-24T18:43:51Z</dc:date>
    <item>
      <title>LVDS Display resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323368#M43287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the maximum resolution we can get by using only one LVDS Channel.?? As per information I think it is not possible to achieve 1080p HD resolution by using only one LVDS channel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a 31.5 inch LVDS Display, having two channel input, and resolution 1920x1080. How is it possible to increase the resolution to get Full HD 1920x1080 ? i.e. what input must be supplied to the LCD input pins,? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jun 2014 09:57:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323368#M43287</guid>
      <dc:creator>pankajrana</dc:creator>
      <dc:date>2014-06-24T09:57:34Z</dc:date>
    </item>
    <item>
      <title>Re: LVDS Display resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323369#M43288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;To get 1080P you need to use two channel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jun 2014 11:01:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323369#M43288</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-06-24T11:01:08Z</dc:date>
    </item>
    <item>
      <title>Re: LVDS Display resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323370#M43289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Saurabh,&lt;/P&gt;&lt;P&gt;Using two channels is fine, even the Display supports that, but am worried about the mode to be used, Should I go with Dual Channel Mode , or Split Channel mode ?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Pankaj Rana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jun 2014 11:17:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323370#M43289</guid>
      <dc:creator>pankajrana</dc:creator>
      <dc:date>2014-06-24T11:17:50Z</dc:date>
    </item>
    <item>
      <title>Re: LVDS Display resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323371#M43290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should use Split channel mode to get 1080P working...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jun 2014 12:04:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323371#M43290</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-06-24T12:04:15Z</dc:date>
    </item>
    <item>
      <title>Re: LVDS Display resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323372#M43291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you can achieve 1080p by using split channel mode.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Sergio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jun 2014 18:43:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323372#M43291</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2014-06-24T18:43:51Z</dc:date>
    </item>
    <item>
      <title>Re: LVDS Display resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323373#M43292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/SergioSolis"&gt;SergioSolis&lt;/A&gt; &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/SaurabhPatel"&gt;SaurabhPatel&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Split mode is understood, but what if I don't go for SPLIT mode, instead I choose Dual Channel Mode.&lt;BR /&gt;i.e. Using only channel one , and then providing the same data to both the input ports of the Display.?&lt;/P&gt;&lt;P&gt;will that give a proper image/display, or will it spoil the contents !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Pankaj Rana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2014 05:05:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323373#M43292</guid>
      <dc:creator>pankajrana</dc:creator>
      <dc:date>2014-06-25T05:05:43Z</dc:date>
    </item>
    <item>
      <title>Re: LVDS Display resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323374#M43293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you don't use split mode than you will not get the 1080P.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dual Mode is used to display same data on two display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can try if you want, and share your result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2014 05:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LVDS-Display-resolution/m-p/323374#M43293</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-06-25T05:27:01Z</dc:date>
    </item>
  </channel>
</rss>