<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Using new (DTS-based) Linux on Embedsky E9 board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-new-DTS-based-Linux-on-Embedsky-E9-board/m-p/323010#M43200</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to build barebox with&lt;/P&gt;&lt;P&gt;make ARCH=arm imx_v7_defconfig&lt;/P&gt;&lt;P&gt;make ARCH=arm&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or you can do a 'make ARCH=arm menuconfig' and disable other imx boards that will be built by default.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This will produce an 'images/barebox-freescale-imx6q-embedsky-e9.img'&lt;/P&gt;&lt;P&gt;copy it to SD card with&lt;/P&gt;&lt;P&gt;dd if=images/barebox-freescale-imx6q-embedsky-e9.img of=&amp;lt;/dev/sdcard&amp;gt; bs=1k seek=1 skip=1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Make 2 partitions on SD&lt;/P&gt;&lt;P&gt;First is bootfs, second is rootfs&lt;/P&gt;&lt;P&gt;You should put zImage and DTB to bootfs, default filenames are 'zImage' and 'imx6q-embedsky-e9.dtb'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can drop in barebox shell and edit boot scripts if needed, they are in /env/boot/* files&lt;/P&gt;&lt;P&gt;Default is mmc1 or mmc3, depends on boot media.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edit it with command 'edit /env/boot/mmc1' and save with 'saveenv'&lt;/P&gt;&lt;P&gt;Other usage examples are in barebox documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Look at my github tree at &lt;A href="https://github.com/apxii/linux/tree/embedsky-e9" title="https://github.com/apxii/linux/tree/embedsky-e9"&gt;apxii/linux · GitHub&lt;/A&gt; &lt;/P&gt;&lt;P&gt;But it is mainline-based, and DTS will not fit in Freescale tree.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Jun 2015 07:23:23 GMT</pubDate>
    <dc:creator>andreypanov</dc:creator>
    <dc:date>2015-06-19T07:23:23Z</dc:date>
    <item>
      <title>Using new (DTS-based) Linux on Embedsky E9 board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-new-DTS-based-Linux-on-Embedsky-E9-board/m-p/323007#M43197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;Does anyone use Embedsky E9 board (&lt;A href="http://en.embedsky.com/product_info.php?cateid=169&amp;amp;id=169" title="http://en.embedsky.com/product_info.php?cateid=169&amp;amp;id=169"&gt;http://en.embedsky.com/product_info.php?cateid=169&amp;amp;id=169&lt;/A&gt;) with 3.15 kernel?&lt;/P&gt;&lt;P&gt;It is i.MX6Q based board with (vendor said) design based on SabreSD, but it is not compatible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had ported Barebox bootloader and was able to boot Linux to commandline.&lt;/P&gt;&lt;P&gt;It works, but has a few issues: &lt;/P&gt;&lt;P&gt;a) Ethernet PHY detection is unstable, it has Realtek RTL8211 chip, but it detected in 50% cases.&lt;/P&gt;&lt;P&gt;b) Sound doesn't work at all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe someone had a proper DTS for this board?&lt;/P&gt;&lt;P&gt;Or some linux kernel patches?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jun 2014 14:43:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-new-DTS-based-Linux-on-Embedsky-E9-board/m-p/323007#M43197</guid>
      <dc:creator>andreypanov</dc:creator>
      <dc:date>2014-06-23T14:43:43Z</dc:date>
    </item>
    <item>
      <title>Re: Using new (DTS-based) Linux on Embedsky E9 board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-new-DTS-based-Linux-on-Embedsky-E9-board/m-p/323008#M43198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My patches was accepted in barebox repo, so booting a Linus kernel will work.&lt;/P&gt;&lt;P&gt;Kernel from Freescale repo doesn't detect a RTL8211E gigabit PHY.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jul 2014 06:18:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-new-DTS-based-Linux-on-Embedsky-E9-board/m-p/323008#M43198</guid>
      <dc:creator>andreypanov</dc:creator>
      <dc:date>2014-07-25T06:18:35Z</dc:date>
    </item>
    <item>
      <title>Re: Using new (DTS-based) Linux on Embedsky E9 board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-new-DTS-based-Linux-on-Embedsky-E9-board/m-p/323009#M43199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Great Job!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but how to booting kernel?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using 3.10.53 from freescale (with android), but can't boot it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found a patch in meta-fsl-arm,&amp;nbsp; but it looks like we need extra dts which is not in the patch.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2015 01:34:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-new-DTS-based-Linux-on-Embedsky-E9-board/m-p/323009#M43199</guid>
      <dc:creator>yiqingliang</dc:creator>
      <dc:date>2015-06-19T01:34:34Z</dc:date>
    </item>
    <item>
      <title>Re: Using new (DTS-based) Linux on Embedsky E9 board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-new-DTS-based-Linux-on-Embedsky-E9-board/m-p/323010#M43200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to build barebox with&lt;/P&gt;&lt;P&gt;make ARCH=arm imx_v7_defconfig&lt;/P&gt;&lt;P&gt;make ARCH=arm&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or you can do a 'make ARCH=arm menuconfig' and disable other imx boards that will be built by default.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This will produce an 'images/barebox-freescale-imx6q-embedsky-e9.img'&lt;/P&gt;&lt;P&gt;copy it to SD card with&lt;/P&gt;&lt;P&gt;dd if=images/barebox-freescale-imx6q-embedsky-e9.img of=&amp;lt;/dev/sdcard&amp;gt; bs=1k seek=1 skip=1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Make 2 partitions on SD&lt;/P&gt;&lt;P&gt;First is bootfs, second is rootfs&lt;/P&gt;&lt;P&gt;You should put zImage and DTB to bootfs, default filenames are 'zImage' and 'imx6q-embedsky-e9.dtb'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can drop in barebox shell and edit boot scripts if needed, they are in /env/boot/* files&lt;/P&gt;&lt;P&gt;Default is mmc1 or mmc3, depends on boot media.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edit it with command 'edit /env/boot/mmc1' and save with 'saveenv'&lt;/P&gt;&lt;P&gt;Other usage examples are in barebox documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Look at my github tree at &lt;A href="https://github.com/apxii/linux/tree/embedsky-e9" title="https://github.com/apxii/linux/tree/embedsky-e9"&gt;apxii/linux · GitHub&lt;/A&gt; &lt;/P&gt;&lt;P&gt;But it is mainline-based, and DTS will not fit in Freescale tree.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2015 07:23:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-new-DTS-based-Linux-on-Embedsky-E9-board/m-p/323010#M43200</guid>
      <dc:creator>andreypanov</dc:creator>
      <dc:date>2015-06-19T07:23:23Z</dc:date>
    </item>
  </channel>
</rss>