<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TFTPboot over USB OTG in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/TFTPboot-over-USB-OTG/m-p/322705#M43143</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yep. We're doing that on a very regular basis. This is especially useful when we load up boards with on-board eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We added this into our 2014.01 release of U-Boot and some details are in this post:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://boundarydevices.com/u-boot-2014-01/#details" title="http://boundarydevices.com/u-boot-2014-01/#details"&gt;http://boundarydevices.com/u-boot-2014-01/#details&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 Jun 2014 17:26:47 GMT</pubDate>
    <dc:creator>EricNelson</dc:creator>
    <dc:date>2014-06-21T17:26:47Z</dc:date>
    <item>
      <title>TFTPboot over USB OTG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TFTPboot-over-USB-OTG/m-p/322704#M43142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to tftpboot the kernel and rootfs over USB OTG on the imx6. I think I would have to enable ethernet over the USB OTG connection. I don't have the Ethernet pins brought out on my custom board so am looking for a solution over USB OTG port. Has anyone done this? What are the steps to enable this in the kernel?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Jun 2014 17:11:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TFTPboot-over-USB-OTG/m-p/322704#M43142</guid>
      <dc:creator>varsmolta</dc:creator>
      <dc:date>2014-06-21T17:11:54Z</dc:date>
    </item>
    <item>
      <title>Re: TFTPboot over USB OTG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TFTPboot-over-USB-OTG/m-p/322705#M43143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yep. We're doing that on a very regular basis. This is especially useful when we load up boards with on-board eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We added this into our 2014.01 release of U-Boot and some details are in this post:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://boundarydevices.com/u-boot-2014-01/#details" title="http://boundarydevices.com/u-boot-2014-01/#details"&gt;http://boundarydevices.com/u-boot-2014-01/#details&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Jun 2014 17:26:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TFTPboot-over-USB-OTG/m-p/322705#M43143</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-06-21T17:26:47Z</dc:date>
    </item>
    <item>
      <title>Re: TFTPboot over USB OTG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TFTPboot-over-USB-OTG/m-p/322706#M43144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks for that link. One more question: is it possible to use this in the 2009.08 u-boot version from boundarydevices? If not, can I back port changes into 2009.08? Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Jun 2014 19:07:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TFTPboot-over-USB-OTG/m-p/322706#M43144</guid>
      <dc:creator>varsmolta</dc:creator>
      <dc:date>2014-06-22T19:07:00Z</dc:date>
    </item>
    <item>
      <title>Re: TFTPboot over USB OTG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TFTPboot-over-USB-OTG/m-p/322707#M43145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't really know the state of the 2009.08 release, but I don't believe USB OTG is functional, or at least not as a network device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's your reason for wanting to back-port?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Jun 2014 21:15:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TFTPboot-over-USB-OTG/m-p/322707#M43145</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-06-22T21:15:59Z</dc:date>
    </item>
    <item>
      <title>Re: TFTPboot over USB OTG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TFTPboot-over-USB-OTG/m-p/322708#M43146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using an off the shelf imx6 board from bluechiptechnology called the RM3. They only support the 2009.08 release of u-boot. I could try to use the mainline 2014 u-boot version from boundarydevices and try to add the RM3 board support into it. How big of an effort would that be if I started with the nitrogen6x config? Could I do it in a couple of days? I've never really tweaked u-boot code before.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jun 2014 00:49:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TFTPboot-over-USB-OTG/m-p/322708#M43146</guid>
      <dc:creator>varsmolta</dc:creator>
      <dc:date>2014-06-23T00:49:49Z</dc:date>
    </item>
    <item>
      <title>Re: TFTPboot over USB OTG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TFTPboot-over-USB-OTG/m-p/322709#M43147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All I can say is that you should talk to your vendor. Porting U-Boot versions isn't something you should dive into with an expectation of a quick fix.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that this message thread has drifted off of the original topic, and I think the original question is answered. If you want to discuss porting the U-Boot version for this board, please start another topic.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jun 2014 14:06:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TFTPboot-over-USB-OTG/m-p/322709#M43147</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-06-23T14:06:31Z</dc:date>
    </item>
  </channel>
</rss>