<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic DCDC_BATT and VDD4P2 connection in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DCDC-BATT-and-VDD4P2-connection/m-p/321946#M43002</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're using imx28 in 4V input only scenario and supplying power to DCDC_BATT and BATTERY pins. Since VDD5V is not used, 4P2LinReg is not used and I assume there's no use of the VDD4P2 pin. But why is there a diode connecting DCDC_BATT to VDD4P2? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd appreciate if you could briefly explain this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Semih&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Jul 2014 09:40:23 GMT</pubDate>
    <dc:creator>semihhazar</dc:creator>
    <dc:date>2014-07-18T09:40:23Z</dc:date>
    <item>
      <title>DCDC_BATT and VDD4P2 connection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DCDC-BATT-and-VDD4P2-connection/m-p/321946#M43002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're using imx28 in 4V input only scenario and supplying power to DCDC_BATT and BATTERY pins. Since VDD5V is not used, 4P2LinReg is not used and I assume there's no use of the VDD4P2 pin. But why is there a diode connecting DCDC_BATT to VDD4P2? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd appreciate if you could briefly explain this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Semih&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jul 2014 09:40:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DCDC-BATT-and-VDD4P2-connection/m-p/321946#M43002</guid>
      <dc:creator>semihhazar</dc:creator>
      <dc:date>2014-07-18T09:40:23Z</dc:date>
    </item>
    <item>
      <title>Re: DCDC_BATT and VDD4P2 connection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DCDC-BATT-and-VDD4P2-connection/m-p/321947#M43003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Semih&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the purpose of the diode to guarantee the supply to the DCDC is not&lt;/P&gt;&lt;P&gt;interrupted when switching from battery to VDD4P2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jul 2014 15:04:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DCDC-BATT-and-VDD4P2-connection/m-p/321947#M43003</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-18T15:04:30Z</dc:date>
    </item>
  </channel>
</rss>