<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX28 linux boot problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321447#M42891</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, i have used DEBUG UART cable and HyperTerminal, i was successfull logged in as root. &lt;/P&gt;&lt;P&gt;So it is working, but on VGA Display still only penguin is visible. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is possible to install own linux build with some GUI which will appear on VGA Display? &lt;/P&gt;&lt;P&gt;In video tutorial after boot some window and folders are visible on VGA... &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Jul 2014 13:08:59 GMT</pubDate>
    <dc:creator>wyder</dc:creator>
    <dc:date>2014-07-18T13:08:59Z</dc:date>
    <item>
      <title>i.MX28 linux boot problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321444#M42888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have i.MX28 EVK. I try to start OS from SD0 from provided SC cards.&lt;/P&gt;&lt;P&gt;WINCE start with no problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i try to boot from ubuntu SD, only penguin appears on left up corner, nothing else happens.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't figure out when the problem is, i make new SD card according to instruction on CD (virtual machine, etc.. )&lt;/P&gt;&lt;P&gt;but result is the same. It is possible that something is wrong with hardware ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please, help! Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jul 2014 12:20:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321444#M42888</guid>
      <dc:creator>wyder</dc:creator>
      <dc:date>2014-07-17T12:20:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 linux boot problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321445#M42889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrzej&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;provided Freescale Demo (link below) is Linux Demo (not Ubuntu), so small&lt;/P&gt;&lt;P&gt;penguin is correct image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L2.6.35_1.1.0_DEMO_IMAGE&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : i.MX28 Linux Binary Demo Files&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can build Gnome image in ltib, it resembles Ubuntu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L2.6.35_1.1.0_ER_SOURCE&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : i.MX28 Linux 2.6.35 Source Code &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jul 2014 15:24:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321445#M42889</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-17T15:24:51Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 linux boot problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321446#M42890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't know which linux is on SDs, however, it doesn't matter, it just doesnt work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After power on, i see only the penguin icon and black screen. nothing else happens.&lt;/P&gt;&lt;P&gt;There is no terminal or somethink which give me ability to interact with the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Someone could describe how linux boot process should look and what is the final state on the screen after booting ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to boot on linux SD card provided by producer, and also on own SD with linux created using provided DVD. Effects are the same.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jul 2014 09:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321446#M42890</guid>
      <dc:creator>wyder</dc:creator>
      <dc:date>2014-07-18T09:34:24Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 linux boot problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321447#M42891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, i have used DEBUG UART cable and HyperTerminal, i was successfull logged in as root. &lt;/P&gt;&lt;P&gt;So it is working, but on VGA Display still only penguin is visible. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is possible to install own linux build with some GUI which will appear on VGA Display? &lt;/P&gt;&lt;P&gt;In video tutorial after boot some window and folders are visible on VGA... &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jul 2014 13:08:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321447#M42891</guid>
      <dc:creator>wyder</dc:creator>
      <dc:date>2014-07-18T13:08:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 linux boot problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321448#M42892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrzej&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"GUI" is Gnome image in ltib, it resembles Ubuntu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L2.6.35_1.1.0_ER_SOURCE&lt;/A&gt; &lt;A href="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif"&gt;&lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt;&lt;/A&gt; : i.MX28 Linux 2.6.35 Source Code &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Probably you wish to try QT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="loading" href="https://community.nxp.com/message/234156#234156" title="https://community.freescale.com/message/234156#234156"&gt;https://community.freescale.com/message/234156#234156&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding "own linux build", I doubt it since i.MX28 programming&lt;/P&gt;&lt;P&gt;is not easy.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jul 2014 15:13:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321448#M42892</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-18T15:13:38Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 linux boot problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321449#M42893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I guess you could download the image[1] which you can dd directly to the SD and boot the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. &lt;A href="http://ci.ossystems.com.br/public/fsl-community-bsp/daisy/22/framebuffer/imx28evk/fsl-image-machine-test-imx28evk-20140717-22.rootfs.sdcard" title="http://ci.ossystems.com.br/public/fsl-community-bsp/daisy/22/framebuffer/imx28evk/fsl-image-machine-test-imx28evk-20140717-22.rootfs.sdcard"&gt;http://ci.ossystems.com.br/public/fsl-community-bsp/daisy/22/framebuffer/imx28evk/fsl-image-machine-test-imx28evk-201407…&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jul 2014 19:16:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321449#M42893</guid>
      <dc:creator>OtavioSalvador</dc:creator>
      <dc:date>2014-07-18T19:16:37Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 linux boot problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321450#M42894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for responses guys. Sorry for nooby questions. &lt;/P&gt;&lt;P&gt;I am C++ programmer, but I'm totally new in freescale stuff, and unfortunately I'm not too much familiar with linux... &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, let't move to merits: &lt;/P&gt;&lt;P&gt;What I finally need is working linux platform with sample program in Qt, which uses SQLite. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How is the easiest way to do it ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will try the images you posted and will write about the effcts.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jul 2014 16:59:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321450#M42894</guid>
      <dc:creator>wyder</dc:creator>
      <dc:date>2014-07-21T16:59:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 linux boot problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321451#M42895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrzej&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for starting with QT, link below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-objectid="234156" data-objecttype="2" href="https://community.nxp.com/message/234156#234156"&gt;https://community.freescale.com/message/234156#234156&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jul 2014 05:50:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321451#M42895</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-22T05:50:52Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 linux boot problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321452#M42896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for Qt link. currently i have following problems: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will try to run platform with working Eth0 and Eth1, I build image using LTIB and setup in config &lt;/P&gt;&lt;P&gt;to start Eth0, Eth1, but during boot process i have following logs: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Setting up networking on loopback device:&lt;/P&gt;&lt;P&gt;Setting up networking on eth0:&lt;/P&gt;&lt;P&gt;udhcpc (v1.15.0) started&lt;/P&gt;&lt;P&gt;ifconfig: SIOCSIFFLAGS: Cannot assign requested address&lt;/P&gt;&lt;P&gt;Sending discover...&lt;/P&gt;&lt;P&gt;udhcpc: sendto: Network is down&lt;/P&gt;&lt;P&gt;Read error: Network is down, reopening socket&lt;/P&gt;&lt;P&gt;Sending discover...&lt;/P&gt;&lt;P&gt;udhcpc: sendto: Network is down&lt;/P&gt;&lt;P&gt;Read error: Network is down, reopening socket&lt;/P&gt;&lt;P&gt;Sending discover...&lt;/P&gt;&lt;P&gt;udhcpc: sendto: Network is down&lt;/P&gt;&lt;P&gt;Read error: Network is down, reopening socket&lt;/P&gt;&lt;P&gt;No lease, forking to background&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And network doesn't work. What i am doing wrong ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jul 2014 14:43:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321452#M42896</guid>
      <dc:creator>wyder</dc:creator>
      <dc:date>2014-07-22T14:43:09Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 linux boot problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321453#M42897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrzej&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please create new thread for this new problem. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jul 2014 03:47:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-linux-boot-problem/m-p/321453#M42897</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-23T03:47:30Z</dc:date>
    </item>
  </channel>
</rss>