<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NVCC_MIPI on 3P3V in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NVCC-MIPI-on-3P3V/m-p/321424#M42887</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manuel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes your remark is correct: according to&lt;/P&gt;&lt;P&gt;i.MX6Q Datasheet NVCC_MIPI should be from 2.25 to 2.75V.&lt;/P&gt;&lt;P&gt;Please note that these boards are not Freescale boards, so question&lt;/P&gt;&lt;P&gt;should be directed to vendors of these boards.&lt;/P&gt;&lt;P&gt;Though sometimes designers just mark power rail as "3P3V",&lt;/P&gt;&lt;P&gt;really later it can be programmed to other value. I think&lt;/P&gt;&lt;P&gt;this should be investigated on real board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Jul 2014 14:11:26 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-07-17T14:11:26Z</dc:date>
    <item>
      <title>NVCC_MIPI on 3P3V</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NVCC-MIPI-on-3P3V/m-p/321423#M42886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On Wandboard and SabreLite NVCC_MIPI is connected to 3P3V.&lt;/P&gt;&lt;P&gt;The datasheet IMX6SDLIEC sets the operating ranges for NVCC_MIPI from 2.25 to 2.75V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why is there a difference?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Manuel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jul 2014 08:35:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NVCC-MIPI-on-3P3V/m-p/321423#M42886</guid>
      <dc:creator>mosmos</dc:creator>
      <dc:date>2014-07-17T08:35:01Z</dc:date>
    </item>
    <item>
      <title>Re: NVCC_MIPI on 3P3V</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NVCC-MIPI-on-3P3V/m-p/321424#M42887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manuel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes your remark is correct: according to&lt;/P&gt;&lt;P&gt;i.MX6Q Datasheet NVCC_MIPI should be from 2.25 to 2.75V.&lt;/P&gt;&lt;P&gt;Please note that these boards are not Freescale boards, so question&lt;/P&gt;&lt;P&gt;should be directed to vendors of these boards.&lt;/P&gt;&lt;P&gt;Though sometimes designers just mark power rail as "3P3V",&lt;/P&gt;&lt;P&gt;really later it can be programmed to other value. I think&lt;/P&gt;&lt;P&gt;this should be investigated on real board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jul 2014 14:11:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NVCC-MIPI-on-3P3V/m-p/321424#M42887</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-17T14:11:26Z</dc:date>
    </item>
  </channel>
</rss>