<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX35 eSDHC boot example in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX35-eSDHC-boot-example/m-p/321119#M42816</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am embarking on the journey of booting an iMX35 board from an SD card (eSDHC-1) using the internal boot mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After much investigation of the u-boot source code, it appears that I will have the dubious distinction of being the first to try this. Given the age of the iMX35, I find this surprising. However, a quick check of the latest errata turned up nothing that indicates this can't be done.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my mind, it seems that "all that needs to be done" within the first 2KB (besides filling in the HAB flash header etc) is to use eSDHC-1 to read in the remaining portion of the first stage boot loader from the SD card into internal RAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And... given that the internal boot ROM has already initialized eSDHC-1, this should be "easy"... right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have no experience with the SD command language, and finding/reading the appropriate parts of that spec is on the agenda.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But a good short-cut "alternative" is to ask this community if they already have an example for this operation... so here it is&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have any example source code for reading the next "n" blocks from the SD card (in assembler)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you,&lt;/P&gt;&lt;P&gt;mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jun 2014 18:22:38 GMT</pubDate>
    <dc:creator>michaelmoran</dc:creator>
    <dc:date>2014-06-18T18:22:38Z</dc:date>
    <item>
      <title>iMX35 eSDHC boot example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX35-eSDHC-boot-example/m-p/321119#M42816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am embarking on the journey of booting an iMX35 board from an SD card (eSDHC-1) using the internal boot mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After much investigation of the u-boot source code, it appears that I will have the dubious distinction of being the first to try this. Given the age of the iMX35, I find this surprising. However, a quick check of the latest errata turned up nothing that indicates this can't be done.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my mind, it seems that "all that needs to be done" within the first 2KB (besides filling in the HAB flash header etc) is to use eSDHC-1 to read in the remaining portion of the first stage boot loader from the SD card into internal RAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And... given that the internal boot ROM has already initialized eSDHC-1, this should be "easy"... right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have no experience with the SD command language, and finding/reading the appropriate parts of that spec is on the agenda.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But a good short-cut "alternative" is to ask this community if they already have an example for this operation... so here it is&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have any example source code for reading the next "n" blocks from the SD card (in assembler)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you,&lt;/P&gt;&lt;P&gt;mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jun 2014 18:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX35-eSDHC-boot-example/m-p/321119#M42816</guid>
      <dc:creator>michaelmoran</dc:creator>
      <dc:date>2014-06-18T18:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: iMX35 eSDHC boot example</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX35-eSDHC-boot-example/m-p/321120#M42817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for SD boot one can look at attached file and check below tests&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX35PDK&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;IMX35_SDK_LINUX_BSP_TESTS&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : IMX35 SDK LINUX BSP Validation Tests.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jun 2014 01:37:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX35-eSDHC-boot-example/m-p/321120#M42817</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-19T01:37:18Z</dc:date>
    </item>
  </channel>
</rss>