<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DNS nameserver in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DNS-nameserver/m-p/320081#M42638</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to avoid to add external script to update the resolv.conf, since it should be done from the information in the interface file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Jul 2014 00:18:40 GMT</pubDate>
    <dc:creator>niklasmolin</dc:creator>
    <dc:date>2014-07-15T00:18:40Z</dc:date>
    <item>
      <title>DNS nameserver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DNS-nameserver/m-p/320079#M42636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder how I set the DNS nameserver when using static IP.&lt;/P&gt;&lt;P&gt;I tried to include dns-nameservers in the interface file, but resolv.conf won't be updated.&lt;/P&gt;&lt;P&gt;If I use DHCP, then the resolv.conf will be updated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jul 2014 19:23:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DNS-nameserver/m-p/320079#M42636</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2014-07-14T19:23:47Z</dc:date>
    </item>
    <item>
      <title>Re: DNS nameserver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DNS-nameserver/m-p/320080#M42637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have You tried the following ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# echo nameserver 8.8.8.8 &amp;gt;&amp;gt; /etc/resolv.conf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# echo nameserver 8.8.8.8 &amp;gt; /etc/resolv.conf&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;It works under i.MX6 Ubuntu demo image.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Yuri&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jul 2014 23:58:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DNS-nameserver/m-p/320080#M42637</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-07-14T23:58:30Z</dc:date>
    </item>
    <item>
      <title>Re: DNS nameserver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DNS-nameserver/m-p/320081#M42638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to avoid to add external script to update the resolv.conf, since it should be done from the information in the interface file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jul 2014 00:18:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DNS-nameserver/m-p/320081#M42638</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2014-07-15T00:18:40Z</dc:date>
    </item>
  </channel>
</rss>