<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX287 internal DC-DC failure during boot process observed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX287-internal-DC-DC-failure-during-boot-process-observed/m-p/319963#M42618</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maik&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX28 VDDIO can not tolerate 5.3V according to&lt;/P&gt;&lt;P&gt;Table 6 "DC Absolute Maximum Ratings" datasheet&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX28CEC.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation"&gt;IMX28CEC&lt;/A&gt; &lt;/P&gt;&lt;P&gt;chip may be damaged.&lt;/P&gt;&lt;P&gt;Probably some peripheral (may be LCD ?) backs power&lt;/P&gt;&lt;P&gt;processor.&lt;/P&gt;&lt;P&gt;Also it may be recommended to add patch below (seems it as not&lt;/P&gt;&lt;P&gt;implemented in Windows CE 6.0 package)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L2.6.35_10.12_5V_SUPPLY_PATCH&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : Linux patch for i.MX28 SDK 2010.12 to&lt;/P&gt;&lt;P&gt;add the most robust support possible for a VDD5V or DCDC_BATT only configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For testing one can test board with minimum soldered components,&lt;/P&gt;&lt;P&gt;then add them one by one.&lt;/P&gt;&lt;P&gt;It is highly recommended to test with OBDS bare metal tests &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;IMX_OBDS&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : On-Board Diagnostic Suit for the i.MX28.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jun 2014 05:26:34 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-06-18T05:26:34Z</dc:date>
    <item>
      <title>i.MX287 internal DC-DC failure during boot process observed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX287-internal-DC-DC-failure-during-boot-process-observed/m-p/319962#M42617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;We have developed our own PCB with an i.MX28, using type MCIMX287CVM4B. There are 128MB DDR2 RAM are installed, which are supplied by an external dc-dc converter, as well as NAND Flash, ethernet phy, 4.3" TFT display and other periphery, also supplied external. So, the internal dc-dc converters are used for cpu interfaces, JTAG and boot mode selection only. As OS we are running Windows CE 6.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;When we put the first 24 boards into operation, we observed a strange behaviour of the internal DC-DC converter on 4 of these boards:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Case 1: The device is booting properly, but when Windows CE 6.0 switches the display mode to show the desktop, a reboot is performed, caused by internal dc-dc converter that stops switching for ~ 1ms. In consequence, VDDD drops from 1.55V to 1.15V, VDDA drops from 1.8V to 1.6V. After this pause the converter starts switching again, but all voltages rising too high (VDDD (cyan)=2.3V, VDDA (pink)=2.7V, VDDIO (green)=5.1V), while VDD4P2 (yellow) keeps 4.2V continously. It takes nearly 1 ms until all voltage rails have returned to its nominal values.&lt;/P&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="12497_12497.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119835iF76FD8C1D620951D/image-size/large?v=v2&amp;amp;px=999" role="button" title="12497_12497.png" alt="12497_12497.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="025.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43418i13CB3EC389E665A6/image-size/large?v=v2&amp;amp;px=999" role="button" title="025.png" alt="025.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="12498_12498.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119836iD4B6235009EA6F7B/image-size/large?v=v2&amp;amp;px=999" role="button" title="12498_12498.png" alt="12498_12498.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="026.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43419i18C7DA31DA2E28C3/image-size/large?v=v2&amp;amp;px=999" role="button" title="026.png" alt="026.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;In picture 2 the pink graph shows the switching node at the external inductor, pin A16, instead of VDDA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Case 2: The device is not booting at all, VDDD swings from 1.0V to 2.4V, VDDA swings from 1.8V to 2.9V and VDDIO swings from 3.3V to 5.3V.&lt;/P&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="12499_12499.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119837iB6CC2E16C9DE60A6/image-size/large?v=v2&amp;amp;px=999" role="button" title="12499_12499.png" alt="12499_12499.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="SN01424405_VDDD_1P2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43423iE1BF648D104E8E71/image-size/large?v=v2&amp;amp;px=999" role="button" title="SN01424405_VDDD_1P2.png" alt="SN01424405_VDDD_1P2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="12500_12500.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119838i4577E2FC7F0D1345/image-size/large?v=v2&amp;amp;px=999" role="button" title="12500_12500.png" alt="12500_12500.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="SN01424405_VDDA_1P8.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43524i8B9172385DB05B61/image-size/large?v=v2&amp;amp;px=999" role="button" title="SN01424405_VDDA_1P8.png" alt="SN01424405_VDDA_1P8.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="12501_12501.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119839i0878A0CCF12DA078/image-size/large?v=v2&amp;amp;px=999" role="button" title="12501_12501.png" alt="12501_12501.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="SN01424405_VDDIO_3P3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43575i4602CA18A101FE01/image-size/large?v=v2&amp;amp;px=999" role="button" title="SN01424405_VDDIO_3P3.png" alt="SN01424405_VDDIO_3P3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;In both cases we replaced the cpu with new parts and all boards were running properly. So, obvious there was no problem with our board but with some CPU's.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Did anyone of you observed the same behaviour? What could have caused these defects? A failure rate of 17% is too high to enter series production of our board with good feeling.&lt;/P&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Although we have put another 15 boards into operation in the meantime without failure, we are still wondering about these 4 defects.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Best regards,&lt;/P&gt;&lt;P style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Maik&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Message was edited by: Grant Whitacre

Maik, your images did not come through so I reproduced your discussion entry with images intact.

Regards,
Grant&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jun 2014 07:57:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX287-internal-DC-DC-failure-during-boot-process-observed/m-p/319962#M42617</guid>
      <dc:creator>maikhoelzel</dc:creator>
      <dc:date>2014-06-17T07:57:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX287 internal DC-DC failure during boot process observed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX287-internal-DC-DC-failure-during-boot-process-observed/m-p/319963#M42618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maik&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX28 VDDIO can not tolerate 5.3V according to&lt;/P&gt;&lt;P&gt;Table 6 "DC Absolute Maximum Ratings" datasheet&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX28CEC.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation"&gt;IMX28CEC&lt;/A&gt; &lt;/P&gt;&lt;P&gt;chip may be damaged.&lt;/P&gt;&lt;P&gt;Probably some peripheral (may be LCD ?) backs power&lt;/P&gt;&lt;P&gt;processor.&lt;/P&gt;&lt;P&gt;Also it may be recommended to add patch below (seems it as not&lt;/P&gt;&lt;P&gt;implemented in Windows CE 6.0 package)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L2.6.35_10.12_5V_SUPPLY_PATCH&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : Linux patch for i.MX28 SDK 2010.12 to&lt;/P&gt;&lt;P&gt;add the most robust support possible for a VDD5V or DCDC_BATT only configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For testing one can test board with minimum soldered components,&lt;/P&gt;&lt;P&gt;then add them one by one.&lt;/P&gt;&lt;P&gt;It is highly recommended to test with OBDS bare metal tests &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;IMX_OBDS&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : On-Board Diagnostic Suit for the i.MX28.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jun 2014 05:26:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX287-internal-DC-DC-failure-during-boot-process-observed/m-p/319963#M42618</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-18T05:26:34Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX287 internal DC-DC failure during boot process observed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX287-internal-DC-DC-failure-during-boot-process-observed/m-p/319964#M42619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chip,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot for your fast reply!&lt;/P&gt;&lt;P&gt;We downloaded the patch and are analyzing the source code at the moment. Obviously, this is a patch for linux. Is there also a version for Windows CE available? Or is the patch used for eboot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, we have another board found yet, that shows the same behaviour. It does not matter if the LCD is connected or not. So, we now have a hardware for approving effectiveness of this patch.&lt;/P&gt;&lt;P&gt;We will also have a look at the OBDS tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will come back with our results.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Maik&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jun 2014 15:12:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX287-internal-DC-DC-failure-during-boot-process-observed/m-p/319964#M42619</guid>
      <dc:creator>maikhoelzel</dc:creator>
      <dc:date>2014-06-19T15:12:06Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX287 internal DC-DC failure during boot process observed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX287-internal-DC-DC-failure-during-boot-process-observed/m-p/319965#M42620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maik&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think there is no such patch for Windows CE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jun 2014 04:55:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX287-internal-DC-DC-failure-during-boot-process-observed/m-p/319965#M42620</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-20T04:55:49Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX287 internal DC-DC failure during boot process observed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX287-internal-DC-DC-failure-during-boot-process-observed/m-p/319966#M42621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chip,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when we analyzed the patch for linux we found that we forgot to disable the battery as possible voltage source in our software. Because we have an external 5V supply as only source, sometimes there were a false detection of the connected power supply.&lt;/P&gt;&lt;P&gt;Now all boards are working proberly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your support!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Maik&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jul 2014 18:13:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX287-internal-DC-DC-failure-during-boot-process-observed/m-p/319966#M42621</guid>
      <dc:creator>maikhoelzel</dc:creator>
      <dc:date>2014-07-18T18:13:56Z</dc:date>
    </item>
  </channel>
</rss>