<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: armhf kernel and library support for imx6 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/armhf-kernel-and-library-support-for-imx6/m-p/319957#M42616</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm currently using a Debian Wheezy armhf, kernel 3.10.17 on a Udoo Dual Board, which is based on the imx.6DL. You can find some armhf Ubuntu or Debian rootfs on their website. They even have a Yocto to build your own rootfs, I guess you can adapt it to your board with a bit of tweaking.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So yes, it exists. I'm doing some image processing with openCV and some NEON code to speed up things a bit, and gained a little more than 30% in performance compared to a softfp test :smileyhappy: ! This is quite nice !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jun 2014 09:27:41 GMT</pubDate>
    <dc:creator>KailoKyra</dc:creator>
    <dc:date>2014-06-17T09:27:41Z</dc:date>
    <item>
      <title>armhf kernel and library support for imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/armhf-kernel-and-library-support-for-imx6/m-p/319956#M42615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are developing a IMX6DL board, and we have to run a detection algorithm over a camera image stream.&lt;/P&gt;&lt;P&gt;In order to improve the performance of execution, we are now trying to switch from the current armel build to a armhf build,&lt;/P&gt;&lt;P&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN class="hps"&gt;but&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;we have not yet&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;managed to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;achieve this.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN class="hps"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;We have found out this discussion &lt;A href="https://community.nxp.com/thread/306017"&gt;armhf libraries for imx6&lt;/A&gt; and &lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;we have not yet&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;figured out if&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN class="hps"&gt;nowadays&lt;/SPAN&gt;&lt;SPAN&gt;, support for&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;armhf&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;architecture&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;exists or not for the imx6 platform...Can anyone help us to find out?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;I thank you in advice for any help,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;Daniele&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jun 2014 08:13:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/armhf-kernel-and-library-support-for-imx6/m-p/319956#M42615</guid>
      <dc:creator>danieleaccattol</dc:creator>
      <dc:date>2014-06-17T08:13:42Z</dc:date>
    </item>
    <item>
      <title>Re: armhf kernel and library support for imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/armhf-kernel-and-library-support-for-imx6/m-p/319957#M42616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm currently using a Debian Wheezy armhf, kernel 3.10.17 on a Udoo Dual Board, which is based on the imx.6DL. You can find some armhf Ubuntu or Debian rootfs on their website. They even have a Yocto to build your own rootfs, I guess you can adapt it to your board with a bit of tweaking.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So yes, it exists. I'm doing some image processing with openCV and some NEON code to speed up things a bit, and gained a little more than 30% in performance compared to a softfp test :smileyhappy: ! This is quite nice !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jun 2014 09:27:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/armhf-kernel-and-library-support-for-imx6/m-p/319957#M42616</guid>
      <dc:creator>KailoKyra</dc:creator>
      <dc:date>2014-06-17T09:27:41Z</dc:date>
    </item>
  </channel>
</rss>