<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6 ODT Setting. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ODT-Setting/m-p/319611#M42559</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;these registers are working independently from each other (no priority).&lt;/P&gt;&lt;P&gt;And yes:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"3.&amp;nbsp; It is recommended to use only MMDC_MPODTCTRL register to configure ODT of i.MX6."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Jul 2014 23:20:37 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-07-14T23:20:37Z</dc:date>
    <item>
      <title>i.MX6 ODT Setting.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ODT-Setting/m-p/319610#M42558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about i.MX6DQ ODT.&lt;/P&gt;&lt;P&gt;Please see IOMUXC_SW_PAD_CTL_GRP_TERM_CTLx register in IMX6DQRM Rev.1.&lt;/P&gt;&lt;P&gt;These registers have "ODT" fields to determine the ODT values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand, please see MMDCx_MPODTCTRL register (chapter 44.12.38).&lt;/P&gt;&lt;P&gt;These have "ODTx_INT_RES" fields to determine the ODT values, also.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then, which registers have a priority to setting ODT value?&lt;/P&gt;&lt;P&gt;According to the following comment in &lt;A href="https://community.nxp.com/thread/326388"&gt;IMX6D ODT&lt;/A&gt;, I guess MMDCx_MPODTCTRL have a priority, is this correct?&lt;/P&gt;&lt;P&gt;"3.&amp;nbsp; It is recommended to use only MMDC_MPODTCTRL register to configure ODT of i.MX6."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jul 2014 05:44:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ODT-Setting/m-p/319610#M42558</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-07-14T05:44:40Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 ODT Setting.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ODT-Setting/m-p/319611#M42559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;these registers are working independently from each other (no priority).&lt;/P&gt;&lt;P&gt;And yes:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"3.&amp;nbsp; It is recommended to use only MMDC_MPODTCTRL register to configure ODT of i.MX6."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jul 2014 23:20:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ODT-Setting/m-p/319611#M42559</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-14T23:20:37Z</dc:date>
    </item>
  </channel>
</rss>