<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: WFI instruction in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/WFI-instruction/m-p/318916#M42431</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Takafumi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, definitely it is possible (and necessary)&lt;/P&gt;&lt;P&gt;to use WFI instruction with iMX6 Solo processor.&lt;/P&gt;&lt;P&gt;I would suggest to start search cause of this misbehaviour by narrowing&lt;/P&gt;&lt;P&gt;down possible reasons: software, hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please start with SDK low power test (SDK/apps/power_modes_test)&lt;/P&gt;&lt;P&gt;and check if it will work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX 6Series Platform SDK&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Other option - run minimal image (without GPU,VPU, GUI).&lt;/P&gt;&lt;P&gt;This may point to power supply issues (spikes, bad filtering) on power lines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 12 Jul 2014 13:59:16 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-07-12T13:59:16Z</dc:date>
    <item>
      <title>WFI instruction</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WFI-instruction/m-p/318915#M42430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chipexpert.&lt;/P&gt;&lt;P&gt; &lt;BR /&gt;After returning from WFI instruction,&amp;nbsp; 5% of our custom boards doesn't work properly.&lt;/P&gt;&lt;P&gt; &lt;BR /&gt;For example, after calling WFI instruction, &lt;/P&gt;&lt;P&gt;PWM&amp;nbsp; doesn't output any signal(always LOW or HIGH) until 1msec timer interrupt happens.&lt;/P&gt;&lt;P&gt; &lt;BR /&gt;Is there any procedure for using WFI instructnion?&lt;/P&gt;&lt;P&gt;Is it possible to use WFI instruction with iMX6 Solo processor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our BSP is "Custom Board" based Collage(by Sophia Systems Japan).&lt;/P&gt;&lt;P&gt; &lt;BR /&gt;Regards,&lt;/P&gt;&lt;P&gt;Takafumi.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jul 2014 06:21:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WFI-instruction/m-p/318915#M42430</guid>
      <dc:creator>takafuminaka</dc:creator>
      <dc:date>2014-07-11T06:21:07Z</dc:date>
    </item>
    <item>
      <title>Re: WFI instruction</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WFI-instruction/m-p/318916#M42431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Takafumi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, definitely it is possible (and necessary)&lt;/P&gt;&lt;P&gt;to use WFI instruction with iMX6 Solo processor.&lt;/P&gt;&lt;P&gt;I would suggest to start search cause of this misbehaviour by narrowing&lt;/P&gt;&lt;P&gt;down possible reasons: software, hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please start with SDK low power test (SDK/apps/power_modes_test)&lt;/P&gt;&lt;P&gt;and check if it will work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX 6Series Platform SDK&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Other option - run minimal image (without GPU,VPU, GUI).&lt;/P&gt;&lt;P&gt;This may point to power supply issues (spikes, bad filtering) on power lines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Jul 2014 13:59:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WFI-instruction/m-p/318916#M42431</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-12T13:59:16Z</dc:date>
    </item>
  </channel>
</rss>