<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Can i.MX6DL use nandwrite command to program a boot image to NAND?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-i-MX6DL-use-nandwrite-command-to-program-a-boot-image-to/m-p/318804#M42390</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi,&lt;/P&gt;&lt;P&gt;unfortunately can not, "nandwrite" command is used for jffs2 file system.&lt;/P&gt;&lt;P&gt;Freescale i.MX6 BSPs support only ubifs, while i.MX51&amp;nbsp; - jffs2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jun 2014 02:40:58 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-06-17T02:40:58Z</dc:date>
    <item>
      <title>Can i.MX6DL use nandwrite command to program a boot image to NAND?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-i-MX6DL-use-nandwrite-command-to-program-a-boot-image-to/m-p/318803#M42389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our partner tried programing a boot image to NAND (/dev/mtd0) by i.MX6DL with "nandwrite" command, but it was failed.&lt;/P&gt;&lt;P&gt;So they tried also programing with "kobs-ng", and it was succeeded.&lt;/P&gt;&lt;P&gt;On the other hand, i.MX51 could progam a boot image to NAND with "nandwrite" command.&lt;/P&gt;&lt;P&gt;So we want to know is there some restrict to use "nandwrite" with i.MX6DL.&lt;/P&gt;&lt;P&gt;Could you let me know it?&lt;/P&gt;&lt;P&gt;Or there is no restrict and some procedure of our partner was wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jun 2014 10:35:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-i-MX6DL-use-nandwrite-command-to-program-a-boot-image-to/m-p/318803#M42389</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-06-13T10:35:36Z</dc:date>
    </item>
    <item>
      <title>Re: Can i.MX6DL use nandwrite command to program a boot image to NAND?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-i-MX6DL-use-nandwrite-command-to-program-a-boot-image-to/m-p/318804#M42390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi,&lt;/P&gt;&lt;P&gt;unfortunately can not, "nandwrite" command is used for jffs2 file system.&lt;/P&gt;&lt;P&gt;Freescale i.MX6 BSPs support only ubifs, while i.MX51&amp;nbsp; - jffs2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jun 2014 02:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-i-MX6DL-use-nandwrite-command-to-program-a-boot-image-to/m-p/318804#M42390</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-17T02:40:58Z</dc:date>
    </item>
  </channel>
</rss>