<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Cinterion PH8 GSM Mobile Broadband Module Not Responding the AT Command</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Cinterion-PH8-GSM-Mobile-Broadband-Module-Not-Responding-the-AT/m-p/318700#M42353</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am currently porting Cinterion PH8 GSM Mobile Broadband Module on SabreSD Linux Kernel 3.0.35 Ubuntu 11.10。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made the follow changes to Kernel Configs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;+CONFIG_MD=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP_MULTILINK=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP_FILTER=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP_ASYNC=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP_SYNC_TTY=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP_DEFLATE=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP_BSDCOMP=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP_MPPE=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPPOE=y&lt;/P&gt;&lt;P&gt;+CONFIG_USB_SERIAL=y&lt;/P&gt;&lt;P&gt;+CONFIG_USB_SERIAL_GENERIC=y&lt;/P&gt;&lt;P&gt;+CONFIG_USB_SERIAL_OPTION=y&lt;/P&gt;&lt;P&gt;-CONFIG_CRC_CCITT=m&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and then found the device node at /dev/ttyUSB0 ~ 4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But after echo AT command to /dev/ttyUSB3: "echo -ne "AT+COPS?" &amp;gt; /dev/ttyUSB3", I did not see any response except "AT+COPS?".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used command "lsusb" to check the device info, but I can only see the VID and PID without any information of it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What else can I do now?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Jun 2014 09:47:13 GMT</pubDate>
    <dc:creator>changyuheng</dc:creator>
    <dc:date>2014-06-13T09:47:13Z</dc:date>
    <item>
      <title>Cinterion PH8 GSM Mobile Broadband Module Not Responding the AT Command</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cinterion-PH8-GSM-Mobile-Broadband-Module-Not-Responding-the-AT/m-p/318700#M42353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am currently porting Cinterion PH8 GSM Mobile Broadband Module on SabreSD Linux Kernel 3.0.35 Ubuntu 11.10。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made the follow changes to Kernel Configs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;+CONFIG_MD=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP_MULTILINK=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP_FILTER=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP_ASYNC=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP_SYNC_TTY=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP_DEFLATE=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP_BSDCOMP=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPP_MPPE=y&lt;/P&gt;&lt;P&gt;+CONFIG_PPPOE=y&lt;/P&gt;&lt;P&gt;+CONFIG_USB_SERIAL=y&lt;/P&gt;&lt;P&gt;+CONFIG_USB_SERIAL_GENERIC=y&lt;/P&gt;&lt;P&gt;+CONFIG_USB_SERIAL_OPTION=y&lt;/P&gt;&lt;P&gt;-CONFIG_CRC_CCITT=m&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and then found the device node at /dev/ttyUSB0 ~ 4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But after echo AT command to /dev/ttyUSB3: "echo -ne "AT+COPS?" &amp;gt; /dev/ttyUSB3", I did not see any response except "AT+COPS?".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used command "lsusb" to check the device info, but I can only see the VID and PID without any information of it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What else can I do now?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jun 2014 09:47:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cinterion-PH8-GSM-Mobile-Broadband-Module-Not-Responding-the-AT/m-p/318700#M42353</guid>
      <dc:creator>changyuheng</dc:creator>
      <dc:date>2014-06-13T09:47:13Z</dc:date>
    </item>
  </channel>
</rss>