<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Put a u-boot in flash memory in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Put-a-u-boot-in-flash-memory/m-p/318578#M42323</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to put a u-boot on the flash memory. I downloaded one named "u-boot.nitrogen6q" it was supposed to be a good one.I found this method to put it in the flash:&lt;/P&gt;&lt;P&gt;mmc dev 1&lt;/P&gt;&lt;P&gt;mmc read 0x10800000 0 800&lt;/P&gt;&lt;P&gt;sf probe&lt;/P&gt;&lt;P&gt;sf erase 0 0x40000&lt;/P&gt;&lt;P&gt;sf write 0x10800000 0 0x40000&lt;/P&gt;&lt;P&gt; then it should be in the flash, however, it's not and when i reboot the sabrelite, the u-boot didn't lauch and if i put a sd card with android in it, nothing happened.&lt;/P&gt;&lt;P&gt;Is it the method i use which is bad, did i forgot something or is it the u-boot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have a good link to help me to put android on the card, it would be helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alexandre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Jul 2014 15:40:14 GMT</pubDate>
    <dc:creator>alexandredel</dc:creator>
    <dc:date>2014-07-10T15:40:14Z</dc:date>
    <item>
      <title>Put a u-boot in flash memory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Put-a-u-boot-in-flash-memory/m-p/318578#M42323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to put a u-boot on the flash memory. I downloaded one named "u-boot.nitrogen6q" it was supposed to be a good one.I found this method to put it in the flash:&lt;/P&gt;&lt;P&gt;mmc dev 1&lt;/P&gt;&lt;P&gt;mmc read 0x10800000 0 800&lt;/P&gt;&lt;P&gt;sf probe&lt;/P&gt;&lt;P&gt;sf erase 0 0x40000&lt;/P&gt;&lt;P&gt;sf write 0x10800000 0 0x40000&lt;/P&gt;&lt;P&gt; then it should be in the flash, however, it's not and when i reboot the sabrelite, the u-boot didn't lauch and if i put a sd card with android in it, nothing happened.&lt;/P&gt;&lt;P&gt;Is it the method i use which is bad, did i forgot something or is it the u-boot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have a good link to help me to put android on the card, it would be helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alexandre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jul 2014 15:40:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Put-a-u-boot-in-flash-memory/m-p/318578#M42323</guid>
      <dc:creator>alexandredel</dc:creator>
      <dc:date>2014-07-10T15:40:14Z</dc:date>
    </item>
  </channel>
</rss>