<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx258 scc driver - secure ram usage</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx258-scc-driver-secure-ram-usage/m-p/318182#M42244</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please use Linux Driver as an example:&lt;/P&gt;&lt;P&gt;Chapter 19 (Security drivers) of the i.Mx25 Linux Reference manual:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jun 2014 16:25:02 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2014-06-18T16:25:02Z</dc:date>
    <item>
      <title>imx258 scc driver - secure ram usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx258-scc-driver-secure-ram-usage/m-p/318181#M42243</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you supply us a sample secure ram usage scenario for imx258? What will be the best architecture in order to use the secure ram as a keystore? We have embedded jre and the application is written in Java. Java has its own keystore mechanism to deal with public/private keys. And there is a keystore password which I suppose can be stored on imx258’s secure ram Any other opinion would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also what is the best way to use the SCC driver in linux user space as it is written in kernel space?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 12:16:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx258-scc-driver-secure-ram-usage/m-p/318181#M42243</guid>
      <dc:creator>erhan14</dc:creator>
      <dc:date>2014-06-12T12:16:53Z</dc:date>
    </item>
    <item>
      <title>Re: imx258 scc driver - secure ram usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx258-scc-driver-secure-ram-usage/m-p/318182#M42244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please use Linux Driver as an example:&lt;/P&gt;&lt;P&gt;Chapter 19 (Security drivers) of the i.Mx25 Linux Reference manual:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jun 2014 16:25:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx258-scc-driver-secure-ram-usage/m-p/318182#M42244</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2014-06-18T16:25:02Z</dc:date>
    </item>
    <item>
      <title>Re: imx258 scc driver - secure ram usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx258-scc-driver-secure-ram-usage/m-p/318183#M42245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the sample driver has nothing to do on the user space. I actually identify what is the best way using the red and black memory that is defined in sample driver.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jun 2014 09:47:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx258-scc-driver-secure-ram-usage/m-p/318183#M42245</guid>
      <dc:creator>erhan14</dc:creator>
      <dc:date>2014-06-20T09:47:00Z</dc:date>
    </item>
  </channel>
</rss>