<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx 6 sdio 3.0</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318107#M42201</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jim&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shousheng Zhao already answered regarding usage of sdio 3.0,&lt;/P&gt;&lt;P&gt;you can ask him.&lt;/P&gt;&lt;P&gt;I added comments because from customer description was not clear his&lt;/P&gt;&lt;P&gt;hardware configuration. Other users can read this thread, so I added comments for&lt;/P&gt;&lt;P&gt;clarification and avoiding confusion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Jul 2014 03:30:30 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-07-14T03:30:30Z</dc:date>
    <item>
      <title>imx 6 sdio 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318101#M42195</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the Freescale i.MX6SOLO supporting SDIO3.0 SDR104 mode ? Have any board can verify the throughput(sdio 3.0 wifi module) ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I transferred a package over 10KBytes or test by iperf.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We used the BCM module and using yocto kernel 3.10.17. I would like to know what are the missing keys in order to enable it correctly?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jul 2014 08:08:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318101#M42195</guid>
      <dc:creator>weikeng-jimmy</dc:creator>
      <dc:date>2014-07-10T08:08:45Z</dc:date>
    </item>
    <item>
      <title>Re: imx 6 sdio 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318102#M42196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jimmy Chen&lt;/P&gt;&lt;P&gt;Sorry I don't quite understand your "what are the missing keys in order to enable it", can you&amp;nbsp; explain it more specifically. thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jul 2014 09:55:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318102#M42196</guid>
      <dc:creator>JasonZhao</dc:creator>
      <dc:date>2014-07-10T09:55:56Z</dc:date>
    </item>
    <item>
      <title>Re: imx 6 sdio 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318103#M42197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sir&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I modify some devicetree setting for sdhc . What I need to pay attention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;// Booting log.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;sdhci-esdhc-imx 2194000.usdhc: Ultra high speed SDR104&lt;/P&gt;&lt;P&gt;mmc0: no vqmmc regulator found&lt;/P&gt;&lt;P&gt;mmc0: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I test throughput&lt;SPAN style="font-size: 10pt;"&gt; by iperf and get some error message .&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;mmc0: Timeout waiting for hardware interrupt.&lt;/P&gt;&lt;P&gt;dhdsdio_readframes: RXHEADER FAILED: -35&lt;/P&gt;&lt;P&gt;dhdsdio_rxfail: abort command, terminate frame, send NAK&lt;/P&gt;&lt;P&gt;dhdsdio_rxglom (superframe): len 0x0012, rounded 0x0080, expect 0x0c80&lt;/P&gt;&lt;P&gt;dhdsdio_rxfail: abort command, terminate frame, send NAK&lt;/P&gt;&lt;P&gt;dhdsdio_rxglom (superframe): len 0x1580, rounded 0x1580, expect 0x0c80&lt;/P&gt;&lt;P&gt;dhdsdio_rxfail: abort command, terminate frame, send NAK&lt;/P&gt;&lt;P&gt;dhdsdio_rxglom (superframe): len 0x0014, rounded 0x0080, expect 0x0c80&lt;/P&gt;&lt;P&gt;dhdsdio_rxfail: abort command, terminate frame, send NAK&lt;/P&gt;&lt;P&gt;dhdsdio_rxglom (superframe): len 0x1820, rounded 0x1880, expect 0x0c80&lt;/P&gt;&lt;P&gt;dhdsdio_rxfail: abort command, terminate frame&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jul 2014 01:57:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318103#M42197</guid>
      <dc:creator>weikeng-jimmy</dc:creator>
      <dc:date>2014-07-11T01:57:33Z</dc:date>
    </item>
    <item>
      <title>Re: imx 6 sdio 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318104#M42198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jimmy,&lt;/P&gt;&lt;P&gt;i.MX6 series's uSDHC supports:&lt;/P&gt;&lt;P&gt;• 1-bit or 4-bit operation for SD3.0 and SDIO 2.0 cards (so far we support SDIO v2.0(AR6003 is verified)).&lt;/P&gt;&lt;P&gt;• Support SD3.0 SDR50 and SDR104 modes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So sdio 3.0 is not supported by default,&amp;nbsp; We had the customer to enable BCM WiFi SDIO3.0 based on 3.0.35 kernel. It approved SDIO3.0 capability is fine. You can contact local support team for the issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jul 2014 09:28:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318104#M42198</guid>
      <dc:creator>JasonZhao</dc:creator>
      <dc:date>2014-07-11T09:28:28Z</dc:date>
    </item>
    <item>
      <title>Re: imx 6 sdio 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318105#M42199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JIMMY&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SDIO3.0 SDR104 mode requires switching to 1.8V SD signals,&lt;/P&gt;&lt;P&gt;which supports by Sabre-AI board. Check U508 switch&lt;/P&gt;&lt;P&gt;on SPF-27142. So your board also should support that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREAUTO&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX6_SABRE_AI_DESIGNFILES&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 13 Jul 2014 14:01:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318105#M42199</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-13T14:01:18Z</dc:date>
    </item>
    <item>
      <title>Re: imx 6 sdio 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318106#M42200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello chip,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think the customer is using SDHC2 in this case, the SD signal of the device is running at 1.8V in the beginning(no need to switch voltage), and the basic function is working(can "ping" through this WiFi card), so supposed the hardware setting is good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when running stress I/O test by "iperf", there are error messages as paste, and the vendor(Broadcom) checked the code and feedback that there should be something wrong with FSL's BSP(SD stack).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the customer is asking for:&lt;/P&gt;&lt;P&gt;1. need comment from experts regarding the error messages&lt;/P&gt;&lt;P&gt;2. has FSL ever enabled SDIO3.0 devices in Linux BSP(no matter which version)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Jim Lin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jul 2014 02:12:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318106#M42200</guid>
      <dc:creator>jim_lin</dc:creator>
      <dc:date>2014-07-14T02:12:13Z</dc:date>
    </item>
    <item>
      <title>Re: imx 6 sdio 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318107#M42201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jim&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shousheng Zhao already answered regarding usage of sdio 3.0,&lt;/P&gt;&lt;P&gt;you can ask him.&lt;/P&gt;&lt;P&gt;I added comments because from customer description was not clear his&lt;/P&gt;&lt;P&gt;hardware configuration. Other users can read this thread, so I added comments for&lt;/P&gt;&lt;P&gt;clarification and avoiding confusion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jul 2014 03:30:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318107#M42201</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-14T03:30:30Z</dc:date>
    </item>
    <item>
      <title>Re: imx 6 sdio 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318108#M42202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi sirs,&lt;/P&gt;&lt;P&gt;Do you mean they enable BCM WiFi SDIO3.0 with running in SDR104 mode under 1.8 signaling voltage, 208MHz SD clock and got expected throughput (i.e. 300Mbps? Maximum bus speed of SDR104 is 104MB/s)? Could you kindly share us which Freescale processor they used and the actual throughput? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jul 2014 01:11:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318108#M42202</guid>
      <dc:creator>starhou</dc:creator>
      <dc:date>2014-07-16T01:11:28Z</dc:date>
    </item>
    <item>
      <title>Re: imx 6 sdio 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318109#M42203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-size: 12.7272720336914px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Dear,&lt;/P&gt;&lt;P style="font-size: 12.7272720336914px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;/P&gt;&lt;P style="font-size: 12.7272720336914px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Could you please help to update for Star Hou' question? Your help will be appreciated.&lt;/P&gt;&lt;P style="font-size: 12.7272720336914px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;/P&gt;&lt;P style="font-size: 12.7272720336914px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Hi sirs,&lt;/P&gt;&lt;P style="font-size: 12.7272720336914px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Do you mean they enable BCM WiFi SDIO3.0 with running in SDR104 mode under 1.8 signaling voltage, 208MHz SD clock and got expected throughput (i.e. 300Mbps? Maximum bus speed of SDR104 is 104MB/s)? Could you kindly share us which Freescale processor they used and the actual throughput? Thanks.&lt;/P&gt;&lt;P style="font-size: 12.7272720336914px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;/P&gt;&lt;P style="font-size: 12.7272720336914px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Thanks&lt;/P&gt;&lt;P style="font-size: 12.7272720336914px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;/P&gt;&lt;P style="font-size: 12.7272720336914px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;BR&lt;/P&gt;&lt;P style="font-size: 12.7272720336914px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Keith&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Nov 2014 08:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318109#M42203</guid>
      <dc:creator>keithchang</dc:creator>
      <dc:date>2014-11-26T08:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: imx 6 sdio 3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318110#M42204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Keith,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think "enable the device" and "optimize the throughput" are two different things.&lt;/P&gt;&lt;P&gt;If the function is enabled and optimized by the customer, we can't force them to share details including the source code and test result, FYI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jim Lin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Nov 2014 03:11:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/318110#M42204</guid>
      <dc:creator>jim_lin</dc:creator>
      <dc:date>2014-11-28T03:11:24Z</dc:date>
    </item>
    <item>
      <title>This an automatic process.  We are marking this post as s...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/1135443#M161096</link>
      <description>&lt;B&gt;This an automatic process.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;
We are marking this post as solved, due to the either low activity or any reply marked as correct.&lt;BR /&gt;&lt;BR /&gt;
If you have additional questions, please create a new post and reference to this closed post.&lt;BR /&gt;&lt;BR /&gt;
NXP Community!</description>
      <pubDate>Thu, 03 Sep 2020 14:23:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-sdio-3-0/m-p/1135443#M161096</guid>
      <dc:creator>CommunityBot</dc:creator>
      <dc:date>2020-09-03T14:23:31Z</dc:date>
    </item>
  </channel>
</rss>