<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Add a package to my base distribution in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Add-a-package-to-my-base-distribution/m-p/318066#M42172</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The thing is that I do not build in SSH in the distribution. Adding the recipe in the image.bb (dropbear) works. I had the impression that I could build the package separately then install it in an already existing rootfs, maybe that's where I am mistaken?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Jun 2014 07:25:42 GMT</pubDate>
    <dc:creator>gauthier</dc:creator>
    <dc:date>2014-06-25T07:25:42Z</dc:date>
    <item>
      <title>Add a package to my base distribution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Add-a-package-to-my-base-distribution/m-p/318064#M42170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have successfully built a core-image for my Sabre-SD board.&lt;/P&gt;&lt;P&gt;Now I want to customize the image, and start simple by just adding a package.&lt;/P&gt;&lt;P&gt;I noticed I could bitbake openssh, which generated files in:&lt;/P&gt;&lt;P&gt;- build/tmp/sysroots/imx6qsabresd/usr/lib&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It generated NO files in:&lt;/P&gt;&lt;P&gt;- build/tmp/sysroots/imx6qsabresd/usr/bin&lt;/P&gt;&lt;P&gt;- build/tmp/sysroots/imx6qsabresd/usr/sbin (which does not even exist)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did try to copy the openssh-related files in lib to my SDcard, but that couldn't let me use openssh.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the recipe for openssh was there, I thought I could just bake it, and copy the generated files to my rootfs. Apparently I am wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I missing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 10:04:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Add-a-package-to-my-base-distribution/m-p/318064#M42170</guid>
      <dc:creator>gauthier</dc:creator>
      <dc:date>2014-06-12T10:04:22Z</dc:date>
    </item>
    <item>
      <title>Re: Add a package to my base distribution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Add-a-package-to-my-base-distribution/m-p/318065#M42171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you delploy the sdcard do you get the same problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94989"&gt;Task #4 - Deploy and test&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jun 2014 15:54:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Add-a-package-to-my-base-distribution/m-p/318065#M42171</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2014-06-24T15:54:10Z</dc:date>
    </item>
    <item>
      <title>Re: Add a package to my base distribution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Add-a-package-to-my-base-distribution/m-p/318066#M42172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The thing is that I do not build in SSH in the distribution. Adding the recipe in the image.bb (dropbear) works. I had the impression that I could build the package separately then install it in an already existing rootfs, maybe that's where I am mistaken?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2014 07:25:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Add-a-package-to-my-base-distribution/m-p/318066#M42172</guid>
      <dc:creator>gauthier</dc:creator>
      <dc:date>2014-06-25T07:25:42Z</dc:date>
    </item>
  </channel>
</rss>