<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックBoot from SATA ISSUES</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-from-SATA-ISSUES/m-p/317524#M42078</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;I was able to blow the fuse and see that the boot device is now SATA, but now I’m getting a “Card&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;did not respond to voltage select!” and “MMC init failed” error.&amp;nbsp; I wonder if there is something in &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;the code that is still wanting to grab code from the SD card.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Is there an easy way to blow the fuse in the Manufacturing Tool?&amp;nbsp; I tried to set it up, but being new&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;to it I was getting no ware slowly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Image attached.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Jun 2014 16:51:46 GMT</pubDate>
    <dc:creator>Chicago1984</dc:creator>
    <dc:date>2014-06-11T16:51:46Z</dc:date>
    <item>
      <title>Boot from SATA ISSUES</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-from-SATA-ISSUES/m-p/317524#M42078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;I was able to blow the fuse and see that the boot device is now SATA, but now I’m getting a “Card&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;did not respond to voltage select!” and “MMC init failed” error.&amp;nbsp; I wonder if there is something in &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;the code that is still wanting to grab code from the SD card.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Is there an easy way to blow the fuse in the Manufacturing Tool?&amp;nbsp; I tried to set it up, but being new&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;to it I was getting no ware slowly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Image attached.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 16:51:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-from-SATA-ISSUES/m-p/317524#M42078</guid>
      <dc:creator>Chicago1984</dc:creator>
      <dc:date>2014-06-11T16:51:46Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from SATA ISSUES</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-from-SATA-ISSUES/m-p/317525#M42079</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;It seems that you board is not the official reference board powered by Freescale.&lt;/P&gt;&lt;P&gt;Can you tell me where your kernel and rootfs, in SATA or SD card?&lt;/P&gt;&lt;P&gt;As with SadreSD board, booting from the SATA is supported through changing u-boot configs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 05:19:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-from-SATA-ISSUES/m-p/317525#M42079</guid>
      <dc:creator>tonyzheng</dc:creator>
      <dc:date>2014-06-12T05:19:17Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from SATA ISSUES</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-from-SATA-ISSUES/m-p/317526#M42080</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If your kernel and rootfs reside in the SATA SSD, you don't need to detect SD Card.&lt;/P&gt;&lt;P&gt;For more information, you can refer to:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/318957#318957"&gt;https://community.freescale.com/message/318957#318957&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 05:25:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-from-SATA-ISSUES/m-p/317526#M42080</guid>
      <dc:creator>tonyzheng</dc:creator>
      <dc:date>2014-06-12T05:25:39Z</dc:date>
    </item>
  </channel>
</rss>