<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックKernel support for bluez</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-support-for-bluez/m-p/317371#M42052</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have the L3 source of ltib with kernel version 3.0.35. I have been working on BLE using the bluez. Now I need to get my device into the BLE peripheral and central mode. For this I need bluez-5.x versions that doesn't seem to be compatible with the 3.0.35 kernel versio as there is no management interface support in the kernel.&lt;BR /&gt;So for this can we have some patches or we need to upgrade kernel to 3.5+. It will be better if we can get the patches, as most of the development has already been done on this kernel version and there is much difference among the both.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Jul 2014 10:51:20 GMT</pubDate>
    <dc:creator>sumitsharma</dc:creator>
    <dc:date>2014-07-08T10:51:20Z</dc:date>
    <item>
      <title>Kernel support for bluez</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-support-for-bluez/m-p/317371#M42052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have the L3 source of ltib with kernel version 3.0.35. I have been working on BLE using the bluez. Now I need to get my device into the BLE peripheral and central mode. For this I need bluez-5.x versions that doesn't seem to be compatible with the 3.0.35 kernel versio as there is no management interface support in the kernel.&lt;BR /&gt;So for this can we have some patches or we need to upgrade kernel to 3.5+. It will be better if we can get the patches, as most of the development has already been done on this kernel version and there is much difference among the both.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jul 2014 10:51:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-support-for-bluez/m-p/317371#M42052</guid>
      <dc:creator>sumitsharma</dc:creator>
      <dc:date>2014-07-08T10:51:20Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel support for bluez</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-support-for-bluez/m-p/317372#M42053</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sumit&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not think that such patches can be provided here, since&lt;/P&gt;&lt;P&gt;developing kernel patches is not minute job. Please try to work together&lt;/P&gt;&lt;P&gt;with local FAE on this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jul 2014 02:21:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-support-for-bluez/m-p/317372#M42053</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-10T02:21:22Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel support for bluez</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-support-for-bluez/m-p/317373#M42054</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using bluez 5.30 in android Kitkat 4.4.2, It's working fine and i am getting all the profiles except spp. if i try to browse spp it shows an error like "No SDP records found". Can anyone please help me to solve this problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2015 11:33:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-support-for-bluez/m-p/317373#M42054</guid>
      <dc:creator>yashwanthks</dc:creator>
      <dc:date>2015-06-03T11:33:02Z</dc:date>
    </item>
  </channel>
</rss>