<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Serial over Audio IN/Audio OUT support from audio jack.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Serial-over-Audio-IN-Audio-OUT-support-from-audio-jack/m-p/317329#M42050</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this Audio jack has only Audio Out support and not the Audio In , still Serial Tx - Rx communication is possible ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Jun 2014 10:03:24 GMT</pubDate>
    <dc:creator>pankajrana</dc:creator>
    <dc:date>2014-06-24T10:03:24Z</dc:date>
    <item>
      <title>Serial over Audio IN/Audio OUT support from audio jack.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-over-Audio-IN-Audio-OUT-support-from-audio-jack/m-p/317327#M42048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With respect to the SABRE platform's Audio interface, "&lt;SPAN lang="EN-US" style="font-family: 'Calibri','sans-serif'; color: #1f497d; font-size: 11pt;"&gt;Serial over Audio IN/Audio OUT support" is possible through the Audio Jack?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Calibri','sans-serif'; color: #1f497d; font-size: 11pt;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Calibri','sans-serif'; color: #1f497d; font-size: 11pt;"&gt;Can this feature be implemented only through software or are any hardware changes required ?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 10:35:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-over-Audio-IN-Audio-OUT-support-from-audio-jack/m-p/317327#M42048</guid>
      <dc:creator>pankajrana</dc:creator>
      <dc:date>2014-06-11T10:35:58Z</dc:date>
    </item>
    <item>
      <title>Re: Serial over Audio IN/Audio OUT support from audio jack.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-over-Audio-IN-Audio-OUT-support-from-audio-jack/m-p/317328#M42049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pankaj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes this may be performed using telephony modem algorithms.&lt;/P&gt;&lt;P&gt;Very simply put, for example using amplitude modulation:&lt;/P&gt;&lt;P&gt;Snd 1000KHz sinusoid&amp;nbsp; with amplitude "0" - means digital "0".&lt;/P&gt;&lt;P&gt;Send 1000KHz sinusoid&amp;nbsp; with max. amplitude "0xff" - means digital "1".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On receiving side one needs to decode it in software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Other more complicated methods FM modulations (such as 2400Hz - "1",&lt;/P&gt;&lt;P&gt;1200Hz - "0") one can read in V22 and other telephony modem specs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 06:37:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-over-Audio-IN-Audio-OUT-support-from-audio-jack/m-p/317328#M42049</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-12T06:37:50Z</dc:date>
    </item>
    <item>
      <title>Re: Serial over Audio IN/Audio OUT support from audio jack.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-over-Audio-IN-Audio-OUT-support-from-audio-jack/m-p/317329#M42050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this Audio jack has only Audio Out support and not the Audio In , still Serial Tx - Rx communication is possible ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jun 2014 10:03:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-over-Audio-IN-Audio-OUT-support-from-audio-jack/m-p/317329#M42050</guid>
      <dc:creator>pankajrana</dc:creator>
      <dc:date>2014-06-24T10:03:24Z</dc:date>
    </item>
    <item>
      <title>Re: Serial over Audio IN/Audio OUT support from audio jack.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-over-Audio-IN-Audio-OUT-support-from-audio-jack/m-p/317330#M42051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Surely. :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"An expert will always state the obvious."&lt;/P&gt;&lt;P&gt;[Murphy's laws]&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2014 14:12:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-over-Audio-IN-Audio-OUT-support-from-audio-jack/m-p/317330#M42051</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-25T14:12:36Z</dc:date>
    </item>
  </channel>
</rss>