<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLPDDR2 pin swapping on iMx6DL</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LPDDR2-pin-swapping-on-iMx6DL/m-p/317213#M42034</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am designing an board with a iMx6DL with 2 LPDDR2 (MT42L256M32D2) chips.&lt;/P&gt;&lt;P&gt;I noticed the LPDDR2 and DRAM pin mux mapping on page 3828 in the TRM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is bit swapping allowed on the data lines for easy pcb routing? Which are the restrictions? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Jun 2014 08:27:39 GMT</pubDate>
    <dc:creator>sebp20</dc:creator>
    <dc:date>2014-06-11T08:27:39Z</dc:date>
    <item>
      <title>LPDDR2 pin swapping on iMx6DL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPDDR2-pin-swapping-on-iMx6DL/m-p/317213#M42034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am designing an board with a iMx6DL with 2 LPDDR2 (MT42L256M32D2) chips.&lt;/P&gt;&lt;P&gt;I noticed the LPDDR2 and DRAM pin mux mapping on page 3828 in the TRM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is bit swapping allowed on the data lines for easy pcb routing? Which are the restrictions? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 08:27:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPDDR2-pin-swapping-on-iMx6DL/m-p/317213#M42034</guid>
      <dc:creator>sebp20</dc:creator>
      <dc:date>2014-06-11T08:27:39Z</dc:date>
    </item>
    <item>
      <title>Re: LPDDR2 pin swapping on iMx6DL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPDDR2-pin-swapping-on-iMx6DL/m-p/317214#M42035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Strictly speaking, JEDEC provides pad sequence standardization for LPDDR2 :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Ordering of DQ bits shall be maintained in the system, including within the &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;package and on the PCB. DQ byte swapping and DQ bit Swapping are not allowed in &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;the system. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt; And MCIMX6SLEVK design follows such approach. In the same time i.MX53 design &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;with LPDDR2&amp;nbsp; does not : byte and bit within byte swapping is applied there.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 08:52:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPDDR2-pin-swapping-on-iMx6DL/m-p/317214#M42035</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-06-11T08:52:32Z</dc:date>
    </item>
  </channel>
</rss>