<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6 DDR3 DDR21 Parameter clarification</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-DDR3-DDR21-Parameter-clarification/m-p/316425#M41918</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; In general : even through some parameters, measured on i.MX6 pins, do not&lt;/P&gt;&lt;P&gt;provide the margins,&amp;nbsp; when DDR design follows recommendations (in Hardware&lt;/P&gt;&lt;P&gt;Development Guide for i.MX6), problems should not take place, since (mainly)&lt;/P&gt;&lt;P&gt;only additional delays (because of PCB traces), common for all signals may influence&lt;/P&gt;&lt;P&gt;here. &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; As for the DDR3 timings of the i.MX6 : right now we do not have more&lt;/P&gt;&lt;P&gt;data, than provided in the Datasheet. In the future the timings may be&lt;/P&gt;&lt;P&gt;corrected, but I am afraid it will take some time.&lt;/P&gt;&lt;P&gt;&amp;nbsp; In the same time, we have duty cycle tuning register for clk and dqs, which&lt;/P&gt;&lt;P&gt;can tune the output duty cycle (~1.5%). The tuning function is (by default)&lt;/P&gt;&lt;P&gt;disabled in ddr script. But if we know how the board affect duty cycle, we can&lt;/P&gt;&lt;P&gt;apply the tuning to&amp;nbsp; compensate it. Please refer to descriptiobn of MMDC Duty&lt;/P&gt;&lt;P&gt;Cycle Control Register (MMDCx_MPDCCR).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Jul 2014 09:55:21 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2014-07-07T09:55:21Z</dc:date>
    <item>
      <title>IMX6 DDR3 DDR21 Parameter clarification</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-DDR3-DDR21-Parameter-clarification/m-p/316424#M41917</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;The DQS-CLK output from the controller is specified as +/- 0.25 CLK.&amp;nbsp; The DRAM’s input by itself allows for a maximum variation of DQS to CLK (tDQSS) of +/-0.25 CLK, which leaves zero margin for any other effects. Can you please look at the parameter called DDR21 given in the datasheet &lt;/SPAN&gt;IMX6DQIEC Rev. 2.3, 07/2013? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jul 2014 09:03:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-DDR3-DDR21-Parameter-clarification/m-p/316424#M41917</guid>
      <dc:creator>rajniks</dc:creator>
      <dc:date>2014-07-07T09:03:35Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 DDR3 DDR21 Parameter clarification</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-DDR3-DDR21-Parameter-clarification/m-p/316425#M41918</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; In general : even through some parameters, measured on i.MX6 pins, do not&lt;/P&gt;&lt;P&gt;provide the margins,&amp;nbsp; when DDR design follows recommendations (in Hardware&lt;/P&gt;&lt;P&gt;Development Guide for i.MX6), problems should not take place, since (mainly)&lt;/P&gt;&lt;P&gt;only additional delays (because of PCB traces), common for all signals may influence&lt;/P&gt;&lt;P&gt;here. &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; As for the DDR3 timings of the i.MX6 : right now we do not have more&lt;/P&gt;&lt;P&gt;data, than provided in the Datasheet. In the future the timings may be&lt;/P&gt;&lt;P&gt;corrected, but I am afraid it will take some time.&lt;/P&gt;&lt;P&gt;&amp;nbsp; In the same time, we have duty cycle tuning register for clk and dqs, which&lt;/P&gt;&lt;P&gt;can tune the output duty cycle (~1.5%). The tuning function is (by default)&lt;/P&gt;&lt;P&gt;disabled in ddr script. But if we know how the board affect duty cycle, we can&lt;/P&gt;&lt;P&gt;apply the tuning to&amp;nbsp; compensate it. Please refer to descriptiobn of MMDC Duty&lt;/P&gt;&lt;P&gt;Cycle Control Register (MMDCx_MPDCCR).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jul 2014 09:55:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-DDR3-DDR21-Parameter-clarification/m-p/316425#M41918</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-07-07T09:55:21Z</dc:date>
    </item>
  </channel>
</rss>