<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC34709 Li Cell Charger in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MC34709-Li-Cell-Charger/m-p/316234#M41879</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark&lt;/P&gt;&lt;P&gt;yes installing diode will definitely &lt;/P&gt;&lt;P&gt;fix the problem of reverse battery connection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 12px; font-family: inherit;"&gt;Best regards&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 12px; font-family: inherit;"&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Jun 2014 03:56:52 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-06-11T03:56:52Z</dc:date>
    <item>
      <title>MC34709 Li Cell Charger</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MC34709-Li-Cell-Charger/m-p/316231#M41876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the MC34709 in a design.&amp;nbsp;&amp;nbsp; We are using a 3.0V rechargeable lithium cell to backup the RTC on the MC34709.&amp;nbsp;&amp;nbsp;&amp;nbsp; I was wondering if there were any parameters or ratings on the charger circuit since it seems to be poorly documented in the datasheet.&amp;nbsp; The datasheet only lists the parameters of Table 19.&amp;nbsp;&amp;nbsp; All of the values in this table are only "Typical" values and there are no minimums or maximums listed.&amp;nbsp;&amp;nbsp;&amp;nbsp; For example for safety reasons I would like to know what the maximum charge current is.&amp;nbsp;&amp;nbsp;&amp;nbsp; Also, is there any kind of reverse charge protection built in to the charger?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If a user accidentally installs the battery in reverse, what will happen?&amp;nbsp; Will this damage the MC34709?&amp;nbsp; Will it attempt to reverse charge the cell causing leakage or worse damage to the cell?&lt;/P&gt;&lt;P&gt;If there are no protections for reverse polarity then I may need to use a permanent battery instead to remove the possibility of user error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mark Roy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 16:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MC34709-Li-Cell-Charger/m-p/316231#M41876</guid>
      <dc:creator>MarkRoy</dc:creator>
      <dc:date>2014-06-09T16:55:33Z</dc:date>
    </item>
    <item>
      <title>Re: MC34709 Li Cell Charger</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MC34709-Li-Cell-Charger/m-p/316232#M41877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark&lt;/P&gt;&lt;P&gt;Table 19 is only available official data.&lt;/P&gt;&lt;P&gt;Regarding "If a user accidentally installs the battery in reverse", battery will&lt;/P&gt;&lt;P&gt;be shorted to internal ESD diode (max. allowable current about 2mA). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 06:55:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MC34709-Li-Cell-Charger/m-p/316232#M41877</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-10T06:55:34Z</dc:date>
    </item>
    <item>
      <title>Re: MC34709 Li Cell Charger</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MC34709-Li-Cell-Charger/m-p/316233#M41878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Chip,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So are you saying then that the ESD diode would be able to handle a reverse battery?&amp;nbsp; &lt;/P&gt;&lt;P&gt;Or would this kill the ESD diode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I put a low voltage schottky diode from LICELL (pin M2) to the cell, would this fix the problem of reverse charging or would the charger then have problems correctly sensing the voltage? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mark Roy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 16:52:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MC34709-Li-Cell-Charger/m-p/316233#M41878</guid>
      <dc:creator>MarkRoy</dc:creator>
      <dc:date>2014-06-10T16:52:50Z</dc:date>
    </item>
    <item>
      <title>Re: MC34709 Li Cell Charger</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MC34709-Li-Cell-Charger/m-p/316234#M41879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark&lt;/P&gt;&lt;P&gt;yes installing diode will definitely &lt;/P&gt;&lt;P&gt;fix the problem of reverse battery connection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 12px; font-family: inherit;"&gt;Best regards&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 12px; font-family: inherit;"&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 03:56:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MC34709-Li-Cell-Charger/m-p/316234#M41879</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-11T03:56:52Z</dc:date>
    </item>
  </channel>
</rss>