<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: To find the root cause of i.MX6Q IPU error interrupt. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315813#M41734</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chipexpert,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Table 37-35 shows these error are occurred SMFC or IDMAC, so I guessed this is camera input performance issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;According to your reply, are these error "IPU_INT_STAT5[0] and "IPU_INT_STAT10[0]" also occurred by not only camera input performance but also system memory bandwidth?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Jun 2014 04:15:00 GMT</pubDate>
    <dc:creator>satoshishimoda</dc:creator>
    <dc:date>2014-06-10T04:15:00Z</dc:date>
    <item>
      <title>To find the root cause of i.MX6Q IPU error interrupt.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315811#M41732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about i.MX6Q IPU.&lt;/P&gt;&lt;P&gt;Please see Table 37-35 in IMX6DQRM Rev.1.&lt;/P&gt;&lt;P&gt;Sometimes IPU_INT_STAT5[0] and IPU_INT_STAT10[0] is occurred on a custom board.&lt;/P&gt;&lt;P&gt;These interrupts seem that these are generated by input data from CSI, so we checked whether input data from camera is over &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;the i.MX6Q CSI spec, but the input data is smaller than the maximum spec of CSI sufficiently. (camera data: 1920x1080@30fps BT.1120) &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;And they have already set IPUx_HSP_CLK_ROOT to large value adequately (264MHz), so we think the root cause is not &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;performance of CSI.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In this case, could you give me a advice what should we check to find root cause?&lt;/P&gt;&lt;P&gt;(e.g. we should check the signal integrity of camera data, IPU output IPU_INT_STAT5[0] or IPU_INT_STAT10[0] if memory &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;bandwitdh is not sufficient, etc..)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your information, IPU is used to output 320x240 10fps also.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 05:52:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315811#M41732</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-06-09T05:52:37Z</dc:date>
    </item>
    <item>
      <title>Re: To find the root cause of i.MX6Q IPU error interrupt.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315812#M41733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi,&lt;/P&gt;&lt;P&gt;you are right, this is performance issue as described in link below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/320553#320553"&gt;https://community.freescale.com/message/320553#320553&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please understand that this is specific application issue - &lt;/P&gt;&lt;P&gt;that is, this depends on customers configuration.&lt;/P&gt;&lt;P&gt;Issue may be solved by finding source of bandwidth limitation:&lt;/P&gt;&lt;P&gt;you can start test with SDK, then with Linux min. configuration.&lt;/P&gt;&lt;P&gt;Then, adding drivers one by one, you can find when error will start to appear:&lt;/P&gt;&lt;P&gt;this will be source of this error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 03:18:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315812#M41733</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-10T03:18:18Z</dc:date>
    </item>
    <item>
      <title>Re: To find the root cause of i.MX6Q IPU error interrupt.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315813#M41734</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chipexpert,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Table 37-35 shows these error are occurred SMFC or IDMAC, so I guessed this is camera input performance issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;According to your reply, are these error "IPU_INT_STAT5[0] and "IPU_INT_STAT10[0]" also occurred by not only camera input performance but also system memory bandwidth?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 04:15:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315813#M41734</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-06-10T04:15:00Z</dc:date>
    </item>
    <item>
      <title>Re: To find the root cause of i.MX6Q IPU error interrupt.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315814#M41735</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes I agree with you.&lt;/P&gt;&lt;P&gt;One can try to reserve more memory to IPU tasks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="loading" href="https://community.nxp.com/docs/DOC-93591" title="https://community.freescale.com/docs/DOC-93591"&gt;https://community.freescale.com/docs/DOC-93591&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;or use more new 3.10.17 kernel which has better memory&lt;/P&gt;&lt;P&gt;management&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L3.10.17_1.0.0_IMX6QDLS_BUNDLE&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 07:44:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315814#M41735</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-10T07:44:25Z</dc:date>
    </item>
    <item>
      <title>Re: To find the root cause of i.MX6Q IPU error interrupt.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315815#M41736</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chip,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We changed the resolution of camera input from 1080p to VGA to reduce load for memory.&lt;/P&gt;&lt;P&gt;But these error have remained yet.&lt;/P&gt;&lt;P&gt;So we think these error are not performance issue.&lt;/P&gt;&lt;P&gt;Do you think so?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your information, the following messages are log when the error was occurred.&lt;/P&gt;&lt;P&gt;=====&lt;/P&gt;&lt;P&gt;[pattern 1]&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: mxc_v4l_dqueue() interrupt received&lt;/P&gt;&lt;P&gt;Segmentation fault&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00000001&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[pattern 2]&lt;/P&gt;&lt;P&gt;Segmentation fault&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00000001&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[pattern 3]&lt;/P&gt;&lt;P&gt;VPU interrupt received.&lt;/P&gt;&lt;P&gt;imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00000001&lt;/P&gt;&lt;P&gt;Segmentation fault&lt;/P&gt;&lt;P&gt;=====&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We can find "Segmentation fault" in all patterns.&lt;/P&gt;&lt;P&gt;So we doubt it as the root cause.&lt;/P&gt;&lt;P&gt;Could you let me know what module output "Segmentation fault" and when output it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 10:34:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315815#M41736</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-06-10T10:34:22Z</dc:date>
    </item>
    <item>
      <title>Re: To find the root cause of i.MX6Q IPU error interrupt.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315816#M41737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you can, could you let me know the root cause of the above 3 patterns error?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 10:08:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315816#M41737</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-06-11T10:08:21Z</dc:date>
    </item>
    <item>
      <title>Re: To find the root cause of i.MX6Q IPU error interrupt.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315817#M41738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi,&lt;/P&gt;&lt;P&gt;to answer your question&lt;/P&gt;&lt;P&gt;it is necessary to check this issue on our side.&lt;/P&gt;&lt;P&gt;Could you tell steps, how this issue can be reproduced&lt;/P&gt;&lt;P&gt;on Freescale reference board with Freescale BSPs ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW had you chance to try new 3.10.17 kernel&lt;/P&gt;&lt;P&gt;which has much better memory management ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L3.10.17_1.0.0_IMX6QDLS_BUNDLE&lt;/A&gt; &lt;A data-content-finding="Community" href="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif"&gt;&lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt;&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 10:55:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315817#M41738</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-11T10:55:47Z</dc:date>
    </item>
    <item>
      <title>Re: To find the root cause of i.MX6Q IPU error interrupt.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315818#M41739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chip,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, we cannot reproduce this issue with SABRE board because SABRE board cannot receive BT.1120.&lt;/P&gt;&lt;P&gt;So could you reply to our simple question one by one to investigate what is the root cause of this issue?&lt;/P&gt;&lt;P&gt;At first,&amp;nbsp; our first simple question is "Could you let me know what module output "Segmentation fault" and when output it?"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 08:38:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315818#M41739</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-06-12T08:38:34Z</dc:date>
    </item>
    <item>
      <title>Re: To find the root cause of i.MX6Q IPU error interrupt.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315819#M41740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regarding "what module output "Segmentation fault" and when output it" -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it outputs by IPU, when - please look below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://en.wikipedia.org/wiki/Segmentation_fault" title="http://en.wikipedia.org/wiki/Segmentation_fault"&gt;Segmentation fault - Wikipedia, the free encyclopedia&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you post this issue&amp;nbsp; to meta-fsl-arm mailing list, so that someone familiar with&lt;/P&gt;&lt;P&gt;IPU "Segmentation fault" errors could try to assist you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://lists.yoctoproject.org/listinfo/meta-freescale"&gt;https://lists.yoctoproject.org/listinfo/meta-freescale&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also did you check below patch&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/356584"&gt;Support BT1120 progressive mode in Mx6Q&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 11:55:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315819#M41740</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-12T11:55:53Z</dc:date>
    </item>
    <item>
      <title>Re: To find the root cause of i.MX6Q IPU error interrupt.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315820#M41741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chip,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=====&lt;/P&gt;&lt;P&gt;&amp;gt; it outputs by IPU, when - please look below&lt;/P&gt;&lt;P&gt;&amp;gt; Segmentation fault - Wikipedia, the free encyclopedia&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you know, could you let me know what source code in BSP (L3.0.35_4.1.0) output the "Segmentation fault" also?&lt;/P&gt;&lt;P&gt;=====&lt;/P&gt;&lt;P&gt;&amp;gt; Could you post this issue&amp;nbsp; to meta-fsl-arm mailing list, so that someone familiar with&lt;/P&gt;&lt;P&gt;&amp;gt; IPU "Segmentation fault" errors could try to assist you.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;gt;&amp;nbsp; &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://lists.yoctoproject.org/listinfo/meta-freescal"&gt;https://lists.yoctoproject.org/listinfo/meta-freescal&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry, I don't know what is the mailing list and don't know how to use.&lt;/P&gt;&lt;P&gt;=====&lt;/P&gt;&lt;P&gt;&amp;gt; Also did you check below patch&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&amp;gt;&amp;nbsp; &lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-content-finding="Community" data-objectid="356584" data-objecttype="2" href="https://community.nxp.com/message/356584#356584" style="font-weight: inherit; font-style: inherit; font-family: inherit; color: #6a737b;"&gt;Support BT1120 progressive mode in Mx6Q&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your information, out partner have already applied&amp;nbsp; the below patch.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-content-finding="Community" data-objectid="356584" data-objecttype="2" href="https://community.nxp.com/message/356584#356584" style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #6a737b;"&gt;Support BT1120 progressive mode in Mx6Q&lt;/A&gt;&lt;/P&gt;&lt;P&gt;=====&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jun 2014 05:38:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315820#M41741</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-06-16T05:38:45Z</dc:date>
    </item>
    <item>
      <title>Re: To find the root cause of i.MX6Q IPU error interrupt.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315821#M41742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi,&lt;/P&gt;&lt;P&gt;when one goes on link below, there you will be prompted to enter e-mail&lt;/P&gt;&lt;P&gt;&lt;A class="loading" href="https://lists.yoctoproject.org/listinfo/meta-freescale" title="https://lists.yoctoproject.org/listinfo/meta-freescale"&gt;https://lists.yoctoproject.org/listinfo/meta-freescale&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Regarding :&lt;/P&gt;&lt;P&gt;"If you know, could you let me know what source code in BSP (L3.0.35_4.1.0) output the&lt;/P&gt;&lt;P&gt;"Segmentation fault" also?"&lt;/P&gt;&lt;P&gt;- sorry, it is impossible to say in which on many thousands of Linux instructions&lt;/P&gt;&lt;P&gt;this error happens.&lt;/P&gt;&lt;P&gt;Actually, as you correctly noted, this case is not supported in Freescale Linux BSPs&lt;/P&gt;&lt;P&gt;and it is not possible to reproduce it on Freescale boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can post issue on this mailing list, there&lt;/P&gt;&lt;P&gt;i.MX developers are working and they know many typical errors, they may help.&lt;/P&gt;&lt;P&gt;Alternatively you can apply to FPS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="loading" href="http://cache.freescale.com/files/training/doc/ftf/2014/FTF-SDS-F0251.pdf" title="http://cache.freescale.com/files/training/doc/ftf/2014/FTF-SDS-F0251.pdf"&gt;http://cache.freescale.com/files/training/doc/ftf/2014/FTF-SDS-F0251.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jun 2014 16:13:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/To-find-the-root-cause-of-i-MX6Q-IPU-error-interrupt/m-p/315821#M41742</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-16T16:13:56Z</dc:date>
    </item>
  </channel>
</rss>