<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using all 4 i.MX53x USB ports? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-all-4-i-MX53x-USB-ports/m-p/164691#M4172</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The docs tout that the i.MX53 devices have 4 USB ports. Has anyone actually been able to get all 4 four to work?&lt;/P&gt;&lt;P&gt;When we have asked for app notes or examples, we are pointed to other products or to a design that adds a hub to extend the 1 host on the QSB into 3 hubs.&lt;/P&gt;&lt;P&gt;Is the four USB port claim bogus?&lt;/P&gt;&lt;P&gt;We cannot even find an example (we have asked technical support) of any i.MX53 implementation of the USB PHY interfaces.&lt;/P&gt;&lt;P&gt;Thanks for any feedback.&lt;/P&gt;&lt;P&gt;-Ted&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 May 2012 20:54:30 GMT</pubDate>
    <dc:creator>TedMichon</dc:creator>
    <dc:date>2012-05-30T20:54:30Z</dc:date>
    <item>
      <title>Using all 4 i.MX53x USB ports?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-all-4-i-MX53x-USB-ports/m-p/164691#M4172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The docs tout that the i.MX53 devices have 4 USB ports. Has anyone actually been able to get all 4 four to work?&lt;/P&gt;&lt;P&gt;When we have asked for app notes or examples, we are pointed to other products or to a design that adds a hub to extend the 1 host on the QSB into 3 hubs.&lt;/P&gt;&lt;P&gt;Is the four USB port claim bogus?&lt;/P&gt;&lt;P&gt;We cannot even find an example (we have asked technical support) of any i.MX53 implementation of the USB PHY interfaces.&lt;/P&gt;&lt;P&gt;Thanks for any feedback.&lt;/P&gt;&lt;P&gt;-Ted&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2012 20:54:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-all-4-i-MX53x-USB-ports/m-p/164691#M4172</guid>
      <dc:creator>TedMichon</dc:creator>
      <dc:date>2012-05-30T20:54:30Z</dc:date>
    </item>
    <item>
      <title>Re: Using all 4 i.MX53x USB ports?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-all-4-i-MX53x-USB-ports/m-p/164692#M4173</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You should take a look on QSB schematics, I´m pretty sure QSB hardware cannot handle 4 USB port because there is some USB pins used for another&amp;nbsp;purpose.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you would need another hardware project to explore all 4 USB, and understand the IOMUXing for they.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 May 2012 13:27:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-all-4-i-MX53x-USB-ports/m-p/164692#M4173</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2012-05-31T13:27:55Z</dc:date>
    </item>
    <item>
      <title>Re: Using all 4 i.MX53x USB ports?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-all-4-i-MX53x-USB-ports/m-p/164693#M4174</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Access to 2 of the 4 USB ports require external USB PHYs and the QSB does not have any.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-Ted&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jun 2012 15:25:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-all-4-i-MX53x-USB-ports/m-p/164693#M4174</guid>
      <dc:creator>TedMichon</dc:creator>
      <dc:date>2012-06-04T15:25:18Z</dc:date>
    </item>
    <item>
      <title>Re: Using all 4 i.MX53x USB ports?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-all-4-i-MX53x-USB-ports/m-p/164694#M4175</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i.MX53 do have 4 USB port, 1 OTG and 3 for HOST. And OTG and Host3 have intergated phy within the chip, while Host1, and Host2 has no intergareted phy, but a phy interface which can connected with extern phy or hub&amp;nbsp;were provided. Please refer i.MX53_EVK board for detail, (the hub USB2517 was used.).&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jun 2012 05:37:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-all-4-i-MX53x-USB-ports/m-p/164694#M4175</guid>
      <dc:creator>JerryFan</dc:creator>
      <dc:date>2012-06-15T05:37:38Z</dc:date>
    </item>
    <item>
      <title>Re: Using all 4 i.MX53x USB ports?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-all-4-i-MX53x-USB-ports/m-p/164695#M4176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are echoing my observation that the only way we have seen an i.MX53 4 USB solution implemented used a HUB to extend one of the internal USBs. We have never seen a design that uses the 4 internal ports nor one that adds an external PHY. Also, the external PHY connections listed on the IOMux tool are NOT for the minimal 12 pin PHY interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To repeat, there are NO documented examples of all 4 internal USB ports in use!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-Ted&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jun 2012 15:33:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-all-4-i-MX53x-USB-ports/m-p/164695#M4176</guid>
      <dc:creator>TedMichon</dc:creator>
      <dc:date>2012-06-18T15:33:32Z</dc:date>
    </item>
  </channel>
</rss>