<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Re: Re: Re: MX6Q+LPDDR2(32bit) boot issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315536#M41657</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ofer,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I took a quick look at your schematic and layout files. Two things jumped out at me:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Bulk capacitance on NVCC_PLL_OUT. The Hardware User Guide recommends a minimum value of 10 uF, and I actually have a 22 uF capacitor on the SABRE SDB board. NVCC_PLL_OUT is the pin connected to the output side of the LDO_1p1 internal regulator which supplies a number of critical items in the SNVS domain: Chief among them is the clock generating block (CCM). Without the bulk capacitor, you run the risk of increased jitter on all of your clocks. Jitter is a very likely suspect in this case. It would tend to explain why one frequency would work better than another, and the effects of jitter become more pronounce with higher frequency operations. It may be that with the Linux kernal running, the increased loading on NVCC_PLL_OUT is causing issues that are not seen with the DDR Stress test, due to the presence of higher jitter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Recommendation: Try soldering a 10 uF capacitor on top of C242 underneath the processor and see if this makes your errors go away.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jitter is cumulative and can be also be decreased by lowering the drive strengths on your DDR pads. I don't think the high drive strengths you are using are causing the problems by themselves, but if you lower DSE to a setting of 0x28, you might see some additional improvement if jitter is your only problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) One bulk capacitors for each of VDDARM_CAP, VDDSOC_CAP, VDDPU, and LPDDR_1V2 should be place directly underneath the processor. (The Hardware User Guide recommends a maximum distance of 50 mils to processor pin. Testing has shown that outside the boundaries of the processor is really too far away. That was specifically on the VDDSOC_CAP that was causing problems, but the bulk cap for LPDDR_1V2 being far away would definately be a major cause of jitter on the DDR pads, coupled with the high drive strengths. VDDSOC_CAP actually supplies the logic levels for the MMDC signals, so increased demand on VDDSOC_CAP could be causing problems in the MMDC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Recommendation: Try soldering a 22 uF capacitor on top of the following decoupling caps:&lt;/P&gt;&lt;P&gt;- C171&lt;/P&gt;&lt;P&gt;- C213&lt;/P&gt;&lt;P&gt;- C222&lt;/P&gt;&lt;P&gt;- C131&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think if you try adding these capacitors, you should be able to tell very quickly if they are helping or not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Dec 2014 00:51:14 GMT</pubDate>
    <dc:creator>TheAdmiral</dc:creator>
    <dc:date>2014-12-04T00:51:14Z</dc:date>
    <item>
      <title>MX6Q+LPDDR2(32bit) boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315479#M41600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As I mentioned in some threads, we are trying on MX6Q+LPDDR2 combined design. but make no sense why boot failure in mfg bootimage.&lt;/P&gt;&lt;P&gt;We use Mx6DQSDL LPDDR2 Script Aid V0.04.xlsx to generate flashheader DCD part (attached file 6q_lpddr2_32.inc). The Samsung eMCP&lt;/P&gt;&lt;P&gt;DS attched,too.&lt;/P&gt;&lt;P&gt;Our DDR config:&lt;/P&gt;&lt;P&gt;Single Channel 32bit&lt;/P&gt;&lt;P&gt;2CS, each cs is 128Mx32 (totally 1GB)&lt;/P&gt;&lt;P&gt;With default DSE 40ohm (SI configuration in Mx6DQSDL LPDDR2 Script Aid V0.04.xlsx ), 400MHz DDR stress test failure, but it's okay change them&lt;/P&gt;&lt;P&gt;to 34ohm. But with this stress pass DCD, my uboot_mfg can't boot properly (no output in default console).&lt;/P&gt;&lt;P&gt;Please help us!&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336254"&gt;6q_lpddr2_32.inc.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336254"&gt;mx6q_tdh_lpddr2_400_v004.inc.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jun 2014 02:45:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315479#M41600</guid>
      <dc:creator>raymondwang</dc:creator>
      <dc:date>2014-06-06T02:45:43Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2 boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315480#M41601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raymond&lt;/P&gt;&lt;P&gt;suggest to build just Uboot (not MFG) and try to boot it,&lt;/P&gt;&lt;P&gt;flash_header.S should be modified with new DCD settings.&lt;/P&gt;&lt;P&gt;Regarding MFG Tool, its firmware (initramfs.cpio.gz.uboot)&lt;/P&gt;&lt;P&gt;should be rebuilt with new DCD, please check&lt;/P&gt;&lt;P&gt;i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf&lt;/P&gt;&lt;P&gt;sect.3.9 "Building Manufacturing Firmware".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fasp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation"&gt;L3.0.35_4.1.0_LINUX_DOCS&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually you can download just modified Uboot with MFG Tool,&lt;/P&gt;&lt;P&gt;modifiy ucl2.xml (also one can create new Profile, check with MFG2 Tool documentation).&lt;/P&gt;&lt;P&gt;u-boot-mx6q-sabresd_nopad.bin is Uboot image&amp;nbsp; without offset (0x400).&lt;/P&gt;&lt;P&gt;Note, for USB loading one needs the same images, but without offset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Changed "SabreSD-SD" profile:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;LIST name="SabreSD-SD" desc="USB SDP"&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;CMD state="BootStrap" type="boot" body="BootStrap" file ="u-boot-mx6q-sabresd_nopad.bin" &amp;gt;Loading image&amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;CMD state="BootStrap" type="jump" &amp;gt; Jumping to image. &amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;CMD state="Updater" type="push" body="$ echo Load Complete!"&amp;gt;Done&amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;/LIST&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Windows platform for creating Uboot image without offset, "dd" &lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;utility may be used (&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.chrysocome.net/dd):"&gt;http://www.chrysocome.net/dd):&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;dd.exe if=u-boot-mx6q-sabresd.bin of=u-boot-mx6q-sabresd_nopad.bin&amp;nbsp; bs=1024 skip=1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jun 2014 10:25:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315480#M41601</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-06T10:25:41Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2 boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315481#M41602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/igorpadykov"&gt;igorpadykov&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.I use different profile to test my mfg uboot.&lt;/P&gt;&lt;P&gt;&amp;lt;LIST name="Android-TDH-eMMC" desc="Choose eMMC android as media"&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;lt;CMD state="BootStrap" type="boot" body="BootStrap" file ="u-boot-mx6q-tdh-lpddr2_nopad.bin" &amp;gt;Loading U-boot&amp;lt;/CMD&amp;gt; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;CMD state="BootStrap" type="jump" &amp;gt; Jumping to OS image. &amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&amp;nbsp; &amp;lt;CMD state="Updater" type="push" body="$ echo Load Complete!"&amp;gt;Done&amp;lt;/CMD&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;/LIST&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; 2.Following your instruction, I cut first 1k bytes of my mfg uboot&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;dd if=u-boot-mx6q-tdh-lpddr2.bin of=u-boot-mx6q-tdh-lpddr2_nopad.bin bs=1024 skip=1&lt;/P&gt;&lt;P&gt;142+1 records in&lt;/P&gt;&lt;P&gt;142+1 records out&lt;/P&gt;&lt;P&gt;146332 bytes (146 kB) copied, 0.00187831 s, 77.9 MB/s&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; Still there is no message output in uart console.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jun 2014 11:23:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315481#M41602</guid>
      <dc:creator>raymondwang</dc:creator>
      <dc:date>2014-06-06T11:23:18Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2 boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315482#M41603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I also have a double check on existed mfg u-boot-mx6q-sabresd.bin. It contains first 1k padding bytes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jun 2014 11:28:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315482#M41603</guid>
      <dc:creator>raymondwang</dc:creator>
      <dc:date>2014-06-06T11:28:35Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2 boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315483#M41604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raymond&lt;/P&gt;&lt;P&gt;could you try to rebuild just Linux Uboot&lt;/P&gt;&lt;P&gt;(not Android) and try ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L3.0.35_4.1.0_ER_SOURCE_BSP&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually does board output anything ?&lt;/P&gt;&lt;P&gt;Did you try SDK ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX 6Series Platform SDK&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jun 2014 11:31:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315483#M41604</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-06T11:31:38Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2 boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315484#M41605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, there is nothing output in uart1 (1st uart). Are you sure that rebuild uboot source useful?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jun 2014 11:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315484#M41605</guid>
      <dc:creator>raymondwang</dc:creator>
      <dc:date>2014-06-06T11:35:54Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2 boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315485#M41606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raymond&lt;/P&gt;&lt;P&gt;suggest to start with SDK and oscilloscope&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX 6Series Platform SDK&lt;/A&gt; &lt;A href="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif"&gt;&lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt;&lt;/A&gt; :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Jun 2014 14:53:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315485#M41606</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-07T14:53:15Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2(32bit) boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315486#M41607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear chipexpert,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Thanks for your response! I checked iMX6 platform sdk, it does not contains LPDDR2 single channel DCD for MX6Q series boards.&lt;/P&gt;&lt;P&gt;MX6Q EVB -&amp;gt;2GB DDR3 @64bit single channel &lt;/P&gt;&lt;P&gt;MX6Q Sabre_ai -&amp;gt;DDR3&lt;/P&gt;&lt;P&gt;MX6Q Sabre_SmartDevice -&amp;gt;DDR3&lt;/P&gt;&lt;P&gt; I don't have JTAG tool,therefore I have to fix my DCD for DDR initialization issue. &lt;/P&gt;&lt;P&gt; BTW,my board DDR signal is routed in inner layer. Probably routing not good enough, we can't run memory stress test pass in 432MHz or &lt;/P&gt;&lt;P&gt;above.&lt;/P&gt;&lt;P&gt; My question is , DDR stress test pass in 400MHz, Why it fails to bringup LPDDR2 using same DCD config?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RaymondW&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 08 Jun 2014 06:50:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315486#M41607</guid>
      <dc:creator>raymondwang</dc:creator>
      <dc:date>2014-06-08T06:50:01Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2(32bit) boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315487#M41608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raymond&lt;/P&gt;&lt;P&gt;you can add to DCD (and Uboot) code to set some GPIO,&lt;/P&gt;&lt;P&gt;then check where code hangs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 08 Jun 2014 15:40:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315487#M41608</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-08T15:40:12Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2(32bit) boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315488#M41609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Chip&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I tried to enable 1 gpio to light on a LED, seems failure . I think this means cpu did not&lt;/P&gt;&lt;P&gt;run there.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; BTW, I found a DCD data to enable DDR 400MHz:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; setmem /32 0x020c4018 = 0x00060324&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Is it right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RaymondWang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 01:40:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315488#M41609</guid>
      <dc:creator>raymondwang</dc:creator>
      <dc:date>2014-06-09T01:40:01Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2(32bit) boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315489#M41610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;Hi Raymond&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;suggest to verify that GPIO module clock is not&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;gated in CCM registers (CCM_CCGR).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;Best regards&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 03:55:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315489#M41610</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-09T03:55:48Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2(32bit) boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315490#M41611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I Add the gpio code in uboot since DCD can't access gpio module directly.&lt;/P&gt;&lt;P&gt;I test my uboot with sabresd DDR3 config, it does work. &lt;/P&gt;&lt;P&gt;&amp;nbsp; Only one CCM register is set in DCD,&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt; setmem /32 0x020c4018 = 0x00060324&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt; I don't think it relevant to GPIO required clocks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&amp;nbsp; I doubt DCD ccm register setting not enough to let LPDDR2 working at 400MHz. Our board&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;can't pass 528MHz DDR stress test.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 04:07:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315490#M41611</guid>
      <dc:creator>raymondwang</dc:creator>
      <dc:date>2014-06-09T04:07:01Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2 boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315491#M41612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raymond&lt;/P&gt;&lt;P&gt;you can try other settings as below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/312033"&gt;iMX6DQ LPDDR2 Initialization Issue&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;Best regards&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 08:07:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315491#M41612</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-09T08:07:14Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2(32bit) boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315492#M41613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried ,same behavior as before. and that init script is 533MHz, running DDR stress test will fail. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 08:43:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315492#M41613</guid>
      <dc:creator>raymondwang</dc:creator>
      <dc:date>2014-06-09T08:43:05Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2(32bit) boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315493#M41614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raymond&lt;/P&gt;&lt;P&gt;what BSP are you using ?&lt;/P&gt;&lt;P&gt;What documents (if any) are you reading when&lt;/P&gt;&lt;P&gt;preparing images ?&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;Best regards&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 09:23:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315493#M41614</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-09T09:23:06Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2(32bit) boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315494#M41615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;my bsp is Android4.2.2-1.1.0-GA And my board design is based on SabreSD ( but using different DDR and PMIC).&lt;/P&gt;&lt;P&gt;Mine is LPDD2 and PMIC is PF0100F1 (specially for LPDDR2 application)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 09:36:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315494#M41615</guid>
      <dc:creator>raymondwang</dc:creator>
      <dc:date>2014-06-09T09:36:28Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2(32bit) boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315495#M41616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raymond&lt;/P&gt;&lt;P&gt;I would suggest to use Linux or even SDK&lt;/P&gt;&lt;P&gt;at bring-up phase. They are simpler, better documented,&lt;/P&gt;&lt;P&gt;easier for debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L3.0.35_4.1.0_ER_SOURCE_BSP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX 6Series Platform SDK&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;Best regards&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 09:45:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315495#M41616</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-09T09:45:09Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q+LPDDR2(32bit) boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315496#M41617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am not familiar on linux or mx6 SDK. But I reviewed sdk source tree, no instinct difference between SDK and UBOOT stand for &lt;/P&gt;&lt;P&gt;board dcd configuration.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 10:31:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315496#M41617</guid>
      <dc:creator>raymondwang</dc:creator>
      <dc:date>2014-06-09T10:31:05Z</dc:date>
    </item>
    <item>
      <title>Re: Re: MX6Q+LPDDR2(32bit) boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315497#M41618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I rebuild sdk_unit_test_ALL.bin with replacing smart_device dcd.c to my LPDDR2.&lt;/P&gt;&lt;P&gt;And add it to mfg tool&lt;/P&gt;&lt;P&gt;&amp;lt;LIST name="DWLD_IN_SDP" desc="Download and execute a binary!"&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;CMD state="BootStrap"&amp;nbsp; type="find" body="Recovery" timeout="180"/&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;CMD state="BootStrap" type="boot" body="Recovery" file="sdk_unit_test_ALL.bin"&amp;gt;Loading&lt;/P&gt;&lt;P&gt;SDK image&amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;CMD state="BootStrap" type="jump"&amp;gt;Jumping to SDK image.&amp;lt;/CMD&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;/LIST&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The mfgtool hangs with display state in "Loading SDK image" about 75% over 5mins.&lt;/P&gt;&lt;P&gt;I enclosed my new dcd.c.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 04:15:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315497#M41618</guid>
      <dc:creator>raymondwang</dc:creator>
      <dc:date>2014-06-10T04:15:12Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Re: MX6Q+LPDDR2(32bit) boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315498#M41619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raymond&lt;/P&gt;&lt;P&gt;I would suggest to start&lt;/P&gt;&lt;P&gt;with attached examples. One uses iRAM,&lt;/P&gt;&lt;P&gt;second DDR3 - you can modify it for LPDDR2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Optionally you can build SDK examples and run in iRAM using link below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95853"&gt;iRAM (OCRAM) i.MX6 SDK Application&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;Best regards&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 07:33:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-LPDDR2-32bit-boot-issue/m-p/315498#M41619</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-10T07:33:08Z</dc:date>
    </item>
  </channel>
</rss>